This shows you the differences between two versions of the page.
Next revisionBoth sides next revision | |||
resources:eval:sdp:sdp-s:getting_started [22 Jul 2011 16:17] – created Jean McAdam | resources:eval:sdp:sdp-s:getting_started [03 Aug 2011 10:10] – Edited figure GS1 Jean McAdam | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ~~UNDERCONSTRUCTION~~ | + | ~~UNDERCONSTRUCTION~~under construction |
====== Getting Started ====== | ====== Getting Started ====== | ||
+ | |||
+ | This chapter provides specific information to assist you with using the SDP board as part of your evaluation system. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | ===== Package Contents ===== | ||
+ | Your EVAL-SDP-CS1Z board package contains the following items. | ||
+ | * [[adi> | ||
+ | * 1m USB Standard-A to mini-B cable | ||
+ | Contact the vendor where you purchased your SDP board or contact Analog Devices, Inc. if any item is missing. | ||
+ | |||
+ | ===== PC Configuration ===== | ||
+ | For correct operation of the SDP board, your computer must have the following minimum configuration | ||
+ | * Windows XP Service Pack 2 or Windows Vista | ||
+ | * USB 2.0 port | ||
+ | |||
+ | <note warning> | ||
+ | |||
+ | When removing the SDP board from the package, handle the board carefully to avoid the discharge of static electricity, | ||
+ | |||
+ | ===== USB Installation ===== | ||
+ | |||
+ | Perform the following tasks to safely install the SDP board onto the computer. | ||
+ | |||
+ | There are two stages in the software application installation procedure. The first installs the application software. The second installs the .NET Framework 3.5 and the necessary drivers. | ||
+ | - Run the application install provided. The first stage will install the Applications GUI and necessary support files onto the computer | ||
+ | - Immediately following the application install, the .NET Framework 3.5 and the driver package for the SDP board is installed. If the .NET Framework 3.5 is already pre-installed on the computer in question, this stage will be skipped and step two will consist of a driver package installation only | ||
+ | |||
+ | ===== Connecting the SDP Board to the PC ===== | ||
+ | * Attach the SDP board to a USB 2.0 port on the computer via the Standard-A to Mini-B cable provided. | ||
+ | |||
+ | ==== Verifying Driver Installation ==== | ||
+ | |||
+ | Before using the SDP board, verify the driver software has installed properly. | ||
+ | * Open the Windows Device Manager and verify the SDP board appears under ADI Development Tools as shown in figure GS1. | ||
+ | |||
+ | {{: | ||
+ | |||
+ | Figure GS1 : Device Manager showing correct SDP installation | ||
+ | ==== Powering Up/Down the SDP ==== | ||
+ | The following sections describe how to safely power up and down the SDP. | ||
+ | | ||
+ | === Powering Up the SDP Board === | ||
+ | - Connect the SDP board to the daughter evaluation board through the 120 pin mating connectors. | ||
+ | - Power the daughter board | ||
+ | - Connect the USB port on the computer to the SDP board. | ||
+ | |||
+ | === Powering Down the SDP Board === | ||
+ | - Power down the daughter evaluation board | ||
+ | - Disconnect the USB port on the computer from the SDP board | ||
+ | - Disconnect the SDP board from the daughter evaluation board | ||