This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:eval:sdp:sdp-h1:getting_started [08 Oct 2012 11:00] – created Rosemary Ryan | resources:eval:sdp:sdp-h1:getting_started [08 Oct 2012 11:58] – Getting started SDP-H1 Rosemary Ryan | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== SDP-H1 Getting Started ====== | ||
+ | This page provides specific information to assist you with using the SDP board as part of your evaluation system. | ||
+ | |||
+ | ===== Package Contents ===== | ||
+ | Your EVAL-SDP-CH1Z board package contains the following items. | ||
+ | * [[adi> | ||
+ | * 1m USB Standard-A to mini-B cable | ||
+ | * 12V 30W wall wart | ||
+ | Contact the vendor where you purchased your SDP board or contact Analog Devices, Inc. if any item is missing. | ||
+ | |||
+ | ===== PC Configuration ===== | ||
+ | For correct operation of the SDP board, your computer must have the following minimum configuration | ||
+ | * Windows XP Service Pack 2 32 bit, Windows Vista 32/64 bit, Windows 7 32/64 bit | ||
+ | * USB 2.0 port | ||
+ | |||
+ | <note warning> | ||
+ | |||
+ | When removing the SDP board from the package, handle the board carefully to avoid the discharge of static electricity, | ||
+ | |||
+ | ===== USB Installation ===== | ||
+ | |||
+ | Perform the following tasks to safely install the SDP board onto the computer. | ||
+ | |||
+ | There are two stages in the software application installation procedure. The first installs the application software. The second installs the .NET Framework 3.5 and the necessary drivers. | ||
+ | - Run the application install provided. The first stage will install the Applications GUI and necessary support files onto the computer | ||
+ | - Immediately following the application install, the .NET Framework 3.5 and the driver package for the SDP board is installed. If the .NET Framework 3.5 is already pre-installed on the computer in question, this stage will be skipped and step two will consist of a driver package installation only | ||
+ | |||
+ | ===== Connecting the SDP-H1 Board to the PC ===== | ||
+ | * Attach the SDP-H1 board to a USB 2.0 port on the computer via the Standard-A to Mini-B cable provided.The SDP-H1 must be powered using the enclosed wall-wart power supply. | ||
+ | |||
+ | ==== Verifying Driver Installation ==== | ||
+ | |||
+ | Before using the SDP-H1 board, verify the driver software has installed properly. | ||
+ | * Open the Windows Device Manager and verify the SDP-H1 board appears under ADI Development Tools as shown in figure GS1. | ||
+ | {{: | ||
+ | |||
+ | Figure GS1 : Device Manager showing correct SDP installation | ||
+ | |||
+ | === Powering Up the SDP-H1 Board === | ||
+ | * Connect the daughter board to the SDP-H1 board through either the 120-pin mating connector or the FMC connector (whichever is applicable). | ||
+ | * Power the daughter board (May not be required for FMC daughterboards (mezzanine cards). See daughterboard documentation for further details). | ||
+ | * Power the SDP-H1 board with the enclosed power supply. | ||
+ | * Connect the USB port on the computer to the SDP-H1 board. | ||
+ | |||
+ | === Powering Down the SDP-H1 Board === | ||
+ | * Disconnect the SDP-H1 board power supply. | ||
+ | * Disconnect any daughterboard power supplies. | ||
+ | * Disconnect the USB port on the computer from the SDP-B board. | ||
+ | * Disconnect the daughterboard from the SDP-H1 board. | ||
+ | |||
+ | |||
+ | |||