This version is outdated by a newer approved version.This version (19 Jan 2022 13:59) is a draft.
Approvals: 0/1
This is an old revision of the document!
Evaluating the ADRF6850 100 MHz to 1000 MHz Integrated Broadband Receiver
Preface
This user guide describes both the hardware and software setup needed to evaluate ADRF6850 integrated broadband receiver using ADRF6850-EVALZ and the SDP-S controller board developed by Analog Devices.
Typical Setup
Figure 1. ADRF6850 Evaluation Setup
Tip: Click on any picture in this guide to open an enlarged version.
Helpful Files
-
Schematics:
Bill of Materials:
PCB Gerber Files:
PCB Layout:
Software Needed
Labview-based Controller Software (runs on PC with Windows 10 or earlier version Windows OS)
Hardware Needed
-
SDP-S (EVAL-SDP-CS1Z) Board which comes with
USB A to mini-B cable
Windows P.C. with ADRF6850 Software
3.3Vdc 0.5A Power Supply
0V Power Supply (or short VGAIN test point to GND)
Spectrum Analyzer (to observe 20MHz tone)
High-Frequency Signal Generator (to output 520MHz at 0dBm level)
50Ω SMA termination
2 SMA Cables
Quick Start Guide
Evaluation Software Installation
Extract the ADRF6850_
USB_v1_Installer zip file.
Inside the folders, run setup.exe.
Follow all prompts to install.
Default install destination is
C:\Program Files (x86)\ADRF6850_USB\
Run the executable either from a shortcut or by going to the location specified above and run the .exe file.
Figure 2. ADRF6850 Evaluation Software
Board Testing
Make sure that J21 is connected by default. Refer to Figure 3 below:
Figure 3. ADRF6850 Evaluation Setup
Attach the SDP-S board on the evaluation board then connect SDP-S to PC via
USB. See Figure 1.
Connect J2 (IBBP RF OUT) to the input of a spectrum analyzer. Connect the 50Ω termination to J3. Set up the analyzer as follows:
-
-
-
RBW and VBW: 100 KHz
Attn.: 30
dB (adjust until noise floor like in Figure 4 is achieved)
Connect a high-frequency signal generator to J9 (RF IN). Set the signal generator output to
520 MHz and 0 dBm, then enable the output.
Connect 3.3V 0.5A supply to VCC and GND test points then 0V VGAIN. Enable the supplies. The 3.3V supply should be sourcing current between 110
mA and 135
mA.
Run the evaluation software on PC. Refer to Figure 2.
Click “Select
SPI Mode” (top left).
Click “Write Default Settings” (just to the right of above button). The +3.3V current should increase to between 310
mA and 380
mA.
Set “LO Frequency” to 540MHz and click “Program LO Frequency”.
A tone at
20MHz with a level of
-2 dBm to -4 dBm should appear on the spectrum analyzer. The tone should be steady at a frequency of 20MHz. Refer to the screenshot in Figure 4.
Figure 4. IBBP Output Spectral Plot at IF = 20 MHz