This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:sdp:eval-adrf6755 [20 Jul 2021 21:32] – Still in progress Eric Webb | resources:eval:sdp:eval-adrf6755 [09 Aug 2021 16:20] – Eric Webb | ||
---|---|---|---|
Line 52: | Line 52: | ||
{{ : | {{ : | ||
+ | |||
+ | This section can be used to initialize the different frequency components of the board going to the PFD. | ||
==== Power Up/Down ==== | ==== Power Up/Down ==== | ||
{{ : | {{ : | ||
+ | |||
+ | This section controls what will be powered up or down on startup of the part. The charge pump current can also be configured here | ||
==== Output Settings ==== | ==== Output Settings ==== | ||
{{ : | {{ : | ||
+ | |||
+ | Here you can control both the MUXOUT and LOMON outputs. LOMON can be used to view the LO Signal while the part is in operation | ||
==== VCO and Autocalibration Settings ==== | ==== VCO and Autocalibration Settings ==== | ||
Line 65: | Line 71: | ||
{{ : | {{ : | ||
+ | This section allows you to control the auto-calibration time as well as disable auto-calibration altogether | ||
+ | |||
==== Lock Detector ==== | ==== Lock Detector ==== | ||
{{ : | {{ : | ||
+ | This section is used to enable/ | ||
+ | |||
+ | ===== Basic Test Case ===== | ||
+ | |||
+ | 1. Begin by enabling the modulator power up setting | ||
+ | |||
+ | 2. Attach a +5.0V supply to the DUT pin with a current limit of 400mA | ||
+ | |||
+ | 3. Attach a Spectrum Analyzer to the RFOut pin of the ADRF6755 | ||
+ | |||
+ | 4. Hit the apply button at the bottom of the ACE | ||
+ | |||
+ | 5. Set the center frequency of the Spectrum Analyzer to 1875MHz and the span to 80MHz | ||
+ | |||
+ | {{: | ||
+ | |||
+ | 6. Measure the output frequency and output power of the main RF output on the spectrum analyzer. The highest power tone at 1850MHz should read be greater than -4dBm | ||
+ | |||
+ | 7. The power of the carrier feedthrough at 1875MHz should be at least 45dB below the 1850MHz tone (-45dBc) | ||
+ | 8. The power of the suppressed sideband at 1900MHz should be at least 30dB below the 1850MHz tone (-30dBc) | ||