This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:sdp:bemicro_sdp [03 Jan 2021 22:11] – fix links Robin Getz | resources:eval:sdp:bemicro_sdp [08 Jan 2021 10:51] – Fixed bad link for SDP-BEMICRO Ioana Chelaru | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== More information ===== | ===== More information ===== | ||
- | [[adi>en/data-converters/ | + | [[adi>SDP-BEMICRO|BeMicro SDK/SDP Interposer]] Information webpage on Analog.com |
<WRAP tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</ | <WRAP tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</ |