This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:sdp:bemicro_sdp [26 Oct 2011 17:06] – Added link to BeMicro Code Jean McAdam | resources:eval:sdp:bemicro_sdp [03 Jan 2021 22:11] – fix links Robin Getz | ||
---|---|---|---|
Line 6: | Line 6: | ||
===== More information ===== | ===== More information ===== | ||
- | [[http:// | + | [[adi>en/ |
- | <note tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</note> | + | <WRAP tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</WRAP> |
==== ADI Authorized Distributors ==== | ==== ADI Authorized Distributors ==== |