This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:sdp:bemicro_sdp [29 Jun 2011 22:22] – Approved Robin Getz | resources:eval:sdp:bemicro_sdp [25 Jan 2021 11:52] – Fixed bad links Ioana Chelaru | ||
---|---|---|---|
Line 2: | Line 2: | ||
===== Preface ===== | ===== Preface ===== | ||
- | The BeMicro SDK/SDP Interposer board is an adaptor that allows Arrow’s [[http://www.arrownac.com/offers/altera-corporation/altera-bemicro|BeMicro SDK]] USB stick to connect to all daughter boards on the SDP Platform. The BeMicro SDK/SDP Interposer provides embedded FPGA system developers the chance to prototype their FPGA + ADI data converter, mixed signal or RF system concept quickly and easily.\\ | + | The BeMicro SDK/SDP Interposer board is an adaptor that allows Arrow’s [[https://www.arrow.com/en/datasheets/89166696/ |
===== More information ===== | ===== More information ===== | ||
- | | + | [[adi> |
- | * [[http:// | + | |
+ | <WRAP tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</ | ||
+ | |||
+ | ==== ADI Authorized Distributors ==== | ||
+ | |||
+ | | ||
+ | * [[http:// | ||
+ | |||
+ | ==== Design Partner/ | ||
* [[http:// | * [[http:// | ||
- | <note tip>This interposer is not an ADI product, and information here is shown to help out ADI's customers who which to evaluate an ADI product with the BeMicro SDK. The BeMicro SDK/SDP Interposer has nothing to do with the SDP Controller Boards, and the BeMicro SDK will not run the SDP product evaluation software. As such, it is not avalible for sale from ADI.</ | ||
===== Product Overview ===== | ===== Product Overview ===== | ||
Line 35: | Line 43: | ||
As such, in order to properly use the BeMicro SDK/SDP Interposer, you will need both of: | As such, in order to properly use the BeMicro SDK/SDP Interposer, you will need both of: | ||
- | * the [[http://www.arrownac.com/offers/altera-corporation/altera-bemicro/|BeMicro SDK]] | + | * the [[https://www.arrow.com/en/datasheets/89166696/ |
* an [[adi>/ | * an [[adi>/ | ||
- | ===== Projects ===== | + | ===== Sample |
- | Projects which show basic connectivity between the BeMicro SDK and the ADI SDP Daughter cards will be pubished | + | Projects which show basic connectivity between the BeMicro SDK and the ADI SDP Daughter cards are available |
- | + | [[resources: | |