This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ltc6952-ace-software-guide [23 Aug 2022 09:48] – size of the screenshots modified Emrecan Gidik | resources:eval:ltc6952-ace-software-guide [23 Aug 2022 13:41] (current) – table edit Emrecan Gidik | ||
---|---|---|---|
Line 5: | Line 5: | ||
The VTUNE and VCO SMAs can mate directly with the DC2664A VCO rider board. This option allows for a quick method to evaluate multiple VCOs. A DC2026 USB serial controller board is used for SPI communication with the LTC6952, controlled by the ACE™ software and LTC6952 Plugin. | The VTUNE and VCO SMAs can mate directly with the DC2664A VCO rider board. This option allows for a quick method to evaluate multiple VCOs. A DC2026 USB serial controller board is used for SPI communication with the LTC6952, controlled by the ACE™ software and LTC6952 Plugin. | ||
{{ : | {{ : | ||
+ | < | ||
+ | |||
===== Getting Started ===== | ===== Getting Started ===== | ||
Line 14: | Line 16: | ||
The DC2026 has the ability to run Linduino code, refer to [[adi> | The DC2026 has the ability to run Linduino code, refer to [[adi> | ||
{{ : | {{ : | ||
+ | < | ||
==== ACE and Plugin Installation ==== | ==== ACE and Plugin Installation ==== | ||
Line 22: | Line 25: | ||
* Search for Board.LTC6952 and install plug-in | * Search for Board.LTC6952 and install plug-in | ||
{{ : | {{ : | ||
+ | < | ||
==== Evaluation Board Set-Up ==== | ==== Evaluation Board Set-Up ==== | ||
Line 28: | Line 32: | ||
- Run the ACE application. Double click the LTC6952 icon that appears on the Attached Hardware tab when the DC2026 board is connected and attached to the board. If the icon does not appear, consider re-installing the LTC6952 plug-in or try refreshing the Attached hardware icon. | - Run the ACE application. Double click the LTC6952 icon that appears on the Attached Hardware tab when the DC2026 board is connected and attached to the board. If the icon does not appear, consider re-installing the LTC6952 plug-in or try refreshing the Attached hardware icon. | ||
- {{ : | - {{ : | ||
+ | < | ||
- Connection is automatically established with DC2026. You can navigate to board and chip view. | - Connection is automatically established with DC2026. You can navigate to board and chip view. | ||
- Double click the LTC6952 Board Icon and the tab shown in Figure 5 appears. | - Double click the LTC6952 Board Icon and the tab shown in Figure 5 appears. | ||
- Double click the LTC6952 icon that appears on the LTC6952 Board tab to open the main control window shown in Figure 6 | - Double click the LTC6952 icon that appears on the LTC6952 Board tab to open the main control window shown in Figure 6 | ||
{{ : | {{ : | ||
+ | < | ||
==== General Software Features ==== | ==== General Software Features ==== | ||
In chip view, one can find various control features of LTC6952. One can read and control all registers which mentioned in the [[adi> | In chip view, one can find various control features of LTC6952. One can read and control all registers which mentioned in the [[adi> | ||
Line 47: | Line 53: | ||
By clicking Proceed to Memory Map button or Memory Map Side-By-Side button, register values can be seen. | By clicking Proceed to Memory Map button or Memory Map Side-By-Side button, register values can be seen. | ||
{{ : | {{ : | ||
+ | < | ||
+ | |||
+ | |||
+ | ===== CML OUTPUTS, OUT[10:0] ===== | ||
+ | |||
+ | The DC2609A has 11 CML outputs. OUT[9:0] have matching trace lengths, which are optimized for skew measurements. OUT10’s trace lengths are longer than the other outputs traces due to the shape of the DC2609A. | ||
+ | |||
+ | Six of these outputs are AC-coupled and brought out to SMAs (OUT9, OUT8, OUT5, OUT4, OUT1, and OUT0). To drive 50Ω impedance instruments connect OUTx+ to the instrument and OUTx– to a 50Ω termination, | ||
+ | |||
+ | The remaining five outputs (OUT10, OUT7, OUT6, OUT3, and OUT2) are terminated with a 100Ω resistor onboard. To connect these outputs to a 50Ω instrument, remove the 100Ω termination, | ||
+ | |||
+ | Refer to LTC6952 data sheet for differential termination options. | ||
+ | |||
+ | ===== Typical DC2609A Requirements and Characteristics===== | ||
+ | |||
+ | ^Parameter | ||
+ | |9V-12V Power Supply|Input | ||
+ | |4V-6V Power Supply |Input | ||
+ | |GND |Output|J33 Banana Jack |Pair with J30 and J32 | | ||
+ | |OUT9+; OUT9– | ||
+ | |OUT8+; OUT8– | ||
+ | |OUT5+; OUT5– | ||
+ | |OUT4+; OUT4– | ||
+ | |OUT1+; OUT1– | ||
+ | |OUT0+; OUT0– | ||
+ | |OUT10+; OUT10– | ||
+ | |OUT7+; OUT7– | ||
+ | |OUT6+; OUT6– | ||
+ | |OUT3+; OUT3– | ||
+ | |OUT2+; OUT2– | ||
+ | |VCO+; VCO– | ||
+ | |REF+; | ||
+ | |EZS_SRQ+ | ||
+ | |EZS_SRQ– | ||
+ | |ISD |Input | ||
+ | |STAT | ||
+ | |||
+ | *Any unused RF output must be powered down or terminated with 50Ω, or poor spurious performance may result. | ||
+ | < | ||
===== Troubleshooting ===== | ===== Troubleshooting ===== | ||
**If the green LEDs (D2, D3, or D4) do not illuminate: | **If the green LEDs (D2, D3, or D4) do not illuminate: | ||
Line 71: | Line 116: | ||
To verify communication with the DC2609A, Go to the start page or system view page and click the button shown below. | To verify communication with the DC2609A, Go to the start page or system view page and click the button shown below. | ||
{{ : | {{ : | ||
+ | < | ||
LEDs on the Serial Interface Boards don’t light up, then perform the following steps: | LEDs on the Serial Interface Boards don’t light up, then perform the following steps: |