Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision |
resources:eval:hmcad15xx [08 Nov 2021 04:38] – new information added for the new evalboard (HMCAD1520-EBZ) Mark Arthur Recio | resources:eval:hmcad15xx [30 May 2022 04:25] – [Quick Start Guide] John Xavier Toledo |
---|
* {{ :resources:eval:eval01-hmcad15xx_user_guide_analog_devices_wiki_.pdf | Previous User Guide}} for EVAL01-HMCAD15xx Evaluation Board | * {{ :resources:eval:eval01-hmcad15xx_user_guide_analog_devices_wiki_.pdf | Previous User Guide}} for EVAL01-HMCAD15xx Evaluation Board |
* [[adi>media/en/technical-documentation/data-sheets/hmcad1520.pdf|HMCAD1520]] and [[adi>media/en/technical-documentation/data-sheets/hmcad1511.pdf|HMCAD1511]] Datasheet | * [[adi>media/en/technical-documentation/data-sheets/hmcad1520.pdf|HMCAD1520]] and [[adi>media/en/technical-documentation/data-sheets/hmcad1511.pdf|HMCAD1511]] Datasheet |
* {{ :resources:eval:02-067426-01-b_1_.pdf | HMCAD15xx-EBZ Schematic}} | * {{ :resources:eval:02-067426-01-d.pdf | HMCAD15xx-EBZ Schematic}} |
* {{ :resources:eval:05-067426-01-b_1_.xls | HMCAD15xx-EBZ BOM}} | * {{ :resources:eval:05-067426-01-d.xls | HMCAD15xx-EBZ BOM}} |
* {{ :resources:eval:08-067426-01-b.pdf | PCB Layout}} | * {{ :resources:eval:08-067426-01-b.pdf | PCB Layout}} |
* {{ :resources:eval:20-067426-01b_1_.zip | PCB Gerber Files}} | * {{ :resources:eval:20-067426-01b_1_.zip | PCB Gerber Files}} |
| * {{ :resources:eval:hmcad15xx_interleaving_spur_calculator.xls | HMCAD15xx-EBZ Interleaving Spurs Calculator}} |
| |
=====Software Needed:===== | =====Software Needed:===== |
=====Evaluation Board Hardware ===== | =====Evaluation Board Hardware ===== |
====Analog Inputs==== | ====Analog Inputs==== |
[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1520.html|HMCAD1520-EBZ]] /[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] evaluation board has four input channels that supports single-ended to differential conversion with the use of a balun. By default, input channels 3 and 4 (SMAs J6 and J7) are balun-coupled; while input channel 1 (SMAs J3 and J4) and input channel 2 (SMA J5) uses the onboard [[adi>en/products/ltc6419.html|LTC6419]] high-speed differential ADC driver. | [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1520.html|HMCAD1520-EBZ]] /[[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] evaluation board has four input channels that supports single-ended to differential conversion with the use of a balun. By default, all input channels 1-4 (SMAs J3, J5, J6 and J7) are balun-coupled. Alternatively, input channel 1 (SMAs J3 and J4) can be configured to differential to differential conversion, and input channel 2 (SMA J5) can be configured to single-ended to differential conversion using the onboard [[adi>en/products/ltc6419.html|LTC6419]] high-speed differential ADC driver. |
| |
Refer to the table below for the default configuration. | Refer to the table below for the optional amplifier configuration. |
| |
| |
^ Analog Input Channel Number ^ Default Input Driver ^ Coupling of analog input signal (AC/DC) ^Signal type on Input/Output ^Additional Comments/Application Notes ^ | ^ Analog Input Channel Number ^ Default Input Driver, AC/DC coupling ^Signal type on Input/Output ^Install ^Uninstall ^ |
| 1 | LTC6419 | DC coupling | Differential/Differential | Unity gain| | | 1 | LTC6419, DC coupling, Unity Gain | Differential/Differential |R23, R24, R41, R42, R45, R60, R61 |R56, R57 | |
| 2 | LTC6419 | DC coupling | Single-Ended/Differential | Unity gain| | | 2 | LTC6419, DC coupling, Unity Gain | Single-Ended/Differential |R23, R24, R46, R58, R59| C53, R54, R55 | |
| 3 | Balun | AC coupling | Single-Ended/Differential | Balun only supports 4.5 to 3000MHz input frequency| | |
| 4 | Balun | AC coupling | Single-Ended/Differential | Balun only supports 4.5 to 3000MHz input frequency| | |
| |
====Analog Input Vcm==== | ====Analog Input Vcm==== |
| |
On the other hand, the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] evaluation board has an on-board 1GHz crystal for clocking the [[adi>media/en/technical-documentation/data-sheets/hmcad1511.pdf|HMCAD1511]]. The user can also configure the board to use an external clock source for the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] board. | On the other hand, the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] evaluation board has an on-board 1GHz crystal for clocking the [[adi>media/en/technical-documentation/data-sheets/hmcad1511.pdf|HMCAD1511]]. The user can also configure the board to use an external clock source for the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] board. |
| |
| Refer to the table below for alternative clock configuration |
| |
| ^Clock Configuration ^Install ^Uninstall ^ |
| | Onboard | R13 | R12 | |
| |External | R12 | R13 | |
| |
====Power Supply==== | ====Power Supply==== |
- Click the **Proceed to Analysis** and click on the **FFT Tab**. Click Run Once to capture an FFT plot. | - Click the **Proceed to Analysis** and click on the **FFT Tab**. Click Run Once to capture an FFT plot. |
- Observe the fundamental frequency and power. Adjust the signal source to obtain -1dBFS fundamental power at 71MHz.<WRAP centeralign>{{ :resources:eval:hmcad1520_fft.jpg?direct&800 |}}//Figure 4. HMCAD1520-EBZ FFT Window//</WRAP> | - Observe the fundamental frequency and power. Adjust the signal source to obtain -1dBFS fundamental power at 71MHz.<WRAP centeralign>{{ :resources:eval:hmcad1520_fft.jpg?direct&800 |}}//Figure 4. HMCAD1520-EBZ FFT Window//</WRAP> |
| - For the manual input of interleaving spurs, go to the **Analysis Tab** and click the **Dynamic Settings**. |
| - Proceed to the **FFT Spurs** Section and click the "+" button on the side and input the following frequencies provided from the spur calculator (refer to the tip below). Then, click **OK**. Figure 5 shows the FFT spurs section of the Quad Mode for 160 MSPS and 70 MHz input.<WRAP centeralign>{{ :resources:eval:hmcad1520_interleave_spurs.png?direct&800 |}}//Figure 5. HMCAD1520-EBZ FFT Spurs Section for Quad Mode (Fs =160MSPS and Fin = 70MHz)//</WRAP> |
| - Lastly, click the **Rerun Analysis**. |
| |
| <note tip>For your reference on what frequencies to include in the section, you can download the **HMCAD15xx-Interleaving Spurs Calculator** in the [[/resources/eval/hmcad15xx#helpful_files|Helpful Files]], and input both the sampling and input frequencies on the yellow boxes provided. The calculator will provide the spur frequencies depending on the selected mode.</note> |
| |
| |
| <note>**Note:** In case the [[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HMCAD1511.html|HMCAD1511-EBZ]] is operating at maximum sampling frequency Fsmax and no data capture is shown, try the following steps below: |
| - When using external clock, decrease the sampling frequency of HMCAD1511 less than the Fsmax of 250MHz/500MHz/1000MHz for quad/dual/single mode. |
| - When using on-board clock, adjust the clock divider making the sampling frequency of HMCAD1511 less than the fsmax of 250MHz/500MHz/1000MHz for quad/dual/single mode. |
| </note> |
| |
| |
| |
| |
====Compensation for Interleaving Spurs on Noise Calculation==== | ====Visual Analog Export for Interleaving Spurs on Noise Calculation==== |
The [[adi>HMCAD1520|HMCAD1520]] and [[adi>HMCAD1511|HMCAD1511]] have interleaving spurs that can be observed at the output. To obtain the AC performance measurements as seen on the typical spec on the datasheet, follow these procedures. | The [[adi>HMCAD1520|HMCAD1520]] and [[adi>HMCAD1511|HMCAD1511]] have interleaving spurs that can be observed at the output. To obtain the AC performance measurements as seen on the typical specification on the datasheet, follow these procedures. |
- On the **Results** tab of the **Analysis** window at ACE, click **Export**. Make sure to export 1 data set at a time to avoid editing the csv file on Visual Analog. To do this, only select 1 channel at the **Display Channels** at the top. <WRAP centeralign>{{ :resources:eval:hmcad1520_ace_export.jpg?direct&400 |}}//Figure 5. HMCAD1520-EBZ ACE Data Export//</WRAP> | - On the **Results** tab of the **Analysis** window at ACE, click **Export**. Make sure to export 1 data set at a time to avoid editing the csv file on Visual Analog. To do this, only select 1 channel at the **Display Channels** at the top. <WRAP centeralign>{{ :resources:eval:hmcad1520_ace_export.jpg?direct&400 |}}//Figure 6. HMCAD1520-EBZ ACE Data Export//</WRAP> |
- Install Visual Analog and install the appropriate canvas for the specific channel mode. These are AD9230 VA canvas that is modified to accommodate the HMCAD15xx device. **Download the canvas here:** {{ :resources:eval:hmcad15xx_visualanalog_canvas.zip |}} | - Install Visual Analog and install the appropriate canvas for the specific channel mode. These are AD9230 VA canvas that is modified to accommodate the HMCAD15xx device. **Download the canvas here:** {{ :resources:eval:hmcad15xx_visualanalog_canvas.zip |}} |
- On the Browse button, open the //**_RawSamples.csv**// file exported from the ACE software. Indicate the correct sampling frequency on the **Pattern Loader** block, and the correct resolution at the **Input Formatter** block. The **Resolution** and **Alignment** value should be the same.<WRAP centeralign>{{ :resources:eval:hmcad1520_va_setting.jpg?direct&400 |}}{{ :resources:eval:hmcad1520_input_formatter.jpg?direct&400 |}}//Figure 6. Visual Analog Settings//</WRAP> | - On the Browse button, open the //**_RawSamples.csv**// file exported from the ACE software. Indicate the correct sampling frequency on the **Pattern Loader** block, and the correct resolution at the **Input Formatter** block. The **Resolution** and **Alignment** value should be the same.<WRAP centeralign>{{ :resources:eval:hmcad1520_va_setting.jpg?direct&400 |}}{{ :resources:eval:hmcad1520_input_formatter.jpg?direct&400 |}}//Figure 7. Visual Analog Settings//</WRAP> |
- Click **Run** button on the top left part. | - Click **Run** button on the top left part. |
- The FFT plot on the left includes the interleaving spurs on the calculations (which is the same with the ACE Results), while the FFT plot on the right excludes the interleaving spurs on the calculations.<WRAP centeralign>{{ :resources:eval:hmcad1520_fft_va.jpg?direct&800 |}}//Figure 7. Visual Analog FFT Plots//</WRAP> | - The FFT plot on the left includes the interleaving spurs on the calculations (which is the same with the ACE Results), while the FFT plot on the right excludes the interleaving spurs on the calculations.<WRAP centeralign>{{ :resources:eval:hmcad1520_fft_va.jpg?direct&800 |}}//Figure 8. Visual Analog FFT Plots//</WRAP> |
| |
=====Troubleshooting Tips===== | =====Troubleshooting Tips===== |