This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:hmcad15xx [25 Jan 2023 20:11] – Draft 1/25 Deferson Romero | resources:eval:hmcad15xx [06 Feb 2023 06:29] – Draft 2/6 Deferson Romero | ||
---|---|---|---|
Line 46: | Line 46: | ||
^ Analog Input Channel Number | ^ Analog Input Channel Number | ||
- | | 1 | LTC6419, DC coupling, Unity Gain | Differential/ | + | | 1 | LTC6419, DC coupling, Unity Gain | Differential/ |
- | | 2 | LTC6419, DC coupling, Unity Gain | Single-Ended/ | + | | 2 | LTC6419, DC coupling, Unity Gain | Single-Ended/ |
====Analog Input Vcm==== | ====Analog Input Vcm==== | ||
Line 96: | Line 96: | ||
This section is intended to provide evaluation board characterization results on Differential-to-Differential configuration in Channel 1 using the LTC6419 amplifier as shown in Figure 7, and on Single-to-Differential configuration in Channel 2 using the said amplifier as shown in Figure 8. | This section is intended to provide evaluation board characterization results on Differential-to-Differential configuration in Channel 1 using the LTC6419 amplifier as shown in Figure 7, and on Single-to-Differential configuration in Channel 2 using the said amplifier as shown in Figure 8. | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | <WRAP centeralign> | + | <WRAP centeralign> |
=====Troubleshooting Tips===== | =====Troubleshooting Tips===== | ||
If the FFT window remains blank after Running Once in ACE, do the following: | If the FFT window remains blank after Running Once in ACE, do the following: |