This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:hmc8362_and_hmc8364_user_guide [12 Aug 2020 12:32] – [EVALUATION BOARD SOFTWARE] Kieran Barrett | resources:eval:hmc8362_and_hmc8364_user_guide [12 Aug 2020 13:04] – Kieran Barrett | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | |||
====== EV1HMC8362LP6G/ | ====== EV1HMC8362LP6G/ | ||
====Evaluating the HMC8362/ | ====Evaluating the HMC8362/ | ||
Line 94: | Line 95: | ||
====EVALUATION BOARD SOFTWARE==== | ====EVALUATION BOARD SOFTWARE==== | ||
===SOFTWARE=== | ===SOFTWARE=== | ||
- | Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino [[adi> | + | Currently there is no software available for the EV1HMC8362LP6G and EV1HMC8364LP6G because they can be evaluated without the use of software. However, the EV1HMC8362LP6G and EV1HMC8364LP6G are configured in a manner that allows use of a Linduino [[adi> |
- | To connect the Arduino Uno microcontroller | + | To connect the [[adi> |
+ | |||
+ | {{ : | ||
+ | Figure 3. SDP-K1 Board mounted to EV1HMC8362LP6 | ||
====EVALUATION AND TEST==== | ====EVALUATION AND TEST==== |