This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:ezlinx:windows_xp_installation_and_setup_guide [26 Jul 2013 15:50] – [Setting up the gadget ethernet IP Address] Hichem Ben Charrada | resources:eval:ezlinx:windows_xp_installation_and_setup_guide [20 Aug 2013 12:10] – [Setting up the ezLINX board IP address] Liam Delahunt | ||
---|---|---|---|
Line 74: | Line 74: | ||
===== Setting up the ezLINX board IP address ===== | ===== Setting up the ezLINX board IP address ===== | ||
Open the ezLINX application window and click on the board icon in the bottom left corner of the window (or click on Configure button). In the IP address settings enter the following: \\ | Open the ezLINX application window and click on the board icon in the bottom left corner of the window (or click on Configure button). In the IP address settings enter the following: \\ | ||
- | {{ : | + | {{ : |
Now click the "use changes" | Now click the "use changes" | ||
===== Verify Connection ===== | ===== Verify Connection ===== |