This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
ezlinx:usb-ip-config [14 May 2012 16:24] – created Neil Quinn | resources:eval:ezlinx:usb-ip-config [14 Apr 2021 23:34] (current) – added retired page tag Neil Quinn | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ===== ezLINX™ Device Driver Installation ===== | + | {{page>/ |
+ | |||
+ | \\ | ||
+ | [[resources/ | ||
+ | \\ | ||
+ | |||
+ | ====== ezLINX™ | ||
+ | ===== Device Driver Installation ===== | ||
A driver must be installed in order to connect to the //ez//LINX Development Platform using the sample PC Application. Instructions to install this device driver are given below. | A driver must be installed in order to connect to the //ez//LINX Development Platform using the sample PC Application. Instructions to install this device driver are given below. | ||
Line 16: | Line 23: | ||
{{ : | {{ : | ||
- | Click on the pop-up which brings up the "Found New Hardware" | + | The device can also be found by accessing the device manager (Control Panel -> System -> Hardware) and looking for the Linux USB Ethernet/ |
+ | |||
+ | {{: | ||
+ | {{ : | ||
+ | {{ : | ||
+ | |||
+ | \\ \\ | ||
+ | |||
+ | Click on the pop-up which brings up the "Found New Hardware" | ||
{{: | {{: | ||
Line 33: | Line 49: | ||
- | Once the USB driver is sucessfully installed, the IP address for the device must be configured. | + | Once the USB driver is sucessfully installed, the IP address for the device must be configur |
+ | ed. | ||
===== Network Adapter IP Configuration ===== | ===== Network Adapter IP Configuration ===== |