Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:ezlinx:isolated-usb [28 May 2012 11:40] – Approved Hein Maraisresources:eval:ezlinx:isolated-usb [03 Jan 2021 22:04] (current) – fix links Robin Getz
Line 7: Line 7:
 ===== Hardware Implementation ===== ===== Hardware Implementation =====
  
-The Isolated USB port is implemented using the [[http://www.analog.com/adum3160|ADuM3160]] Full speed USB Isolator. The [[http://www.analog.com/adum3160|ADuM3160]] connects to the integrated USB PHY of the ADSP-BF548 and is capable of functioning at data rates of up to 12Mbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[http://www.analog.com/adum3160|ADuM3160]] on the //ez//LINX hardware.+The Isolated USB port is implemented using the [[adi>adum3160|ADuM3160]] Full speed USB Isolator. The [[adi>adum3160|ADuM3160]] connects to the integrated USB PHY of the ADSP-BF548 and is capable of functioning at data rates of up to 12Mbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>adum3160|ADuM3160]] on the //ez//LINX hardware.
  
  
Line 15: Line 15:
 \\ \\
  
-The VBUS1 and VDD1 of the [[http://www.analog.com/adum3160|ADuM3160]] is powered from the 5V bus power supply. VBUS2 and VDD2 is powered from 3.3V generated by the //ez//LINX power supply. A mini USB-B connector is used for easy connection to a USB master.+The VBUS1 and VDD1 of the [[adi>adum3160|ADuM3160]] is powered from the 5V bus power supply. VBUS2 and VDD2 is powered from 3.3V generated by the //ez//LINX power supply. A mini USB-B connector is used for easy connection to a USB master.
  
 \\ \\
  
resources/eval/ezlinx/isolated-usb.1338198045.txt.gz · Last modified: 28 May 2012 11:40 by Hein Marais