This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
ezlinx:isolated-usb [09 May 2012 15:51] – Improved layout Neil Quinn | resources:eval:ezlinx:isolated-usb [28 May 2012 11:40] – Approved Hein Marais | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== Isolated USB ====== | ||
- | |||
- | ===== Hardware Implementation ===== | ||
- | |||
- | The Isolated USB port is implemented using the [[http:// | ||
- | |||
- | |||
- | |||
- | |||
- | {{ : | ||
- | |||
\\ | \\ | ||
- | + | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] | |
- | The VBUS1 and VDD1 of the [[http://www.analog.com/ | + | |
- | + | ||
- | A mini USB-B connector is used for easy connection to a USB master. | + | |
\\ | \\ | ||
+ | ====== ezLINX™ Isolated USB Implementation====== | ||
- | ===== Setup ===== | + | ===== Hardware Implementation |
- | ==== Device Installation ==== | + | The Isolated USB port is implemented using the [[http:// |
- | A driver must be installed in order to connect to the //ez//LINX Development Platform using the sample PC Application. Instructions to install this device driver are given below. | ||
- | <WRAP center round download 20% right> | ||
- | {{: | ||
- | </ | ||
- | <WRAP center round important 62% left> | ||
- | **Warning: | ||
- | </ | ||
- | \\ | ||
- | |||
- | First download and extract the above USB Gadget Driver file. To install the USB gadget first plug it into the target PC. A pop-up will appear (see below) saying that Windows has found a new hardware device called a " | ||
- | |||
- | {{ : | ||
- | |||
- | Click on the pop-up which brings up the " | ||
- | |||
- | {{: | ||
- | {{ : | ||
- | |||
- | \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ | ||
- | |||
- | If a " | ||
+ | {{ : | ||
\\ | \\ | ||
- | {{:ezlinx: | + | The VBUS1 and VDD1 of the [[http://www.analog.com/ |
- | {{ : | + | |
- | + | ||
- | \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ \\ | + | |
- | + | ||
- | + | ||
- | Once the USB driver | + | |
- | + | ||
- | ==== IP Configuration ==== | + | |
- | + | ||
- | To set up the network adapter to connect with the // | + | |
- | \\ | + | |
- | + | ||
- | {{ : | + | |
\\ | \\ | ||
- | |||
- | The below window should then open. Select "Use the following IP address" | ||
- | |||
- | **IP Address:** 192.168.1.100\\ | ||
- | **Subnet mask:** 255.255.255.0\\ | ||
- | **Default gateway:** 192.168.1.1\\ | ||
- | \\ | ||
- | {{ : | ||
- | \\ | ||
- | |||
- | Select Ok to confirm. Now the host and the device are on the same network. | ||
- | |||
- | <WRAP center round important 60%> | ||
- | **Note:** Switching the USB port used for the Gadget Ethernet device will require you to perform the above steps again, setting up the appropriate IP address and gateway for the USB device. | ||
- | </ | ||
- | |||