This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:ezlinx:isolated-spi [16 May 2012 18:53] – Approved Hein Marais | resources:eval:ezlinx:isolated-spi [25 Jun 2012 11:05] – Added jumpers 36, 37, 38 and 39 Neil Quinn | ||
---|---|---|---|
Line 1: | Line 1: | ||
\\ | \\ | ||
- | [[resources/ | + | [[resources/ |
\\ | \\ | ||
====== ezLINX™ Isolated SPI Implementation====== | ====== ezLINX™ Isolated SPI Implementation====== | ||
Line 12: | Line 12: | ||
These jumper settings are given in the table below: | These jumper settings are given in the table below: | ||
- | | ^ JP5 ^ JP6 ^ JP7 ^ JP8 ^ JP9 ^ JP10 ^ JP11 ^ JP12 ^ JP13 ^ JP14 ^ JP15 ^ JP16 ^ JP20 ^ JP21 ^ | + | | ^ JP5 ^ JP6 ^ JP7 ^ JP8 ^ JP9 ^ JP10 ^ JP11 ^ JP12 ^ JP13 ^ JP14 ^ JP15 ^ JP16 ^ JP20 ^ JP21 |
- | ^ SPI1 Master | + | ^ SPI1 Master |
- | ^ SPI1 Slave | Open | Connect | + | ^ SPI1 Slave | Open | Connect |
\\ | \\ | ||
Line 28: | Line 28: | ||
These jumper settings are given in the table below: | These jumper settings are given in the table below: | ||
- | | ^ JP22 ^ JP23 ^ JP24 ^ JP25 ^ JP26 ^ JP27 ^ JP28 ^ JP29 ^ JP30 ^ JP31 ^ JP32 ^ JP33 ^ JP34 ^ JP35 ^ | + | | ^ JP22 ^ JP23 ^ JP24 ^ JP25 ^ JP26 ^ JP27 ^ JP28 ^ JP29 ^ JP30 ^ JP31 ^ JP32 ^ JP33 ^ JP34 ^ JP35 |
- | ^ SPI2 Master | + | ^ SPI2 Master |
- | ^ SPI2 Slave | Open | Connect | + | ^ SPI2 Slave | Open | Connect |
\\ | \\ |