This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:ezlinx:isolated-rs485-rs422 [28 May 2012 12:49] – Approved Hein Marais | resources:eval:ezlinx:isolated-rs485-rs422 [03 Jan 2021 22:04] – fix links Robin Getz | ||
---|---|---|---|
Line 5: | Line 5: | ||
====== ezLINX™ Isolated RS-485 / RS-422 Implementation====== | ====== ezLINX™ Isolated RS-485 / RS-422 Implementation====== | ||
- | The Isolated RS-485 and RS-422 port is implemented using the [[http:// | + | The Isolated RS-485 and RS-422 port is implemented using the [[adi>ADM2587E|ADM2587E]] Signal and Power isolated CAN transceiver. The [[adi>ADM2587E|ADM2587E]] connects to UART2 of the ADSP-BF548 and is capable of functioning at data rates of up to 500kbit/s. Figure 1 below shows a circuit diagram of the implementation of the [[adi>ADM2587E|ADM2587E]] on the //ez//LINX hardware. |
\\ | \\ | ||
Line 11: | Line 11: | ||
\\ | \\ | ||
- | The RS-485 Node can be configured using jumpers JP3, JP4, JP19 and JP40. To configure the node as a half-duplex RS-485 node, connect JP3 and JP4. When JP3 is fitted, it will connect B to Z, and when JP4 is fitted it will connect A to Y. When JP3 and JP4 are removed, the node will be configured as a full duplex RS-485 node or as an RS-422 node. When JP19 is fitted, the A and B pins will be terminated with 120Ω. If termination is not required, remove JP19. When JP40 is connected a pull-up resistor on the RxD pin of 10kΩ will be connected. This jumper should be connected when using the [[http:// | + | The RS-485 Node can be configured using jumpers JP3, JP4, JP19 and JP40. To configure the node as a half-duplex RS-485 node, connect JP3 and JP4. When JP3 is fitted, it will connect B to Z, and when JP4 is fitted it will connect A to Y. When JP3 and JP4 are removed, the node will be configured as a full duplex RS-485 node or as an RS-422 node. When JP19 is fitted, the A and B pins will be terminated with 120Ω. If termination is not required, remove JP19. When JP40 is connected a pull-up resistor on the RxD pin of 10kΩ will be connected. This jumper should be connected when using the [[adi>ADM2587E|ADM2587E]] in half-duplex mode. The relevant jumper configurations are shown below. A list of jumper configurations for all the interfaces on //ez//LINX can be found [[resources/ |
\\ | \\ | ||
| ^ Full-Duplex | | ^ Full-Duplex | ||
Line 19: | Line 19: | ||
^ JP40 | N / A | Connected | ^ JP40 | N / A | Connected | ||
\\ | \\ | ||
- | The 3.3V supply is connected to VCC (pin 2 and 8) to power the // | + | The 3.3V supply is connected to VCC (pin 2 and 8) to power the // |
A six pin screw terminal connector, J7 is used for easy access to the A(Pin 2), B(Pin 3), Z(Pin 4), Y(Pin 5) and RS-485_ISO_GND(Pin 1 and 6) connections. | A six pin screw terminal connector, J7 is used for easy access to the A(Pin 2), B(Pin 3), Z(Pin 4), Y(Pin 5) and RS-485_ISO_GND(Pin 1 and 6) connections. | ||
- | Application note [[http:// | + | Application note [[adi>static/ |