Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision |
ezlinx:isolated-i2c [11 May 2012 10:49] – added return to homepage link Neil Quinn | resources:eval:ezlinx:isolated-i2c [31 Dec 2020 07:22] (current) – fix links Robin Getz |
---|
\\ | \\ |
[[http://wiki.analog.com/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Platform Homepage]] | [[resources/eval/ezlinx|ezLINX™ iCoupler® Isolated Interface Development Environment Homepage]] |
\\ | \\ |
====== ezLINX™ Isolated I2C Implementation====== | ====== ezLINX™ Isolated I2C Implementation====== |
| |
The Isolated I2C port is implemented using the [[http://www.analog.com/adum1250|ADuM1250]] I2C Isolator and [[http://www.analog.com/adum5000|ADuM5000]] //iso//Power Isolated DC to DC converter. The [[http://www.analog.com/adum1250|ADuM1250]] connects to TW1 of the ADSP-BF548 and is capable of functioning at a maximum frequency of 1MHz. Figure 1 below shows a circuit diagram of the implementation of the [[http://www.analog.com/adum1250|ADuM1250]] and [[http://www.analog.com/adum5000|ADuM5000]] on the //ez//LINX hardware. | The Isolated I2C port is implemented using the [[adi>ADuM1250]] I2C Isolator and [[adi>ADuM5000]] //iso//Power Isolated DC to DC converter. The [[adi>ADuM1250]] connects to TW1 of the ADSP-BF548 and is capable of functioning at a maximum frequency of 1MHz. Figure 1 below shows a circuit diagram of the implementation of the [[adi>ADuM1250]] and [[adi>ADuM5000]] on the //ez//LINX hardware. |
| |
| {{ :ezlinx:isolatedi2c.png?nolink&600 |Figure 1. Isolated I2C schematic}} |
| |
{{ :ezlinx:i2c.jpg?nolink&600 |Figure 1. Isolated I2C schematic}} | VDD1 of the [[adi>ADuM1250]] and VDD1 of the [[adi>ADuM5000]] are both powered by 3.3V. The ADuM5000 will generate an isolated 3.3V which is used to supply power to VDD2 of the [[adi>ADuM1250]]. |
| |
| |
VDD1 of the [[http://www.analog.com/adum1250|ADuM1250]] and VDD1 of the [[http://www.analog.com/adum5000|ADuM5000]] are both powered by 3.3V. The ADuM5000 will generate an isolated 3.3V which is used to supply power to VDD2 of the [[http://www.analog.com/adum1250|ADuM1250]]. | |
| |
A three pin screw terminal connector, J22, is used for easy access to the SDA (Pin 1), SCL (Pin 2) and I2C_ISO_GND (Pin 3) connections. | A three pin screw terminal connector, J22, is used for easy access to the SDA (Pin 1), SCL (Pin 2) and I2C_ISO_GND (Pin 3) connections. |