This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:eval-advts4152-ebz [07 Jul 2020 10:02] – ↷ Page name changed from resources:eval:eval-advts4152-e1z to resources:eval:eval-advts4152-ebz Celso Aron | resources:eval:eval-advts4152-ebz [05 Apr 2021 11:29] (current) – Ioana Chelaru | ||
---|---|---|---|
Line 35: | Line 35: | ||
- | The [[adi> EVAL-ADVTS4152-EBZ]] demonstration board is intended for systems that require a constant output voltage of 5V like in a Vehicle tracking system (VTS). It is run by a main battery source with a back-up battery in case of unwanted shortage of supply happens in the input. | + | The [[adi> |
Demo board features the three main parts that function as one to achieve the highest performance and reliability of the board. These parts are: | Demo board features the three main parts that function as one to achieve the highest performance and reliability of the board. These parts are: | ||
- | LT4356-1: a surge stopper that protects high voltage transients such as load dumps to electronic automotive loads, with wide range input capability of 4V to 80V and clamps to a desirable voltage output that suites will suite your design need. It also provides protection against reverse input and cold crank. | + | [[adi>LT4356-1]]: a surge stopper that protects high voltage transients such as load dumps to electronic automotive loads, with wide range input capability of 4V to 80V and clamps to a desirable voltage output that suites will suite your design need. It also provides protection against reverse input and cold crank. |
- | LT8609A: | + | [[adi> |
- | And, LTC4040: supply rail and backup battery that contains high current step-up DC/DC regulator that backup the supply from a single cell Li-Ion or LiFePO4 and help power the system when the main supply cuts off. | + | And, [[adi>LTC4040]]: supply rail and backup battery that contains high current step-up DC/DC regulator that backup the supply from a single cell Li-Ion or LiFePO4 and help power the system when the main supply cuts off. |
The demo board has an EMI filter installed for automotive standard requirement and optional ADT6401 circuit for over temp protection if the design needs to protect abnormal high DC Input. | The demo board has an EMI filter installed for automotive standard requirement and optional ADT6401 circuit for over temp protection if the design needs to protect abnormal high DC Input. | ||
Line 58: | Line 58: | ||
- | [[adi> EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. | + | [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. |
EVAL-ADVTS4152-EBZ Block Diagram | EVAL-ADVTS4152-EBZ Block Diagram | ||
Line 101: | Line 101: | ||
===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ||
- | Below set-ups are guide to test the [[adi> EVAL-ADVTS4152-EBZ]]. | + | Below set-ups are guide to test the [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]]. |
Follow diagram details and instruction to ensure proper set-up. | Follow diagram details and instruction to ensure proper set-up. | ||
Line 190: | Line 190: | ||
------------------------------------------------------------------------------------------------------------------- | ------------------------------------------------------------------------------------------------------------------- | ||
- | ==========EVAL-ADVTS4152-E1Z Voltage Output Ripple With Respect to Vinput and Vbackup ============ | ||
- | |||
- | Below tables are Voutput ripple result of the board. | ||
- | |||
- | Table 1. ADVTS4152 Vout ripple voltage (Vin =12, Vbackup=4.1) | ||
- | {{ : | ||
- | |||
- | |||
- | Table 2. ADVTS4152 Vout ripple voltage (Vin =16, Vbackup=4.1) | ||
- | {{ : | ||
- | |||
- | |||
- | Table 3. ADVTS4152 Vout ripple voltage (Vin =20, Vbackup=4.1) | ||
- | {{ : | ||
- | |||
- | |||
- | Table 4. ADVTS4152 Vout ripple voltage (Vin =24, Vbackup=4.1) | ||
- | {{ : | ||
- | |||
- | -------------------------------------------------------------------------------------------------------------------- | ||
- | |||
- | ====EVAL-ADVTS4152-EBZ Test Set-up Plot Results==== | ||
- | |||
- | EVAL-ADVTS4152-EBZ LOAD DUMP PLOT RESULT | ||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | EVAL-ADVTS4152-EBZ VBACK-UP PLOT RESULT | ||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | EVAL-ADVTS4152-EBZ OVERCURRENT PLOT RESULT | ||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | |||
- | EVAL-ADVTS4152-EBZ REVERSE POLARITY PLOT RESULT | ||
- | {{ : | ||
- | |||
- | |||
- | |||
- | |||
- | |||
- | -------------------------------------------------------------------------------------------------------------------- | ||
- | |||
- | |||
- | |||
===== Schematic, PCB Layout, Bill of Materials============== | ===== Schematic, PCB Layout, Bill of Materials============== | ||
[[http:// | [[http:// | ||
Line 259: | Line 196: | ||
| | ||
- | * [[Application Note Page]] | + | * Application Note Page |
-------------------------------------------------------------------------------------------------------------------- | -------------------------------------------------------------------------------------------------------------------- | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
- | | + | |
- | * [[ADI> | + | * [[ADI> |
- | * [[ADI> | + | * [[ADI> |
* [[ADI> | * [[ADI> | ||
- | * [[ADI>|ADT6401|ADT6401 Product Page]] | + | * [[ADI> |
+ | |||
//End of Document// | //End of Document// | ||