This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:eval-advts4152-e1z [26 Jun 2020 09:07] – Celso Aron | resources:eval:eval-advts4152-ebz [05 Apr 2021 11:29] (current) – Ioana Chelaru | ||
---|---|---|---|
Line 35: | Line 35: | ||
- | The [[adi> EVAL-ADVTS4152-EBZ]] demonstration board is intended for systems that require a constant output voltage of 5V like in a Vehicle tracking system (VTS). It is run by a main battery source with a back-up battery in case of unwanted shortage of supply happens in the input. | + | The [[adi> |
Demo board features the three main parts that function as one to achieve the highest performance and reliability of the board. These parts are: | Demo board features the three main parts that function as one to achieve the highest performance and reliability of the board. These parts are: | ||
- | LT4356-1: a surge stopper that protects high voltage transients such as load dumps to electronic automotive loads, with wide range input capability of 4V to 80V and clamps to a desirable voltage output that suites will suite your design need. It also provides protection against reverse input and cold crank. | + | [[adi>LT4356-1]]: a surge stopper that protects high voltage transients such as load dumps to electronic automotive loads, with wide range input capability of 4V to 80V and clamps to a desirable voltage output that suites will suite your design need. It also provides protection against reverse input and cold crank. |
- | LT8609A: | + | [[adi> |
- | And, LTC4040: supply rail and backup battery that contains high current step-up DC/DC regulator that backup the supply from a single cell Li-Ion or LiFePO4 and help power the system when the main supply cuts off. | + | And, [[adi>LTC4040]]: supply rail and backup battery that contains high current step-up DC/DC regulator that backup the supply from a single cell Li-Ion or LiFePO4 and help power the system when the main supply cuts off. |
The demo board has an EMI filter installed for automotive standard requirement and optional ADT6401 circuit for over temp protection if the design needs to protect abnormal high DC Input. | The demo board has an EMI filter installed for automotive standard requirement and optional ADT6401 circuit for over temp protection if the design needs to protect abnormal high DC Input. | ||
Line 58: | Line 58: | ||
- | [[adi> EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. | + | [[adi>EVAL-ADVTS4152|EVAL-ADVTS4152-EBZ]] is consist of three major sections. These are the Fault Protection and Surge Stopper, Step-Down Regulator, Back-Up Supply. These three blocks work together to provide reliable and efficient power to the downstream electronics like VTS. It can operate across a wide range of input voltage of 80V DC and surge voltage of up to 210V. |
EVAL-ADVTS4152-EBZ Block Diagram | EVAL-ADVTS4152-EBZ Block Diagram | ||
Line 68: | Line 68: | ||
{{ : | {{ : | ||
- | | + | |
| | ||
| | ||
Line 77: | Line 77: | ||
{{ : | {{ : | ||
- | | + | |
| | ||
Section 3: This section function as a back-up supply or battery back-up power manager in the board. Mainly catered by the LTC4040 IC – a high-current step-up DC-to-DC regulator to back up the supply from a single-cell Lithium Ion or Lithium-Iron-Phosphate battery. | Section 3: This section function as a back-up supply or battery back-up power manager in the board. Mainly catered by the LTC4040 IC – a high-current step-up DC-to-DC regulator to back up the supply from a single-cell Lithium Ion or Lithium-Iron-Phosphate battery. | ||
Line 85: | Line 85: | ||
{{ : | {{ : | ||
- | | + | |
| | ||
-------------------------------------------------------------------------------------------------------------------- | -------------------------------------------------------------------------------------------------------------------- | ||
Line 101: | Line 101: | ||
===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ===== EVAL-ADVTS4152-EBZ Test Set-up Guide========= | ||
- | Below set-ups are guide set-up in order to test the [[adi> EVAL-ADVTS4152-E1Z]]. | + | Below set-ups are guide to test the [[adi> |
+ | Follow diagram details and instruction to ensure proper set-up. | ||
EVAL-ADVTS4152-EBZ LOAD DUMP TEST SET-UP | EVAL-ADVTS4152-EBZ LOAD DUMP TEST SET-UP | ||
{{ : | {{ : | ||
+ | LOAD DUMP TEST SET-UP | ||
- | EVAL-ADVTS4152-EBZ BACK-UP BATTERY TEST SET-UP | + | 1) Connect low voltage power supply (12V or 24V) to the load dump generator input |
- | {{ : | + | |
- | EVAL-ADVTS4152-EBZ BACK-UP OVERCURRENT TEST SET-UP | + | 2) Connect the high voltage power supply to the triggering input of the load dump generator. |
- | {{ : | + | |
- | EVAL-ADVTS4152-EBZ BACK-UP REVERSE POLARITY TEST SET-UP | + | 3) Connec the output of the load dump generator to the ADVT4152 main input (as shown in the diagram). |
- | {{ : | + | |
- | ------------------------------------------------------------------------------------------------------------------- | + | 4) Connect also the 1A DC electronic load constant current |
- | ===EVAL-ADVTS4152-E1Z Voltage Output Ripple With Respect to Vinput and Vbackup=== | + | 5) Have those voltage input monitor using oscilloscope as indicated above. |
- | Below tables are Voutput ripple result of the board. | + | Oscilloscope Setting: all probe at 200ms time interval. |
+ | |||
+ | Ch1 - set it to 5V/ | ||
- | Table 1. ADVTS4152 Vout ripple voltage (Vin =12, Vbackup=4.1) | + | Ch2 - set it to 10V/Div |
- | {{ : | + | |
+ | Ch3 - set it to 20V/Div | ||
- | Table 2. ADVTS4152 | + | ------------------------------------------------------- |
- | {{ : | + | EVAL-ADVTS4152-EBZ BACK-UP BATTERY TEST SET-UP |
+ | {{ : | ||
+ | 1) Connect low voltage power supply (12V or 24V) or a car battery with the same input voltage to the main input supply. | ||
- | Table 3. ADVTS4152 | + | 2) Connect Li-Ion or LiFePO4 to the battery input located in the below part of the ADVTS4152 |
- | {{ : | + | |
+ | 3) Connect also the 1A DC electronic load constant current at the output of ADVTS4152 or after the LED indicator. | ||
- | Table 4. ADVTS4152 Vout ripple | + | 4) Have those voltage |
- | {{ : | + | |
- | -------------------------------------------------------------------------------------------------------------------- | ||
- | ====EVAL-ADVTS4152-EBZ Test Set-up Plot Results==== | + | Oscilloscope Setting: all probe at 200ms time interval. |
+ | |||
+ | | ||
+ | |||
+ | Ch2 - Back-up Battery Input- set it to 5V/Div | ||
- | EVAL-ADVTS4152-EBZ LOAD DUMP PLOT RESULT | + | |
- | {{ : | + | |
+ | --------------------------------------------------------- | ||
+ | EVAL-ADVTS4152-EBZ BACK-UP OVERCURRENT TEST SET-UP | ||
+ | {{ : | ||
+ | 1) Connect low voltage power supply (12V or 24V) or a car battery with the same input voltage to the main input supply. | ||
+ | 2) Connect Li-Ion or LiPeO4 to the battery input located in the below part of the ADVTS4152 board as shown in the diagram above. | ||
+ | 3) Connect a 1A DC electronic load constant resistance at the output of ADVTS4152 or after the LED indicator. | ||
+ | 4) Connect an Ammeter at the ADVTS4152 output. | ||
+ | 5) Have those voltage input monitor by follow the probe connections in above diagram. | ||
+ | Oscilloscope Setting: all probe at 200ms time interval. | ||
+ | |||
+ | Ch1 - Main Input - set it to 1A/ | ||
- | EVAL-ADVTS4152-EBZ VBACK-UP PLOT RESULT | + | |
- | {{ : | + | |
+ | --------------------------------------------------------- | ||
+ | EVAL-ADVTS4152-EBZ BACK-UP REVERSE POLARITY TEST SET-UP | ||
+ | {{ : | ||
+ | 1) Connect low voltage power supply (12V or 24V) or a car battery positive terminal to the negative port of the ADVTS4152 main input and the negative terminal to the positive port. | ||
+ | 2) Connect Li-Ion or LiPeO4 to the battery input located in the below part of the ADVTS4152 board as shown in the diagram above. | ||
+ | 3) Connect a 1A DC electronic load constant current at the output of ADVTS4152 or after the LED indicator. | ||
+ | 4) Connect an Ammeter at the ADVTS4152 output. | ||
- | EVAL-ADVTS4152-EBZ OVERCURRENT PLOT RESULT | + | 4) Have those voltage input monitor by follow the probe connections in above diagram. |
- | {{ : | + | |
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | EVAL-ADVTS4152-EBZ REVERSE POLARITY PLOT RESULT | + | |
- | {{ : | + | |
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | + | ||
- | -------------------------------------------------------------------------------------------------------------------- | + | |
+ | Oscilloscope Setting: all probe at 200ms time interval. | ||
+ | |||
+ | Ch1 - Main Input - set it to 5V/ | ||
+ | Ch2 - ADVTS4152 output- set it to 5V/Div | ||
+ | |||
+ | ------------------------------------------------------------------------------------------------------------------- | ||
===== Schematic, PCB Layout, Bill of Materials============== | ===== Schematic, PCB Layout, Bill of Materials============== | ||
[[http:// | [[http:// | ||
Line 186: | Line 196: | ||
| | ||
- | * [[Application Note Page]] | + | * Application Note Page |
-------------------------------------------------------------------------------------------------------------------- | -------------------------------------------------------------------------------------------------------------------- | ||
===== More Information and Useful Links ===== | ===== More Information and Useful Links ===== | ||
- | [[adi> | + | EVAL-ADVTS4152-EBZ Other Important Files |
- | * Resource Description | + | |
- | * LT4356-1/ | + | * [[ADI> |
- | * LT8609/ | + | * [[ADI> |
- | * LTC4040 2.5A Battery Backup Power Manager | + | * [[ADI>LTC4040|LTC4040 Product Page]] |
+ | * [[ADI> | ||
+ | |||