This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:eval-ad7175-2sdz [25 Nov 2014 17:32] – [FEATURES] Rob Kiely | resources:eval:eval-ad7175-2sdz [06 Feb 2021 20:30] (current) – fix link Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== Evaluating the AD7175-2 24-Bit, 250 kSPS, Sigma-Delta ADC ====== | ||
+ | ===== Features ===== | ||
+ | * Full featured evaluation board for the [[adi> | ||
+ | * PC control in conjunction with the Analog Devices, Inc., [[adi> | ||
+ | * PC software for control and data analysis (time domain) | ||
+ | * Standalone capability | ||
+ | |||
+ | ===== Evaluation Kit Contents ===== | ||
+ | * [[adi> | ||
+ | * Evaluation software CD | ||
+ | * 7 V to 9 V ac-to-dc adapter | ||
+ | |||
+ | ===== Equipment Needed ==== | ||
+ | * DC signal source | ||
+ | * PC running Windows XP to Windows 7 | ||
+ | |||
+ | |||
+ | ===== General Description ===== | ||
+ | The [[adi> | ||
+ | |||
+ | The [[adi> | ||
+ | Full specifications for the [[adi> | ||
+ | |||
+ | ===== Functional Block Diagram ===== | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //** Figure 1. Functional Block Diagram **// | ||
+ | |||
+ | ====== EVAL-AD7175-2SDZ Quick Start Guide ====== | ||
+ | |||
+ | ===== Recommended Quick Start Guide ===== | ||
+ | Follow these steps to set up the evaluation board: | ||
+ | - Disconnect the SDP-B board from the USB port of the PC. Install the [[adi> | ||
+ | - Connect the SDP-B board to the evaluation board, as shown in Figure 2. | ||
+ | - Fasten the two boards together with the enclosed plastic screw washer set. | ||
+ | - Connect the external 9 V power supply to Connector J5 of the evaluation board as shown in Figure 2. Set Link LK2 to Position B. | ||
+ | - Connect the SDP-B board to the PC via the USB cable. For Windows® XP, you may need to search for the SDP-B drivers. Choose to automatically search for the drivers for the SDP-B board if prompted by the operating system. | ||
+ | - Launch the [[adi> | ||
+ | |||
+ | |||
+ | ===== Quick Start Noise Test ===== | ||
+ | - Insert Link LK8 to Link LK12 to initiate the noise performance test mode. In this mode, analog input channels short to the REFOUT pin. | ||
+ | - Click Start Sampling to acquire samples from the ADC (see Figure 7). | ||
+ | |||
+ | The Samples numeric control in the top right corner of the main window sets the number of samples collected in each batch (see Figure 7). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 2. Hardware Configuration, | ||
+ | |||
+ | ====== Evaluation Board Hardware ====== | ||
+ | ===== Device Description ===== | ||
+ | |||
+ | The [[adi> | ||
+ | See the [[adi> | ||
+ | |||
+ | ===== Hardware Link Options ===== | ||
+ | See Table 1 for default link options. By default, the evaluation board is configured to operate from the supplied 9 V ac-to-dc adapter connected to connector J5. The 5 V supply required for the [[adi> | ||
+ | |||
+ | **Table 1. Default Link and Solder Link Options** | ||
+ | |||
+ | |< 100% 15% 15% 70% >| | ||
+ | ^ Link ^ Default Option | ||
+ | | LK1 | A | Selects the voltage applied to the power supply sequencer circuit (U3); dependent on AVDD1. Place in Position A if using 5 V AVDD1, or Position B if using 2.5 V AVDD1. | | ||
+ | | LK2 | B | Selects the external power supply from Connector J3 (Position A) or Connector J5 (Position B). | | ||
+ | | LK3 to LK7 | Not Inserted | Inserting these links sets up the on-board noise test prior to SL8 to SL11 to allow the inputs to the on board amplifiers, U8 and U9, to be shorted. In this mode, all inputs short to REFOUT. | | ||
+ | | LK8 to LK12 | Inserted | Inserting these links sets up the on-board noise test close to the ADC analog inputs. In this mode, all inputs short to REFOUT. | | ||
+ | | SL1 | A | Sets the voltage applied to the AVDD2 pin. Operates using the AVDD1 supply (default). Position B sets the AVDD2 voltage to 3.3 V supply from the ADP7118 (3.3 V) (U10) regulator. | | ||
+ | | SL2 | A | Selects between an external or on-board AVDD1 source. Supplies AVDD1 from the ADP7118 (5 V) (U7) (default). | | ||
+ | | SL3 | A | Selects between an external or on-board AVSS source. Supplies AVSS from the ADP7182 (−2.5 V) (U4) (default).| | ||
+ | | SL4 | A | Connects AIN4 to: A4/J6 (Position A), REFOUT pin on the [[adi> | ||
+ | | SL5 | B | Selects between an external or on-board IOVDD source. Supplies IOVDD from theADP7118 (3.3 V) (U10) (default). The evaluation board operates with a 3.3 V logic.| | ||
+ | | SL8 | A | Routes A0 to: AIN0 pin on the [[adi> | ||
+ | | SL9 | A | Routes A2 to: AIN2 pin on the [[adi> | ||
+ | | SL10 | A | Routes A3 to: AIN3 pin on the [[adi> | ||
+ | | SL11 | A | Routes A1 to: AIN1 pin on the [[adi> | ||
+ | | G16 | Inserted | Sets the on board In-amp U8 to a gain of 16. Only one of G16, G32, G64 and G128 should be inserted at a time. | | ||
+ | | G32 | Not Inserted | Sets the on board In-amp U8 to a gain of 32. Only one of G16, G32, G64 and G128 should be inserted at a time.| | ||
+ | | G64 | Not Inserted | Sets the on board In-amp U8 to a gain of 64. Only one of G16, G32, G64 and G128 should be inserted at a time. | | ||
+ | | G128 | Not Inserted | Sets the on board In-amp U8 to a gain of 128. Only one of G16, G32, G64 and G128 should be inserted at a time. | | ||
+ | | R49 to R51 | Inserted | Connects AVSS and AGND for single-supply operation. To operate in split supply mode, remove these links.| | ||
+ | |||
+ | ===== Sockets And Connectors ===== | ||
+ | **Table 2. Connector Details** | ||
+ | |||
+ | |< 100% 10% 30% 15%% 15% 15% 15%>| | ||
+ | ^ Connector | ||
+ | | J1 | Connector to the EVAL-SDP-CB1Z | 120-way connector, 0.6 mm pitch | Hirose | FX8-120S-SV(21) | FEC1324660((Order codes starting with FEC are for Farnell)) | | ||
+ | | J2 | External MCLK Input | Straight PCB mount SMB/SMA jack |Tyco | 1-1337482-0 | Not applicable | | ||
+ | | J3 | External bench top voltage supply for the [[adi> | ||
+ | | J5 | External ac-to-dc adapter input for the [[adi> | ||
+ | | J6 | Analog input terminal block; wired connection to external source or sensor | Power socket block, 8-pin, 3.81 mm pitch | Phoenix Contact | MC 1,5/ 8-G-3,81 | FEC3704774 | | ||
+ | | J9 | External bench top voltage supply option for AVDD1/ | ||
+ | | J10 | Optional header | 7-way, 2.54 mm pin header | Samtec | SSW-107-01-T-S | FEC1803478 | | ||
+ | | J13 | Optional header | 7-way, 2.54 mm socket | Samtec | TLW-107-05-G-S | FEC1668499 | | ||
+ | | A0 to A4 | Analog inputs to ADC | Straight PCB mount SMB/SMA jack | Tyco | 1-1337482-0 | Not applicable | | ||
+ | | A7 | PMOD-compatible header | 6-Pin SIL header (0.1" pitch) | Harwin | 20-9990646 | FEC 1022255 | | ||
+ | |||
+ | ===== Serial Interface ===== | ||
+ | The [[adi> | ||
+ | |||
+ | ===== Power Supplies ===== | ||
+ | Power the evaluation board from the ac-to-dc adapter connected to J5, or from an external bench top supply applied to J3 or J9. Linear LDOs generate the required voltages from the applied input voltage (VIN) rail when using J3 or J5. Use J9 to bypass the on-board regulators. An ADP7118 regulator generates the 5 V (single supply) and 2.5 V (split supply) supplies for the AVDD1 and AVDD2 rails to the ADC; a second ADP7118 generates 3.3 V for the IOVDD rail. The ADP7104 supplies 5 V for the SDP-B controller board as well as 5 V for the ADM660 voltage converter to generate −5 V to supply the ADP7182. The ADP7182 generates the −2.5 V supply for AVSS when operating in split supply mode. Each supply is decoupled where it enters the board and again at each device in accordance with the schematic. Table 3 shows the various power supply configurations available, including split supply operation. | ||
+ | |||
+ | **Table 3. Power Supply Configurations** ((Only one configuration can be used at a time)) | ||
+ | |< 100% 15% 15% 70% >| | ||
+ | ^ Configuration ^ Input Voltage Range ^ Description ^ | ||
+ | | Single Supply (Regulated) | 7 V to 9 V |The 7 V to 9 V input is regulated to 5 V for AVDD1/AVDD2 and 3.3 V for IOVDD. This also powers the external 5 V reference. See the Single Supply (Regulated) section in the Power Supply Configurations section. | | ||
+ | | Single Supply (Unregulated) | 7 V to 9 V, 5 V, and 3.3 V |The input is unregulated and connects directly to AVDD1/AVDD2 and IOVDD from J5. The 7 V to 9 V input powers the external 5 V reference. See the Single Supply (Unregulated) section in the Power Supply Configurations section. | | ||
+ | | Split Supply (Regulated) | 7 V to 9 V | The 7 V to 9 V input is regulated to 2.5 V for AVDD1/ | ||
+ | | Split Supply (Unregulated) | 7 V to 9 V, ±2.5 V, and 3.3 V | The input is unregulated and connects directly to AVDD1/AVDD2 and IOVDD from J5. The 7 V to 9 V input powers the external 5 V reference. See the Split Supply (Unregulated) section in the Power Supply Configurations section. | | ||
+ | |||
+ | ===== Power Supply Configurations ===== | ||
+ | === Single Supply (Regulated) === | ||
+ | There are two available power supply options for the single supply (regulated) configuration. | ||
+ | * An ac-to-dc adapter (included) connected to J5. Set LK2 to Position B. | ||
+ | * A bench top power supply connected to J3. Set LK2 to Position A, and ensure that AVSS = AGND = 0 V. | ||
+ | |||
+ | Set all other links and solder links to the default settings as outlined in Table 1. | ||
+ | |||
+ | === Single Supply (Unregulated) === | ||
+ | To set up the evaluation board, use the following procedure: | ||
+ | - Move SL2 to position B and SL5 to position A. | ||
+ | - Connect the two terminals of J9 labeled AGND and AVSS. | ||
+ | - Connect 0 V (GND) to J9 at the terminal labeled AGND. | ||
+ | - Connect 5 V to J9 at the terminal labeled AVDD. | ||
+ | - Connect 3.3 V to J9 at the terminal labeled IOVDD. | ||
+ | - Connect the 7 V to 9 V input to J5. | ||
+ | |||
+ | Set all other links and solder links to the default settings as outlined in Table 1. | ||
+ | |||
+ | === Split Supply (Regulated) === | ||
+ | To set up the evaluation board, use the following procedure: | ||
+ | - Remove R49 to R51. These links connect AVSS to AGND. | ||
+ | - Insert a 0 Ω resistor for R85. | ||
+ | - Set LK1 to Position B, which sets the input to the power monitor circuitry to work with the lower AVDD1 supply of 2.5 V. | ||
+ | - Connect a bench top power supply to J5 and set LK2 to Position B. | ||
+ | |||
+ | Set all other links and solder links to the default settings as outlined in Table 1. | ||
+ | |||
+ | === Split Supply (Unregulated) === | ||
+ | |||
+ | To set up the evaluation board, use the following procedure: | ||
+ | - Move SL2, SL3 to position B and SL5 to position A. | ||
+ | - Remove R49 to R51. | ||
+ | - Connect 0 V (GND) to J9 at the terminal labeled AGND. | ||
+ | - Connect 2.5 V to J9 at the terminal labeled AVDD. | ||
+ | - Connect −2.5 V to J9 at the terminal labeled AVSS. | ||
+ | - Connect 3.3 V to J9 at the terminal labeled IOVDD. | ||
+ | - Connect 7 V to 9 V to J5. | ||
+ | - Set LK1 to Position B. This sets the input to the power monitor circuitry to work with the lower AVDD1 supply of 2.5 V. | ||
+ | |||
+ | Set all other links and solder links set to the default settings as outlined in Table 1. | ||
+ | |||
+ | ===== Analog Inputs ===== | ||
+ | |||
+ | The primary analog inputs of the [[adi> | ||
+ | * J6 connector on the left side of the board | ||
+ | * A0 to A4 SMB/SMA footprints on the evaluation board | ||
+ | |||
+ | The analog inputs route directly to the associated analog input pins on the [[adi> | ||
+ | |||
+ | ===== Reference Options ===== | ||
+ | The [[adi> | ||
+ | |||
+ | ====== Evaluation Board Software ====== | ||
+ | |||
+ | ===== software Installation ===== | ||
+ | |||
+ | The [[adi> | ||
+ | |||
+ | Install the Eval+ software before connecting the evaluation board and EVAL-SDP-CB1Z board to the USB port of the PC to ensure that the evaluation system is correctly recognized when connected to the PC. | ||
+ | |||
+ | There are two parts to the installation. | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | Place the software and drivers in the appropriate locations by proceeding through all of the installation steps. Connect the EVAL-SDP-CB1Z board to the PC only after the software and drivers install. The installer may prompt you to allow the program to make changes to the computer. Click Yes to proceed (see Figure 3). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 3. AD7175-2 User Account Control Permission Dialog Box**// | ||
+ | |||
+ | You may receive a security warning as part of the SDP-B controller board driver installation. Click **Install** to proceed with the installation of the driver (see Figure 4). Without this confirmation, | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 4. [[adi> | ||
+ | |||
+ | After installation is complete, connect the evaluation board to the SDP-B board as shown in Figure 2. Connect the evaluation board via the USB cable to the computer. Follow these steps to verify that the SDP-B controller board driver is installed and working correctly: | ||
+ | - Allow the **Found New Hardware Wizard** to run. | ||
+ | - When the drivers are installed, check that the board has connected correctly by looking at the **Device Manager** of the PC. The **Device Manager** can be found by right clicking **My Computer**, selecting **Manage**, then **Device Manager** from the list of **System Tools** (see Figure 5). | ||
+ | - The [[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 5. Device Manager**// | ||
+ | |||
+ | ===== Launching the Software ===== | ||
+ | The Eval+ software can be launched when the evaluation board and SDP-B board are correctly connected to the PC. The Eval+ software can also be operated without hardware. | ||
+ | |||
+ | To launch the software, complete the following steps: | ||
+ | - From the **Start** menu, click **Programs**, | ||
+ | - If the [[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 6. Select Interface Dialog Box**// | ||
+ | |||
+ | ====== Software Operation ====== | ||
+ | |||
+ | ===== Overview of the Main Window ===== | ||
+ | |||
+ | The main window of the evaluation software displays the significant control buttons and analysis indicators of the [[adi> | ||
+ | |||
+ | ===== Configuration Tab (1) ===== | ||
+ | === Evaluation Mode(2) === | ||
+ | |||
+ | Click here to select the evaluation mode. Selecting **Hardware** evaluation mode uses the [[adi> | ||
+ | === ADC Reset (3) === | ||
+ | Click **ADC Reset** to perform a software reset of the [[adi> | ||
+ | === Ext. REF (4) === | ||
+ | The **Ext. REF** field sets the external reference voltage used for calculating the results on the waveform and histogram tabs. The evaluation board has an external 5 V [[adi> | ||
+ | === Functional Block Diagram (5) === | ||
+ | The functional block diagram of the ADC shows each of the separate functional blocks within the ADC. Clicking a configuration button on this graph opens the configuration popup window for that block. Not all blocks have a configuration button. | ||
+ | === Configuration Popup Button (6) === | ||
+ | Each configuration popup button opens a different window allowing for configuration of the relevant functional block. | ||
+ | === Channel Configuration Overview (7) === | ||
+ | This section shows the channel configuration, | ||
+ | === Status Bar (8) === | ||
+ | The status bar displays status updates such as **Analysis Completed** and **Reset Completed** during software use, as well as the software version and busy indicator. | ||
+ | === Analog Supply Voltage (9 & 13) === | ||
+ | Sets the analog supply voltages used in the functional model for checking power supply limits and calculating the power dissipation figures. These controls are only visible when Functional Model evaluation mode is enabled. | ||
+ | === Digital Supply Voltage (10) === | ||
+ | Sets the digital supply voltage used in the functional model for checking power supply limits and calculating the power dissipation figures. This control is only visible when Functional Model evaluation mode is enabled. | ||
+ | === Analog Input Voltage (11) === | ||
+ | Sets the analog input voltages used in the functional model for calculating the ADC output codes. Note: The voltages set on these controls are DC only voltage with no noise. These controls are only visible when Functional Model evaluation mode is enabled. | ||
+ | === External SCLK Frequency (12) === | ||
+ | Sets the external SCLK frequency for the SPI interface. This value is used in the functional model to determine if they SCLK frequency is within the permitted range. This control is only visible when Functional Model evaluation mode is enabled. | ||
+ | === External MCLK Frequency (14) === | ||
+ | Set the external MCLK frequency | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 7. **Configuration** Tab of the [[adi> | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 8. **Configuration** Tab of the [[adi> | ||
+ | |||
+ | |||
+ | ===== Waveform Tab (15) ===== | ||
+ | === Analysis Channel (16) === | ||
+ | The **Noise Analysis** section and histogram graph show the analysis of the channel selected via the **Analysis Channel** control. | ||
+ | === Samples (17 and 18) === | ||
+ | The **Samples** (17) numeric control and batch control (18) set the number of samples gathered per batch and whether a single batch or multiple batches of samples are gathered. This control is unrelated to the ADC mode. You can capture a defined sample set or continuously gather batches of samples. In both cases, the number of samples set in the **Samples** (17) numeric input dictates the number of samples. | ||
+ | === Sample (19) === | ||
+ | Click the **Sample** button to start gathering ADC results. Results appear in the waveform graph (20). | ||
+ | === Waveform Graph and Controls (20 and 21) === | ||
+ | The data waveform shows each successive sample of the ADC output. Zoom in on the data using the control toolbar (21) in the graph. Change the scales on the graph by typing values into the x-axis and y-axis. | ||
+ | === Channel Selection (22) === | ||
+ | This control chooses which channels display on the data waveform, and also shows the analog inputs for the channel labeled next to the on and off controls. These controls only affect the display of the channels and have no effect on the channel settings in the ADC register map. | ||
+ | === Display Units and Axis Controls (23) === | ||
+ | Click **Display Units** to select whether the data graph displays in units of voltages or codes. This control affects both the waveform graph and the histogram graph. The axis controls can be switched between dynamic and fixed. When dynamic is selected, the axis automatically adjusts to show the entire range of the ADC results after each batch of sample. When fixed is selected, the user can program the axis ranges; the axis ranges do not automatically adjust after each batch of sample. | ||
+ | === CRC Error (24) === | ||
+ | This LED indicator illuminates when a cyclic redundancy check (CRC) error is detected in the communications between the software and the [[adi> | ||
+ | === Noise Analysis (25) === | ||
+ | The **Noise Analysis** section displays the results of the noise analysis for the selected analysis channel, which includes both noise and resolution measurements. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 9. Waveform Tab of the [[adi> | ||
+ | |||
+ | ===== Histogram Tab (26)===== | ||
+ | === Histogram Graph and Controls (27 and 28) === | ||
+ | The data histogram shows the number of times each sample of the ADC output occurs. Zoom in on the data using the control toolbar (28) in the graph. Change the scales on the graph by typing values into the x-axis and y-axis. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 10. Histogram Tab of the [[adi> | ||
+ | |||
+ | ===== Calculated Performance Tab (29) ===== | ||
+ | The Calculated Performance tab shows a number of ADC performance parameters which are calculated using the ADC functional model. All results in the tab are for the current analysis channel (16). | ||
+ | === Filter Profile & Response (30 & 31) === | ||
+ | Shows a frequency response graph for the selected digital filter the rejection / attenuation of the digital filter over the Rej BW for f1 and f2 in dB. | ||
+ | === Performance Summary (32) === | ||
+ | Shows the total power consumption of the part in the current configuration as well as the current consumption on each of the power supply rails. Also shows timing information about the currently selected output data rate (Tsettle, Fnotch, fADC). | ||
+ | === Timing Diagram (33) === | ||
+ | This graph shows the digital interface timing diagram for the current configuration. It shows the timing for both the configuration of the ADC and the subsequent data reads from the ADC. | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 11. Calculated Performance Tab of the [[adi> | ||
+ | |||
+ | | ||
+ | ===== Register Map Tab (34) ===== | ||
+ | === Register Tree (35) === | ||
+ | This control shows the full register map in a tree control. Each register is shown; clicking on the expand button next to each register shows all the bit fields contained within that register. | ||
+ | === Register Control (36) === | ||
+ | This control allows the user to change the individual bit of the register selected in the register tree (35) by clicking on the bits or by programming the register value directly into the number control field on the right. | ||
+ | === Bit Field List (37) === | ||
+ | This list shown all the bit fields of the register selected in the register tree (35). Change the values by using the drop-down box or by directly entering a value into the number control field on the right. | ||
+ | === Documentation (38) === | ||
+ | This field contains the documentation for the register of the bit field selected in the register tree (35). | ||
+ | === Save and Load (39 and 41) === | ||
+ | The Save and Load buttons allow the user to save the current register map setting to a file and to load the setting from the same file. | ||
+ | |||
+ | ===== Exiting the Software ===== | ||
+ | To exit the software, click the close button at the top right corner of the main window (see Figure 7). | ||
+ | |||
+ | {{ : | ||
+ | |||
+ | //**Figure 12. Register Map Tab of the [[adi> |