Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:dpg:eval-ad9789 [23 May 2018 16:37] – added note about DPG2 being obsolete Arik Landsman | resources:eval:dpg:eval-ad9789 [23 May 2018 22:39] – corrected language in "NOTE" Arik Landsman |
---|
Download the [[ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/HSDAC_Update/HSDACUpdate_AD9789_1.0.4686.26799.exe|AD9789 Update]] | Download the [[ftp://ftp.analog.com/pub/HSSP_SW/HSCDAC/HSDAC_Update/HSDACUpdate_AD9789_1.0.4686.26799.exe|AD9789 Update]] |
| |
**Please NOTE:** //The DPG2 Data Pattern Generator platform was recently made obsolete. It is required to properly power-up the AD9789 EVB, so we are working to add AD9789 support to the SDP-H1 platform instead. In the interim, the remaining stocked DPG2 units can be made available to customers while supplies last - for inquiries, please contact ADI's Central Applications or your local FAE. Our deepest apologies for any inconvenience during this transition! // | **Please NOTE:** //The DPG2 Data Pattern Generator platform is nearing its end-of-life and is not recommended for new designs with the AD9789. However, the DPG2 is required to properly power-up the AD9789 EVB - we are aware of this issue and are actively working on a resolution. In the interim, the remaining stocked DPG2 units are available for purchase while supplies last - for inquiries, please contact ADI's Central Applications or your local sales/distributor. Our deepest apologies for any inconvenience during this transition! // |
| |
{{section>resources:eval:dpg#Data Pattern Generator&nofooter&noindent}} | {{section>resources:eval:dpg#Data Pattern Generator&nofooter&noindent}} |