This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:dpg:eval-ad973x [14 Sep 2021 07:21] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlale | resources:eval:dpg:eval-ad973x [28 Sep 2021 08:20] – Update to SDPH1 and ADSV7 Melissa Lorenz Lacanlale | ||
---|---|---|---|
Line 49: | Line 49: | ||
=====Quick Start Guide===== | =====Quick Start Guide===== | ||
- | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J2 to a signal/ | + | - Attach the evaluation board to the FMC connector of SDP-H1 or ADS7-V2 using the AD-DAC-FMC-ADP adapter board. Connect continuous wave generator for clock input to J1, and the DAC output from J2 to a signal/ |
* If using **SDP-H1**, | * If using **SDP-H1**, | ||
* If using **ADS7-V2**, | * If using **ADS7-V2**, | ||
- Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9736 evaluation board. Apply the configuration wizard settings shown in Figure 2. <WRAP centeralign> | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9736 evaluation board. Apply the configuration wizard settings shown in Figure 2. <WRAP centeralign> | ||
- | - Start DPG Lite or DPG Downloader. At the SDP-H1 or ADS7-V2 | + | - Start DPG Lite or DPG Downloader. At the SDP-H1 or ADS7-V2 |
- In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b.Set **Data Rate** to 500 MHz and **Desired Frequency** to 50 MHz. | - In DPG Lite or DPG Downloader, from the **Add Generator Waveforms** pulldown menu, select **Single Tone** and apply the settings as shown in Figures 3a and 3b.Set **Data Rate** to 500 MHz and **Desired Frequency** to 50 MHz. | ||
- Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 14 bits.\\ <WRAP centeralign> | - Continuing on setting up DPG Lite or DPG Downloader, set **DAC resolution** to 14 bits.\\ <WRAP centeralign> |