Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision |
resources:eval:dpg:eval-ad9122 [26 Aug 2013 15:03] – [AD9122 Evaluation Board] Yi Zhang | resources:eval:dpg:eval-ad9122 [13 Sep 2013 17:49] – [AD9121/AD9122 Evaluation Board] Michael Fowler |
---|
| |
======AD9121/AD9122 Evaluation Board====== | ======AD9121/AD9122 Evaluation Board====== |
| |
Note: All of the below information also refers to the AD9121. | <WRAP center round info 40%> |
| <fs medium>All of the below information also refers to the AD9121</fs> |
| </WRAP> |
| |
In addition to the [[adi>AD9122]], the evaluation boards also come with clocking and analog quadrature modulator circuits to ease system level solutions. The AD9122 evaluation board comes in two models; the AD9122-M5372-EBZ has the ADL5372 modulator on board, and the AD9122-M5375-EBZ has the ADL5375 modulator on-board. To operate the evaluation boards, the user must apply power, a clock source, a digital data source, and be able to observe the DAC output on either a spectrum analyzer or an oscilloscope. A low jitter sine or square wave clock will work well as a source. The evaluation board comes with software which allows the user to program the SPI port. Via the SPI port, the DUT and clock circuitry can be programmed into any of its various operating modes. | In addition to the [[adi>AD9122]], the evaluation boards also come with clocking and analog quadrature modulator circuits to ease system level solutions. The AD9122 evaluation board comes in two models; the AD9122-M5372-EBZ has the ADL5372 modulator on board, and the AD9122-M5375-EBZ has the ADL5375 modulator on-board. To operate the evaluation boards, the user must apply power, a clock source, a digital data source, and be able to observe the DAC output on either a spectrum analyzer or an oscilloscope. A low jitter sine or square wave clock will work well as a source. The evaluation board comes with software which allows the user to program the SPI port. Via the SPI port, the DUT and clock circuitry can be programmed into any of its various operating modes. |