This shows you the differences between two versions of the page.
Last revisionBoth sides next revision | |||
resources:eval:dpg:debugging [25 May 2012 18:07] – created Michael Fowler | resources:eval:dpg:debugging [25 May 2012 21:12] – [Restart Evaluation Board service] Michael Fowler | ||
---|---|---|---|
Line 4: | Line 4: | ||
Ensure that the DPG2 and the eval board are detected in the Device Manager:{{ : | Ensure that the DPG2 and the eval board are detected in the Device Manager:{{ : | ||
If the two devices do not appear as shown, reinstall the latest version of DPGDownloader. | If the two devices do not appear as shown, reinstall the latest version of DPGDownloader. | ||
- | ==== Restart Evaluation Board service | + | ==== Restart Evaluation Board Service |
Open the Start Menu, click Run, then type services.msc, | Open the Start Menu, click Run, then type services.msc, | ||
Select the Analog Devices Evaluation Board Service and click Restart the Service. | Select the Analog Devices Evaluation Board Service and click Restart the Service. | ||
==== Verify DLL File is Present ==== | ==== Verify DLL File is Present ==== | ||
- | Open C:\Program Files (x86)\Analog Devices\DPG | + | Verify that the appropriate DLL for your evaluation board is present in: C:\Program Files (x86)\Analog Devices\DPG\ |
+ | the file is named: AnalogDevices.DPG.EvalBoard.ADXXXX.dll where XXXX is the part number of your evaluation board. If the file is not present install the DAC update file for your evaluation board. |