This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad974x-dpg2-ebz [24 Apr 2018 17:11] – [Using the AD9743/AD9745/AD9746/AD9747 Evaluation Boards] Annette Hurman | resources:eval:dpg:ad974x-dpg2-ebz [27 Apr 2018 17:42] – [BASIC HARDWARE SETUP] Annette Hurman | ||
---|---|---|---|
Line 19: | Line 19: | ||
This will install DPGDownloader required for loading vectors into the DPG2 and configuring the AD9747 evaluation board. | This will install DPGDownloader required for loading vectors into the DPG2 and configuring the AD9747 evaluation board. | ||
===== HARDWARE SETUP (DAC OUTPUT) ===== | ===== HARDWARE SETUP (DAC OUTPUT) ===== | ||
- | Once the DPGDownloader software is installed, the hardware can be connected . A single 5V power supply powers the evaluation board. The power supply should be able to source up to 1A to cover all of the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in the document, the modifications for observing the modulator output and different clocking options will be shown. | + | Once the DPGDownloader software is installed, the hardware can be connected . A single 5V power supply powers the evaluation board. The power supply should be able to source up to 1A to cover all the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in the document, the modifications for observing the modulator output and different clocking options will be shown. |
* The evaluation board plugs directly into the DPG2 or DPG3. | * The evaluation board plugs directly into the DPG2 or DPG3. | ||
- | The PC connects to both the DPG2 and the evaluation board through USB cables as showing | + | The PC connects to both the DPG2 and the evaluation board through USB cables as shown in Figure 1 and Figure 2 |
- | * The evaluation | + | * The evaluation |
The PC connects to both the SDP-H1 and the evaluation board through USB cables as shown in Figure 3 and Figure 4. | The PC connects to both the SDP-H1 and the evaluation board through USB cables as shown in Figure 3 and Figure 4. | ||
Line 35: | Line 35: | ||
Figure 4. SDP-H1 and AD9747 Evaluation Board | Figure 4. SDP-H1 and AD9747 Evaluation Board | ||
===== BASIC HARDWARE SETUP ===== | ===== BASIC HARDWARE SETUP ===== | ||
+ | It is suggested that the basic set-up is verified before making any modifications to the evaluation board. | ||
Connect the equipment to the AD9747 evaluation board per the following table: | Connect the equipment to the AD9747 evaluation board per the following table: | ||
- | * Equipment Connects to AD9747 Eval Board | + | * Equipment |
* Power Supply P5(+5V), | * Power Supply P5(+5V), | ||
* Signal Source J1(CLOCK IN), Set source to 100MHz, 2dBm output | * Signal Source J1(CLOCK IN), Set source to 100MHz, 2dBm output | ||
* PC USB Cable XP2 | * PC USB Cable XP2 | ||
* Spectrum Analyzer J5(IOUT1_P) or J9 (IOUT2_P) | * Spectrum Analyzer J5(IOUT1_P) or J9 (IOUT2_P) | ||
- | * DPG2 P1 and P2 | + | * DPG2 |
- | * SDP-H1 J4(FMC connector) | + | * SDP-H1 |
===== DPGDOWNLOADER SOFTWARE ===== | ===== DPGDOWNLOADER SOFTWARE ===== | ||
Power up the DPG and connect the USB cable to the PC. Next, run the DPGDownloader Software. A shortcut will be installed to your Start menu during the installation of the DAC Software Suite. To begin, click on the DPGDownloader shortcut in your Programs menu, typically at Start > Programs > Analog Devices > DPG > DPGDownloader. | Power up the DPG and connect the USB cable to the PC. Next, run the DPGDownloader Software. A shortcut will be installed to your Start menu during the installation of the DAC Software Suite. To begin, click on the DPGDownloader shortcut in your Programs menu, typically at Start > Programs > Analog Devices > DPG > DPGDownloader. |