This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad974x-dpg2-ebz [07 May 2018 17:12] – [WHAT’S IN THE BOX] Annette Hurman | resources:eval:dpg:ad974x-dpg2-ebz [07 Apr 2021 11:22] – Added Quick Start Guide Shine Cabatan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD9743/5/6/7 Evaluation Board Quick Start Guide ====== | + | ======EVALUATING THE AD9743/AD9745/AD9746/ |
- | ===== WHAT’S IN THE BOX ===== | + | =====Preface===== |
- | * AD9747-EBZ Evaluation Board | + | This user guide describes both the hardware and software setup needed |
- | * Mini-USB Cable | + | |
- | * AD9747 Evaluation Board CD | + | |
- | ===== EXAMPLE EQUIPMENT LIST ===== | + | |
- | * +5Vdc Power Supply: Agilent E3630A | + | |
- | * Digital Pattern Generator( DPG2 or DPG3) OR System Demonstration Platform( SDP-H1) and FMC to High-Speed DAC Evaluation Board Adaptor(AD-DAC-FMC-ADP) | + | |
- | * DAC Clock Source: R&S SML 02 | + | |
- | * AQM LO Clock Source: R&S SMA100A | + | |
- | * Spectrum Analyzer: Agilent PSAA or R&S FSU | + | |
- | * PC: Windows PC with 2 or more USB ports (See Appendix for system requirements) | + | |
- | ===== INTRODUCTION | + | |
- | The AD9747 Evaluation Board connects | + | |
- | (Note: The AD9747 operation is described in detail. The operation of the other devices in the family is described in a later section.) | + | |
- | ===== SOFTWARE INSTALLATION ===== | + | |
- | The DAC Software Suite plus AD9747/ | + | |
- | ===== HARDWARE SETUP (DAC OUTPUT) ===== | + | |
- | Once the DPGDownloader software is installed, the hardware can be connected . A single 5V power supply powers the evaluation board. The power supply should be able to source up to 1A to cover all the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in the document, the modifications for observing the modulator output and different clocking options will be shown. | + | |
- | * The evaluation board plugs directly into the DPG2 or DPG3. | + | |
- | The PC connects to both the DPG2 and the evaluation board through USB cables as shown in Figure 1 and Figure 2 | + | |
- | * The evaluation board plugs into the AD-DAC-FMC-ADP adapter board that plugs into the SDP-H1. | + | |
- | The PC connects to both the SDP-H1 and the evaluation board through USB cables as shown in Figure 3 and Figure 4. | + | |
- | (Note: The AD-DAC-FMC-ADP adapter board allows | + | This guide shows how AD974x-DPG2-EBZ |
- | {{ : | + | |
- | Figure 1. DPG2 and AD9747 Evaluation Board Bench set-up | + | =====Typical Setup===== |
- | {{ : | + | <WRAP centeralign> |
- | Figure 2. DPG2 and AD9747 Evaluation Board | + | //Figure |
- | {{ : | + | |
- | Figure | + | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ |
- | {{ :resources: | + | |
- | Figure 4. SDP-H1 and AD9747 Evaluation Board | + | =====Helpful Files:===== |
- | ===== BASIC HARDWARE SETUP ===== | + | * Old version of [[ftp:// |
- | It is suggested that the basic set-up is verified before making any modifications to the evaluation board. | + | * [[adi> |
- | Connect the equipment to the AD9747 evaluation board per the following table: | + | * IBIS Models: [[adi>/ |
- | * Equipment | + | * [[ftp:// |
- | * Power Supply P5(+5V), P6(GND) | + | * [[ftp:// |
- | * Signal Source J1(CLOCK IN), Set source to 100MHz, 2dBm output | + | * [[ftp://ftp.analog.com/ |
- | * PC USB Cable XP2 | + | * [[ftp:// |
- | * Spectrum Analyzer J5(IOUT1_P) or J9 (IOUT2_P) | + | * [[ftp:// |
- | * DPG2 P1 and P2 | + | |
- | * SDP-H1 | + | <note tip>Tip: Open this page in Internet Explorer to avoid problems when downloading files.</ |
- | Power up the DPG and connect the USB cable to the PC. Next, run the DPGDownloader Software. A shortcut will be installed to your Start menu during the installation of the DAC Software Suite. To begin, click on the DPGDownloader shortcut in your Programs menu, typically at Start > Programs > Analog Devices > DPG > DPGDownloader. | + | |
- | The basic parts of the DPGDownloader window are; Hardware Config Panel, EVB Config, Vector Generation Pull-Down Menu, Vector Palette, Vector Selection Panel and the Download and Play buttons. | + | =====Software Needed: |
- | {{ :resources: | + | * [[: |
- | Figure 5. DPGDownloader Window | + | * [[: |
- | * - If the AD9747 | + | |
- | * - Generate a sinewave by pulling down the “Add Generated Waveform” menu and choosing “Single Tone”. Fill in the form as shown in Figure 5 (Sample Rate = 100MHz, Desired Frequency = 17.0MHz, etc.). Select the I and Q data vectors in the data selection panel. | + | =====Hardware Needed: |
- | * - Configure the eval board by writing the value 01 to register 1E1. This configures the AD9516 to use the CLK input to drive the clock path. | + | * [[adi> |
- | {{ : | + | * [[: |
- | * - Bypass the clock dividers on the AD9516. | + | * 12V 1A Wall Adapter for SDP-H1 |
- | {{ : | + | * [[adi>AD-DAC-FMC]]-ADP High-Speed DAC Evaluation Board to FMC Adaptor Board |
- | * - The DCO frequency field in the DPGDownloader window should now be reading something close to 100MHz. | + | * PC with ACE and DPG Lite Software Applications |
- | * - Next hit the download button. This transfers the data from the PC to the DPG memory. | + | * 5V 1A Power Supply |
- | * - When the vector has finished downloading, | + | * High-Frequency Continuous Wave Generator |
- | * - The output from J5 and J9 should be a clean 29MHz tone as shown below: | + | * Signal/ |
- | {{ : | + | * (2) USB A to USB Mini Cables |
- | ===== Using the AD9743/ | + | * (2) SMA Cables |
- | The evaluation boards for the AD9743/ | + | * (2) Banana Plug Cables |
- | These fields | + | |
- | {{ : | + | =====Quick Start Guide===== |
- | ===== Selecting the Modulator Outputs ===== | + | - Attach |
- | By default, solder jumpers JP4, JP5, JP6, and JP7 configure | + | - Connect SDP-H1 to PC via USB and to a 12V 1A power supply. |
- | {{ : | + | - Set clock input to 100MHz and 2dBm. |
- | Figure | + | - Open ACE. The board will be automatically recognized by the software. Otherwise, install |
- | ===== Eval Board Jumper Options ===== | + | - Start DPG Lite or DPG Downloader. At the SDP-H1 part of the software, the device part number and clock frequency |
- | There are 6 pin jumpers on the evaluation board corresponding to the 6 supplies on the board. They serve as ‘switches’ that determine if the on board LDOs or external supplies are used for each individual supply. They are shunted by default, which means on board LDOs are used. When an external supply is necessary, pull off the shunt from the corresponding supply | + | - In ACE, apply the default values in the Initial Configuration wizard as shown in Figure 2.{{ : |
- | {{ : | + | //Figure 2. ACE Initial Configuration Wizard for EVAL-AD9747//</ |
+ | - In DPG Lite or DPG Downloader, from the Add Generator Waveforms pulldown menu select Single Tone and apply the settings as shown in Figure | ||
+ | //Figure | ||
+ | - Select | ||
+ | - Press the download arrow and then the play button. The spectrum similar | ||
+ | //Figure 4. EVAL-AD9747 FFT for Fdac=100MHz, | ||