This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad974x-dpg2-ebz [27 Apr 2018 17:58] – [DPGDOWNLOADER SOFTWARE] Annette Hurman | resources:eval:dpg:ad974x-dpg2-ebz [07 Apr 2021 11:22] – Added Quick Start Guide Shine Cabatan | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD9743/5/6/7 Evaluation Board Quick Start Guide ====== | + | ======EVALUATING THE AD9743/AD9745/AD9746/AD9747 DIGITAL-TO-ANALOG CONVERTER====== |
- | ===== WHAT’S IN THE BOX ===== | + | =====Preface===== |
- | * WHAT’S IN THE BOX | + | This user guide describes both the hardware |
- | * AD9747-EBZ Evaluation Board | + | |
- | * Mini-USB Cable | + | |
- | * AD9747 Evaluation Board CD | + | |
- | EXAMPLE EQUIPMENT LIST | + | |
- | * +5Vdc Power Supply: Agilent E3630A | + | |
- | * Digital Pattern Generator( DPG2 or DPG3) OR System Demonstration Platform( SDP-H1) | + | |
- | * DAC Clock Source: R&S SML 02 | + | |
- | * AQM LO Clock Source: R&S SMA100A | + | |
- | * Spectrum Analyzer: Agilent PSAA or R&S FSU | + | |
- | * PC: Windows PC with 2 or more USB ports (See Appendix for system requirements) | + | |
- | ===== INTRODUCTION ===== | + | |
- | The AD9747 Evaluation Board connects to the Analog Devices Digital Pattern Generator (DPG2, PN: ADI HSC-DAC-DPG-BZ; or DPG3, PN: AD –DPG3) or System Demonstration Platform (SDP-H1, PN: EVAL-SDP-CH1Z) to allow for quick evaluation of the AD9747. The DPG2 or SDP-H1 allows the user to create many types of digital vectors and transmit these at speed to the AD9747 in any of the AD9747 operating modes. The AD9747 | + | |
- | (Note: The AD9747 operation is described in detail. The operation of the other devices in the family is described in a later section.) | + | |
- | ===== SOFTWARE INSTALLATION ===== | + | |
- | The AD9747 application software, DPGDownloader, | + | |
- | This will install DPGDownloader required for loading vectors into the DPG2 and configuring the AD9747 | + | |
- | ===== HARDWARE SETUP (DAC OUTPUT) ===== | + | |
- | Once the DPGDownloader software is installed, the hardware can be connected . A single 5V power supply powers the evaluation board. The power supply should be able to source up to 1A to cover all the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in the document, the modifications for observing the modulator output and different clocking options will be shown. | + | |
- | * The evaluation board plugs directly into the DPG2 or DPG3. | + | |
- | The PC connects to both the DPG2 and the evaluation board through USB cables as shown in Figure 1 and Figure 2 | + | |
- | * The evaluation board plugs into the AD-DAC-FMC-ADP adapter board that plugs into the SDP-H1. | + | |
- | The PC connects | + | |
- | (Note: The AD-DAC-FMC-ADP adapter board allows | + | This guide shows how AD974x-DPG2-EBZ |
- | {{ : | + | |
- | Figure 1. DPG2 and AD9747 Evaluation Board Bench set-up | + | =====Typical Setup===== |
- | {{ :resources:eval: | + | <WRAP centeralign> |
- | Figure 2. DPG2 and AD9747 | + | //Figure 1. EVAL-AD9743/ |
- | {{ :resources: | + | |
- | Figure 3. SDP-H1 and AD9747 | + | <note tip>Tip: Click on any picture in this guide to open an enlarged version.</ |
- | {{ :resources: | + | |
- | Figure 4. SDP-H1 and AD9747 Evaluation Board | + | =====Helpful Files: |
- | ===== BASIC HARDWARE SETUP ===== | + | * Old version of [[ftp:// |
- | It is suggested that the basic set-up is verified before making any modifications to the evaluation board. | + | * [[adi> |
- | Connect the equipment to the AD9747 evaluation board per the following table: | + | * IBIS Models: [[adi>/ |
- | * Equipment | + | * [[ftp:// |
- | * Power Supply P5(+5V), P6(GND) | + | * [[ftp://ftp.analog.com/ |
- | * Signal Source J1(CLOCK IN), Set source | + | * [[ftp:// |
- | * PC USB Cable XP2 | + | * [[ftp://ftp.analog.com/ |
- | * Spectrum Analyzer J5(IOUT1_P) or J9 (IOUT2_P) | + | * [[ftp:// |
- | * DPG2 P1 and P2 | + | |
- | * SDP-H1 | + | <note tip>Tip: Open this page in Internet Explorer to avoid problems when downloading files.</ |
- | ===== DPGDOWNLOADER SOFTWARE | + | |
- | Power up the DPG and connect the USB cable to the PC. Next, run the DPGDownloader Software. A shortcut will be installed | + | =====Software Needed:===== |
- | The basic parts of the DPGDownloader window are; Hardware Config Panel, EVB Config, Vector Generation Pull-Down Menu, Vector Palette, Vector Selection Panel and the Download and Play buttons. | + | * [[: |
- | {{ : | + | * [[:resources: |
- | Figure | + | |
- | | + | =====Hardware Needed: |
- | | + | * [[adi> |
- | | + | * [[: |
- | {{ : | + | * 12V 1A Wall Adapter for SDP-H1 |
- | * - Bypass | + | * [[adi> |
- | {{ : | + | * PC with ACE and DPG Lite Software Applications |
- | * - The DCO frequency | + | * 5V 1A Power Supply |
- | | + | * High-Frequency Continuous Wave Generator |
- | * - When the vector has finished downloading, hit the play button. This starts | + | * Signal/Spectrum Analyzer |
- | * - The output from J5 and J9 should be a clean 29MHz tone as shown below: | + | * (2) USB A to USB Mini Cables |
- | {{ : | + | * (2) SMA Cables |
- | ===== Using the AD9743/AD9745/ | + | * (2) Banana Plug Cables |
- | The evaluation boards for the AD9743/AD9745/AD9746/AD9747 are identical except for the DUT installed. The operation of the eval boards is also the same except for the vector generation “DAC Resolution” field and the Data Width fields as shown below. | + | |
- | These fields should be configured to match the DUT. | + | =====Quick Start Guide===== |
- | {{ : | + | - Attach AD9743-DPG2-EBZ/ |
- | ===== Selecting | + | - Connect SDP-H1 to PC via USB and to a 12V 1A power supply. |
- | By default, solder jumpers JP4, JP5, JP6, and JP7 configure | + | - Set clock input to 100MHz and 2dBm. |
- | {{ : | + | - Open ACE. The board will be automatically recognized |
- | ===== Eval Board Jumper Options ===== | + | - Start DPG Lite or DPG Downloader. At the SDP-H1 part of the software, the device part number and clock frequency should be displayed. |
- | There are 6 pin jumpers on the evaluation board corresponding to the 6 supplies on the board. They serve as ‘switches’ that determine if the LDOs on board or external supplies are used for each individual supply. They are shunted by default, which means on board LDOs are used. When an external supply is necessary, pull off the shunt from the corresponding supply | + | - In ACE, apply the default values in the Initial Configuration wizard |
- | {{ : | + | //Figure 2. ACE Initial Configuration Wizard for EVAL-AD9747//</WRAP> |
+ | - In DPG Lite or DPG Downloader, from the Add Generator Waveforms pulldown menu select Single Tone and apply the settings as shown in Figure | ||
+ | //Figure 3. DPG Lite session for EVAL-AD9747//</ | ||
+ | - Select | ||
+ | - Press the download arrow and then the play button. The spectrum similar | ||
+ | //Figure 4. EVAL-AD9747 FFT for Fdac=100MHz, | ||