This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad917x-fmc-ebz [28 Jan 2019 20:07] – Added AD9175 Michele Viani | resources:eval:dpg:ad917x-fmc-ebz [23 Oct 2019 23:14] – [DC Test/NCO Mode Without ADS7/ADS8/KCU105] Arik Landsman | ||
---|---|---|---|
Line 22: | Line 22: | ||
Once both programs are installed, launch ACE. On the start-up window, navigate to Tools -> Manage Plugins. The plugin manager pop-up window will display. Search for AD9172 and select install plugin to install the appropriate plugin files for the FMC evaluation board. | Once both programs are installed, launch ACE. On the start-up window, navigate to Tools -> Manage Plugins. The plugin manager pop-up window will display. Search for AD9172 and select install plugin to install the appropriate plugin files for the FMC evaluation board. | ||
+ | |||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
+ | ==== ADS7/ADS8 Setup ==== | ||
+ | |||
+ | The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | ||
+ | - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | ||
+ | - Plug the mini USB cable into the AD917x-FMC-EBZ board and connect the other end to the PC being used. | ||
+ | - Connect the ADS7 or ADS8 to the PC being used with the USB cable to the ADS7 or ADS8 board and connect the power supply. | ||
+ | - Connect the DAC0 output (J2) or the DAC1 output (J1) to the spectrum analyzer. | ||
+ | |||
+ | {{ : | ||
+ | Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8 | ||
+ | |||
+ | ==== KCU-105 Setup ==== | ||
The following items should be included in the evaluation kit (KCU-105 platform not included, purchased separately by the customer): | The following items should be included in the evaluation kit (KCU-105 platform not included, purchased separately by the customer): | ||
* Interconnect Board (connects FX3 board to the KCU-105 FMC connector) with Cypress FX3 board (only needed if using the KCU-105) | * Interconnect Board (connects FX3 board to the KCU-105 FMC connector) with Cypress FX3 board (only needed if using the KCU-105) | ||
Line 36: | Line 49: | ||
Connect a reference clock frequency to the “Board Ref Clock” connection shown in Figure 1 (SMA connector J4). This is the configuration required any time the evaluation board is to be measured and used. Turn on the KCU-105 power and plug in both USB cables to the host computer. | Connect a reference clock frequency to the “Board Ref Clock” connection shown in Figure 1 (SMA connector J4). This is the configuration required any time the evaluation board is to be measured and used. Turn on the KCU-105 power and plug in both USB cables to the host computer. | ||
- | ==== Additional KCU105 Setup ==== | + | === Using KCU-105 with DPG Downloader |
The KCU-105 board requires some additional setup steps to be compatible with the DPGDownloader software. | The KCU-105 board requires some additional setup steps to be compatible with the DPGDownloader software. | ||
Line 44: | Line 58: | ||
Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. This step only needs to be done once in order to set up the FPGA board properly for any future use with DPGDownloader software. | Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. This step only needs to be done once in order to set up the FPGA board properly for any future use with DPGDownloader software. | ||
- | ==== ADS7/ | + | ==== DC Test/NCO Mode Without |
- | The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | + | The AD917x can work in DC TEST/NCO mode without |
- | | + | |
- | - Plug the mini USB cable into the AD917x-FMC-EBZ board and connect the other end to the PC being used. | + | |
- | - Connect | + | |
- | - Connect | + | |
- | {{ : | ||
- | Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8 | ||
==== Direct Clock the AD917x ==== | ==== Direct Clock the AD917x ==== | ||
Line 62: | Line 70: | ||
Figure 4. Direct Clocking Option for DAC Clk± Pins | Figure 4. Direct Clocking Option for DAC Clk± Pins | ||
- | ==== DC Test/NCO Mode Without ADS7/ | ||
- | |||
- | The AD917x can work in DC TEST/NCO mode without ADS7/ | ||
===== Using DPGDownloader Software ===== | ===== Using DPGDownloader Software ===== |