This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:dpg:ad917x-fmc-ebz [23 Oct 2019 23:17] – [General Description] Arik Landsman | resources:eval:dpg:ad917x-fmc-ebz [09 Feb 2022 21:18] – [What's In The Box] Arik Landsman | ||
---|---|---|---|
Line 4: | Line 4: | ||
* Mini USB cable | * Mini USB cable | ||
- | **Note: if using the KCU-105 | + | === Additional Components Needed for an ADS7 / ADS8-V1 Evaluation Platform === |
+ | * Pattern generator board: ADS7 (up to 13Gbps SERDES) or ADS8-V1 (covers the full AD917x range): [[adi> | ||
+ | |||
+ | **Note: if using the Xilinx KCU105 | ||
+ | |||
+ | === Additional Components Needed for a KCU105 Evaluation Platform === | ||
+ | * Xilinx | ||
+ | | ||
+ | * Cypress FX3 FMC Interconnect Board (CYUSB3ACC-005): | ||
+ | | ||
- | === What's In The Box: AD-HSDACFX3-EBZ (Needed only with the KCU-105) === | ||
- | * FX3 Cypress Board + FMC Interconnect Board (pre-programmed and assembled for immediate use) | ||
- | * Micro SD card containing FPGA image to be used with the KCU-105 | ||
===== General Description ===== | ===== General Description ===== | ||
- | The AD917x Evaluation Board Setup Guide provides details about how to set up the hardware and software for the evaluation kit. This guide explains how to setup the KCU-105 | + | The AD917x Evaluation Board Setup Guide provides details about how to set up the hardware and software for the evaluation kit. This guide explains how to setup the KCU105 |
The AD917x-FMC-EBZ evaluation board can be driven by an external direct clock with DAC PLL off or the on-board clock from HMC7044 with DAC PLL on. The reference clock of HMC7044 can be provided by the on-board 122.88MHz crystal or the external signal generator. | The AD917x-FMC-EBZ evaluation board can be driven by an external direct clock with DAC PLL off or the on-board clock from HMC7044 with DAC PLL on. The reference clock of HMC7044 can be provided by the on-board 122.88MHz crystal or the external signal generator. | ||
Line 25: | Line 31: | ||
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
- | ==== ADS7/ADS8 Setup ==== | ||
+ | ==== Clocking the AD917x-FMC-EBZ ==== | ||
+ | |||
+ | From the factory, the AD917X-FMC-EBZ is configured to generate all necessary clocks using an on-board clocking IC, the HMC7044. Using PLL2, The HMC7044 generates the lanerate/40 clock, two phase-aligned SYSREF clocks, and a reference for the AD917x' | ||
+ | |||
+ | === Directly Clocking the AD917x-FMC-EBZ === | ||
+ | |||
+ | For some configurations, | ||
+ | |||
+ | |||
+ | ** Clocking for a JESD204B link ** | ||
+ | |||
+ | When using a JESD204B link to the AD917x, the JESD204B link clocks are generated by the HMC7044' | ||
+ | |||
+ | It is best to use a second, low phase noise, reference clock source with 0 dBm output level, connected to the SMA port at J41; the reference clock source must be frequency locked to a common reference with the DAC clock source. Two options exist: Two separate sources can be synchronized through the 10MHz INPUT/ | ||
+ | |||
+ | |||
+ | ** Clocking for NCO-only mode** | ||
+ | |||
+ | When using the AD917x in NCO-only mode, without a JESD204B link, the only external clock needed is at J34. The HMC7044 is not used in this case. | ||
+ | |||
+ | {{ : | ||
+ | Figure 4. Direct Clocking Option for DAC Clk± Pins | ||
+ | |||
+ | |||
+ | ==== ADS7/ | ||
+ | <note important> | ||
The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | The Cypress FX3 and interconnect board are not needed if the ADS7 or ADS8 board is used for data pattern generation. The hardware setup configuration when using the ADS7/ADS8 is as follows: | ||
- Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | - Connect the AD917x-FMC-EBZ board to the FMC connector on the ADS7 or ADS8. | ||
Line 36: | Line 67: | ||
Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8 | Figure 3. Evaluation Board Kit Components Hardware Connection Setup with ADS8 | ||
- | ==== KCU-105 | + | ==== KCU105 |
- | The following items should be included in the evaluation | + | In order to operate |
- | | + | * AD917x-FMC-EBZ Evaluation |
- | | + | * Xilinx KCU105 Evaluation Kit: http:// |
- | * AD917x-FMC-EBZ Evaluation Board | + | * Cypress |
- | * Mini USB to USB Cable (connects mini USB port on evaluation board to USB port on a computer) | + | * Cypress FX3 FMC Interconnect Board (CYUSB3ACC-005): https:// |
- | | + | * Micro SD Card |
- | Connect the boards and cables to the KCU-105 | + | * USB3.0 to USB Cable (connects FX3 board USB3.0 port to USB port on a computer) |
+ | * Mini USB to USB Cable (connects mini USB port on evaluation board to USB port on a computer) | ||
+ | |||
+ | **Before connecting the hardware, the Cypress FX3 board and Micro SD Card must be programmed appropriately.** | ||
+ | |||
+ | |||
+ | === Programming the Cypress FX3 Board for KCU105 Setup === | ||
+ | **FX3 SDP Drivers:** {{ : | ||
+ | |||
+ | Begin by installing the FX3 SDP Drivers using the above link. When installing the drivers, ensure that the FX3 board is NOT plugged into your computer. A successful install will give an exit code of 256 in the printout while an unsuccessful install will try to restart your computer. If you experience an unsuccessful install, try re-running the driver installation executable. Some machines need to run this installer 3 times before the drivers are installed. You may receive a notification that newer drivers have already been installed—in this case, the installer will automatically abort installation as expected. | ||
+ | |||
+ | You can confirm proper installation by following these steps: | ||
+ | - Using the USB3.0 cable, plug the FX3 FMC module into your computer WITHOUT the KCU105 connected. | ||
+ | - Open Device Manager. | ||
+ | - Confirm successful driver installation by verifying the presence of “High Speed Converter USB3.0 Evaluation Platform” under “ADI Development Tools” as shown below:{{ : | ||
+ | |||
+ | If you have confirmed successful driver installation, | ||
+ | |||
+ | Most FX3 boards come preprogrammed with ADI’s firmware, but there are some instances when this firmware is missing. If you have installed the FX3 SDP Drivers but only see an “FX3” device with a warning listed under Device Manager, then your FX3 board is not preprogrammed. In this case, follow these steps to program your FX3 board: | ||
+ | |||
+ | **FX3 Firmware Image:** {{ : | ||
+ | - Download and install the Cypress SDK via http:// | ||
+ | - Open the "USB Control Center" | ||
+ | - **Connect jumper J4** on the FX3 and connect the FX3’s USB cable to your computer. The FX3 will appear as " | ||
+ | - Click on the " | ||
+ | - Select the FX3 firmware image (image can be downloaded at the start of this section) when prompted by the file selection dialog. | ||
+ | - After the programming finishes, **disconnect jumper J4** and reset the FX3 via the pushbutton switch near the USB3.0 connector. | ||
+ | - If successful, the " | ||
+ | |||
+ | As described earlier, successful firmware installation can be confirmed by following these steps: | ||
+ | - Using the USB3.0 cable, plug the FX3 FMC module into your computer WITHOUT the KCU105 connected. | ||
+ | - Open Device Manager. | ||
+ | - Confirm successful firmware installation by verifying the presence of “High Speed Converter USB3.0 Evaluation Platform” under “ADI Development Tools” as shown below:{{ : | ||
+ | |||
+ | === Programming the Micro SD Card for KCU105 Setup === | ||
+ | **FPGA Image:** {{ : | ||
+ | |||
+ | Download the KCU105 FPGA image files and copy them to the MicroSD card so that the xilinx.sys file and kcu105 folder are at the top level of the MicroSD card: | ||
+ | {{ : | ||
+ | |||
+ | === KCU105 Hardware Setup === | ||
+ | Connect the boards and cables to the KCU105 | ||
{{ : | {{ : | ||
Figure 1. Evaluation Board Kit Components Hardware Connection Setup | Figure 1. Evaluation Board Kit Components Hardware Connection Setup | ||
- | Connect a reference clock frequency to the “Board Ref Clock” connection shown in Figure 1 (SMA connector J4). This is the configuration required any time the evaluation board is to be measured and used. Turn on the KCU-105 | + | Connect a reference clock frequency to the “Board Ref Clock” connection shown in Figure 1 (SMA connector J4). This is the configuration required any time the evaluation board is to be measured and used. Turn on the KCU105 |
- | === Using KCU-105 | + | === Using KCU105 |
- | The KCU-105 | + | The KCU105 |
{{ : | {{ : | ||
Figure 2. KCU105 DIP Switch Settings for Loading Image from Micro-SD Card | Figure 2. KCU105 DIP Switch Settings for Loading Image from Micro-SD Card | ||
- | Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. This step only needs to be done once in order to set up the FPGA board properly for any future use with DPGDownloader software. | + | Once these steps are complete, the KCU105 board can be powered on and plugged into the USB ports on the host PC. After powering on the KCU105, wait approximately 10 seconds so that the KCU105 has adequate time to load the FPGA image. If the KCU105' |
- | ==== DC Test/NCO Mode Without ADS7/ | + | ==== Other FPGA Development Kits==== |
+ | The AD917x-FMC-EBZ complies with the VITA57.1 standard. Thus, the AD917x-FMC-EBZ can be used with any FMC-compliant FPGA development kit. The AD917x has a convenient crossbar switch, which allows to remap the physical lanes routed to its SERDESx+/- pins on the PCB (" | ||
+ | ==== NCO-only Mode ("DC Test Mode" | ||
- | The AD917x can work in DC TEST/NCO mode without ADS7/ | + | The AD917x can work in NCO-only mode, without ADS7/ |
+ | If using an external clock source, connect a low phase noise, high frequency clock source to J34. See the " | ||
- | ==== Direct Clock the AD917x | + | The outputs of the AD917x |
- | For some configurations, | + | Some applications |
+ | |||
+ | - reset the board in ACE (Reset Board button in the " | ||
+ | - in the Wizard, under Eval System Option select chip to configure: " | ||
+ | - Under DC Test Mode, select the option " | ||
+ | - Under SERDES Interface, set the link mode and interpolation (this will apply a clock to the corresponding datapaths. E.g. dual-link to enable both datapath0 and datapath1, that would feed DAC0 and DAC1 respectively) | ||
+ | - Under Clock frequencies, | ||
- | {{ : | ||
- | Figure 4. Direct Clocking Option for DAC Clk± Pins | ||
===== Using DPGDownloader Software ===== | ===== Using DPGDownloader Software ===== | ||
Launch the DPGDownloader software from the Start Menu (Start → All Programs → Analog Devices → DPG → DPG Downloader). When the program starts the DPG Panel should look recognize the evaluation board connected as shown in the AD917x panel being displayed as shown in Figure 5. The desired SERDES JESD204B mode can be selected by using the “JSED Mode” drop-down menu. If running in Dual Link mode, check the “Dual Link” checkbox on the panel to enable the second link options. | Launch the DPGDownloader software from the Start Menu (Start → All Programs → Analog Devices → DPG → DPG Downloader). When the program starts the DPG Panel should look recognize the evaluation board connected as shown in the AD917x panel being displayed as shown in Figure 5. The desired SERDES JESD204B mode can be selected by using the “JSED Mode” drop-down menu. If running in Dual Link mode, check the “Dual Link” checkbox on the panel to enable the second link options. | ||
- | //Note: If using the KCU-105, first power up the KCU105 board and wait for the heartbeat LEDs shown in Figure 1 to begin flashing. Then open up DPGDownloader and ensure the Configuration Version displays 11/07/16, confirming that the FPGA image is loaded properly from the microSD card. If this does not display or if the KCU105 has been powered off and back on again, reselect the AD917x from the Evaluation Board dropdown menu to reinitialize the panel and the configuration version should display properly. | + | //Note: If using the KCU105, first power up the KCU105 board and wait for the heartbeat LEDs shown in Figure 1 to begin flashing. Then open up DPGDownloader and ensure the Configuration Version displays 11/07/16, confirming that the FPGA image is loaded properly from the microSD card. If this does not display or if the KCU105 has been powered off and back on again, reselect the AD917x from the Evaluation Board dropdown menu to reinitialize the panel and the configuration version should display properly. |
// | // | ||
Line 168: | Line 247: | ||
The raw macro file will be saved using ACE syntax, which is not easily readable. To remedy this, the ACE software download includes the Macro to Hex Conversion Tool. The user can choose to include or exclude register write, reads, and/or comments in the conversion. The file pathways for the source and save paths should be the same, except that one should be an .acemacro file and the other should be a .txt file. The “Convert” button converts and opens the converted text file, which is easier to read. The conversion tool can also convert back to an .acemacro file if desired. The Macro to Hex converter tool is located in the start menu under "All Programs" | The raw macro file will be saved using ACE syntax, which is not easily readable. To remedy this, the ACE software download includes the Macro to Hex Conversion Tool. The user can choose to include or exclude register write, reads, and/or comments in the conversion. The file pathways for the source and save paths should be the same, except that one should be an .acemacro file and the other should be a .txt file. The “Convert” button converts and opens the converted text file, which is easier to read. The conversion tool can also convert back to an .acemacro file if desired. The Macro to Hex converter tool is located in the start menu under "All Programs" | ||
+ | <note important> | ||
<WRAP column 40%> | <WRAP column 40%> | ||
{{ : | {{ : |