This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad916x-fmcx-ebz [01 Dec 2017 17:39] – [Basic Hardware Issues] Jarrah Bergeron | resources:eval:dpg:ad916x-fmcx-ebz [06 Dec 2017 17:59] – [AD916X-FMCX-EBZ EVALUATION SOFTWARE] Jarrah Bergeron | ||
---|---|---|---|
Line 17: | Line 17: | ||
=====AD916X-FMCX-EBZ EVALUATION SOFTWARE===== | =====AD916X-FMCX-EBZ EVALUATION SOFTWARE===== | ||
The AD916x-FMCx-EBZ Evaluation Board software has an easy-to-use graphical user interface (GUI) called ACE (Analysis, Control, Evaluation). It is included on the Evaluation Board CD. This will install DPG Downloader (for loading vectors into the ADS7) and the AD916x ACE SPI progion. The SPI programmer enables full access to the AD916x’s register map, and has additional functionality such as the ability to record, load, and save macros, or register sequences, to ease programming of the device. The ADF4355 and AD9508 are also configured by ACE. Several macros or register sequences will be used by this guide to demonstrate the usefulness of the function and to ease the setup of the device. ACE also controls the SPDT switch for selecting the clock source. | The AD916x-FMCx-EBZ Evaluation Board software has an easy-to-use graphical user interface (GUI) called ACE (Analysis, Control, Evaluation). It is included on the Evaluation Board CD. This will install DPG Downloader (for loading vectors into the ADS7) and the AD916x ACE SPI progion. The SPI programmer enables full access to the AD916x’s register map, and has additional functionality such as the ability to record, load, and save macros, or register sequences, to ease programming of the device. The ADF4355 and AD9508 are also configured by ACE. Several macros or register sequences will be used by this guide to demonstrate the usefulness of the function and to ease the setup of the device. ACE also controls the SPDT switch for selecting the clock source. | ||
- | + | ||
- | {{ : | + | {{: |
Figure 1. Block diagram of the AD916x-FMCx-EBZ lab bench set-up | Figure 1. Block diagram of the AD916x-FMCx-EBZ lab bench set-up | ||