Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
Next revision
Previous revision
resources:eval:dpg:ad9154-m6720-ebz [26 Feb 2015 22:14] – 35 Larry Welchresources:eval:dpg:ad9154-m6720-ebz [08 Jan 2021 11:03] (current) – Fixed bad link for AD9154-ADRF6720-EBZ Ioana Chelaru
Line 1: Line 1:
-====== AD9154-M6720-EBZ Evaluation Board Quick Start Guide ======     +====== AD9154-ADRF6720-EBZ Evaluation Board Quick Start Guide ======     
-===== Getting Started with the AD9154-M6720-EBZ Evaluation Board and Software =====+===== Getting Started with the AD9154-ADRF6720-EBZ Evaluation Board and Software =====
 ==== What's in the Box ==== ==== What's in the Box ====
-  * [[adi>AD9154-M6720-EBZ]]  Evaluation Board for DPG3+  * [[adi>AD9154|AD9154-ADRF6720-EBZ]]  Evaluation Board for DPG3
   * Evaluation Board CD   * Evaluation Board CD
   * Mini-USB Cable   * Mini-USB Cable
Line 9: Line 9:
   * Two Sinusoidal Clock Sources   * Two Sinusoidal Clock Sources
   * Spectrum Analyzer   * Spectrum Analyzer
-  * Oscilloscope 
   * Data Pattern Generator Series 3 (DPG3)   * Data Pattern Generator Series 3 (DPG3)
 ===== Introduction ====== ===== Introduction ======
-The AD9154-M6720-EBZ connects to a DPG3. The AD9154 is a quad JESD204B signal processing RF Digital to Analog Converter. The DPG3 automatically formats the data and sends it to the AD9154-M6720-EBZ via its JESD204B lanes. The AD9154-M6720-EBZ includes an AD9154 and two ADRF6720-27 Wideband Quadrature Modulators with Integrated PLL and VCO. There is a board level passive low pass filter between the output of each AD9154 DAC and its corresponding ADRF6720-27 baseband input. The Evaluation Board (EVB) runs from a single +5V lab supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a CFRAME clock used by the DPG3. +The AD9154-ADRF6720-EBZ connects to a DPG3. The AD9154 is a quad JESD204B signal processing RF Digital to Analog Converter. The DPG3 automatically formats the data and sends it to the AD9154-M6720-EBZ via its JESD204B lanes. The AD9154-M6720-EBZ includes an AD9154 and two ADRF6720-27 Wideband Quadrature Modulators with Integrated PLL and VCO. There is a board level passive low pass filter between the output of each AD9154 DAC and its corresponding ADRF6720-27 baseband input. The Evaluation Board (EVB) runs from a single +5V lab supply. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a CFRAME clock used by the DPG3. 
 ===== AD9154 and ADRF6720-27 Evaluation Software ===== ===== AD9154 and ADRF6720-27 Evaluation Software =====
 The AD9154 and ADRF6720-27 Evaluation software runs on the easy-to-use SPIPro graphical user interface (GUI). It is included on the Evaluation Board CD.     The AD9154 and ADRF6720-27 Evaluation software runs on the easy-to-use SPIPro graphical user interface (GUI). It is included on the Evaluation Board CD.    
Line 54: Line 53:
  
 b. Select JESD Mode 0.  b. Select JESD Mode 0. 
-c. Uncheck the “Subclass 1” box+c. Uncheck the “Subclass 1” box.
  
 d. Select “2” for Interpolation.  d. Select “2” for Interpolation. 
  
 e. Press the “Configure DAC and Clock” Button  e. Press the “Configure DAC and Clock” Button 
-f. The JESD204B PLL Lock Readback light should turn green and register bit settings will be populated. The GUI will look like Figure 4, except that values in “CodeGrpSync”, “FrameSync”, “GoodCheckSum”, and “InitialLaneSync” may be different because the link JESD204B Transmitter has not yet been set up.+ 
 +f. The JESD204B PLL Lock Readback light should turn green and register bit settings will be populated. The GUI will look like Figure 4, except that values in “CodeGrpSync”, “FrameSync”, “GoodCheckSum”, and “InitialLaneSync” may be different because the link JESD204B Transmitter has not yet been set up.  
 g. Load Register Settings into the ADRF6720 devices by clicking “Restore Registers from File” and locating “ADRF6720.csv”. This should be located at the install directory for the AD9154 SPIPro application.  g. Load Register Settings into the ADRF6720 devices by clicking “Restore Registers from File” and locating “ADRF6720.csv”. This should be located at the install directory for the AD9154 SPIPro application. 
 +
 h. Click on “ADRF6720” tab for Mod 1 and confirm the GUI matches Figure 5 below. h. Click on “ADRF6720” tab for Mod 1 and confirm the GUI matches Figure 5 below.
  
Line 69: Line 71:
 </WRAP center> </WRAP center>
 i. Click on “ADRF67202” tab for Mod 2 and confirm the GUI matches Figure 6 below. i. Click on “ADRF67202” tab for Mod 2 and confirm the GUI matches Figure 6 below.
-{{:resources:eval:dpg:9154m6720_figure_6.png?nolink|}}+{{:resources:eval:dpg:9154m6720_figure_6_1.png?nolink|}}
 |  Figure 6. Configured SPIPro ADRF67202 tab of the AD9154 SPI software   | |  Figure 6. Configured SPIPro ADRF67202 tab of the AD9154 SPI software   |
 4. DPG Downloader Start Up Sequence 4. DPG Downloader Start Up Sequence
resources/eval/dpg/ad9154-m6720-ebz.txt · Last modified: 08 Jan 2021 11:03 by Ioana Chelaru