This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9154-ebz [21 Jun 2017 16:56] – Bailey Meyer | resources:eval:dpg:ad9154-ebz [28 Jul 2017 20:46] (current) – Bailey Meyer | ||
---|---|---|---|
Line 55: | Line 55: | ||
</ | </ | ||
- | Ensure that the {{: | + | Ensure that the {{: |
<WRAP center> | <WRAP center> | ||
Line 150: | Line 150: | ||
d. Set Data Rate to 750 MHz, Desired Frequency to 112 MHz, Amplitude to -1.0 dBFS, uncheck unsigned, check Generate Complex Data (I&Q). | d. Set Data Rate to 750 MHz, Desired Frequency to 112 MHz, Amplitude to -1.0 dBFS, uncheck unsigned, check Generate Complex Data (I&Q). | ||
- | e. Under Data Playback, select I data for DAC 0 and DAC2, and Q data for DAC 1 and DAC3. | + | e. Under Data Playback, select I data for DAC 0 and DAC2, and Q data for DAC 1 and DAC3. The DPGDownloader settings should resemble Figure 14. |
f. Click Download ({{: | f. Click Download ({{: | ||
- | 5. On SPIPro Quick Start Tab, click “Read All Registers” and confirm the GUI looks the same as Figure | + | 5. On SPIPro Quick Start Tab, click “Read All Registers” and confirm the GUI looks the same as Figure |
6. The current on the 5V supply should read around 1800mA - 1950mA. | 6. The current on the 5V supply should read around 1800mA - 1950mA. | ||
Line 163: | Line 163: | ||
| Figure 12. Fully Configured AD9154 SPIPro | | Figure 12. Fully Configured AD9154 SPIPro | ||
</ | </ | ||
+ | <WRAP center> | ||
- | {{: | + | | {{ {{ : |
- | | Figure 13 DPG Downloader Panel at Start Up | + | |
+ | | Figure 13. DPG Downloader Panel at Start Up | | ||
+ | </ | ||
+ | <WRAP center> | ||
- | {{: | + | | {{ {{ : |
- | | Figure 14 Fully Configured DPG Downloader Panel | + | |
+ | | Figure 14. Fully Configured DPG Downloader Panel | | ||
+ | </ | ||
7. Here is what you will see at the output of DAC0 on the Spectrum Analyzer. \\ \\ | 7. Here is what you will see at the output of DAC0 on the Spectrum Analyzer. \\ \\ | ||
+ | <WRAP center> | ||
- | + | | {{ {{ : | |
- | {{: | + | |
| Figure 15. DAC Output Spectrum Analyzer Display | | Figure 15. DAC Output Spectrum Analyzer Display | ||
+ | </ | ||
8. Here’s what you will see on DAC1, DAC2, and DAC3 on the scope. | 8. Here’s what you will see on DAC1, DAC2, and DAC3 on the scope. | ||
+ | <WRAP center> | ||
- | {{: | + | | {{ {{ : |
- | | Figure 16. DAC Outputs Scope Display | | + | | Figure 16. DAC Outputs Scope Display |
+ | </ | ||
===== ACE Software Features ===== | ===== ACE Software Features ===== |