This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad9152-fmc-ebz [14 Jul 2017 15:59] – Bailey Meyer | resources:eval:dpg:ad9152-fmc-ebz [27 Dec 2017 12:59] – Jay Chiang | ||
---|---|---|---|
Line 11: | Line 11: | ||
* Data Pattern Generator ADS7 | * Data Pattern Generator ADS7 | ||
===== Introduction ====== | ===== Introduction ====== | ||
- | The AD9152-FMC-EBZ connects to an ADS7 data pattern generator system. The AD9152 is a dual JESD204B signal processing RF Digital to Analog Converter. The ADS7 automatically formats the data and sends it to the AD9152-FMC-EBZ via its JESD204B lanes. The AD9152-FMC-EBZ is an FMC mezzanine card. +12V, +3.3V, and VADJ power supply rails are provided by the ADS7 system via the FMC connector P1. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a GBTCLK clock used by the ADS7. There is also an FMC standard I2C bus that is used by the ADS7 to identify the AD9144-FMC-EBZ. This I2C interface is implemented in software in the AD9152-FMC-EBZ PIC processor (XU1). All ADS7 to/from AD9152-FMC-EBZ interface signals are connected via the FMC connector P1. | + | The AD9152-FMC-EBZ connects to an ADS7 data pattern generator system. The AD9152 is a dual JESD204B signal processing RF Digital to Analog Converter. The ADS7 automatically formats the data and sends it to the AD9152-FMC-EBZ via its JESD204B lanes. The AD9152-FMC-EBZ is an FMC mezzanine card. +12V, +3.3V, and VADJ power supply rails are provided by the ADS7 system via the FMC connector P1. A clock distribution chip AD9516 is included on this EVB as a clock fan-out and frequency divider for the DACCLK, JESD204B SYSREF signals, and a GBTCLK clock used by the ADS7. There is also an FMC standard I2C bus that is used by the ADS7 to identify the AD9152-FMC-EBZ. This I2C interface is implemented in software in the AD9152-FMC-EBZ PIC processor (XU1). All ADS7 to/from AD9152-FMC-EBZ interface signals are connected via the FMC connector P1. |
===== AD9152 Evaluation Software ===== | ===== AD9152 Evaluation Software ===== | ||
The ACE application software, the preferred evaluation method for the AD9152, is included in the Evaluation Board software or can be downloaded from the ACE website at http:// | The ACE application software, the preferred evaluation method for the AD9152, is included in the Evaluation Board software or can be downloaded from the ACE website at http:// | ||
Line 91: | Line 91: | ||
| {{ : | | {{ : | ||
- | | Figure 9. AD9144-FMC-EBZ Fully Configured DPG Downloader Display | + | | Figure 9. AD9152-FMC-EBZ Fully Configured DPG Downloader Display |
</ | </ | ||
Line 126: | Line 126: | ||
<WRAP center> | <WRAP center> | ||
| {{ : | | {{ : | ||
- | | Figure 13. AD9144-FMC-EBZ Fully Configured DPG Downloader Display | + | | Figure 13. AD9152-FMC-EBZ Fully Configured DPG Downloader Display |
</ | </ | ||