This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9142a-m5372-ebz [15 Jun 2017 19:45] – Bailey Meyer | resources:eval:dpg:ad9142a-m5372-ebz [16 Jun 2017 16:02] (current) – Bailey Meyer | ||
---|---|---|---|
Line 34: | Line 34: | ||
If the board is connected properly, ACE will detect it and display it on the Start page under //Attached Hardware//. Double click this board. | If the board is connected properly, ACE will detect it and display it on the Start page under //Attached Hardware//. Double click this board. | ||
- | {{ : | + | {{ : |
<WRAP clear> | <WRAP clear> | ||
</ | </ | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
- | Ensure that the {{: | + | Ensure that the {{: |
- | {{ : | + | {{ : |
<WRAP clear> | <WRAP clear> | ||
</ | </ | ||
- | <WRAP centeralign> | + | <WRAP centeralign> |
2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1400MHz, and the output level to 6dBm. The spectrum analyzer can be configured with Center Frequency = 2050 MHz, Span = 200 MHz, and Resolution Bandwidth of 30 kHz. Choose Input Attenuation to be 24dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ | 2. Configure the hardware according to the hardware set-up instructions given in the Hardware Setup section above. Set the frequency of the DAC clock signal generator to 1400MHz, and the output level to 6dBm. The spectrum analyzer can be configured with Center Frequency = 2050 MHz, Span = 200 MHz, and Resolution Bandwidth of 30 kHz. Choose Input Attenuation to be 24dB. This can be adjusted later if indications are that the analyzer is causing degradations. \\ \\ | ||
3. Follow the sequence below to configure the AD9142A using ACE. \\ \\ | 3. Follow the sequence below to configure the AD9142A using ACE. \\ \\ | ||
- | a. Click | + | a. Click |
<WRAP column 40%> | <WRAP column 40%> | ||
Line 67: | Line 67: | ||
</ | </ | ||
- | b. Double click on the AD9142A component on the board diagram. This brings up the chip diagram. Set all the settings to match those in the chip diagram below, and click //Apply Changes//. Click //Read All// on the upper left of the page if the DLL is not enabled, as indicated by the green light next to //DLL Lock//. See the ACE Software Features section for more information about changing parameters. \\ \\ | + | b. Double click on the AD9142A component on the board diagram. This brings up the chip diagram. Set all the settings to match those in the chip diagram below, and click "Apply Changes." |
{{ : | {{ : | ||
Line 74: | Line 74: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | c. Open DPGDownloader. (Start > All Programs > Analog Devices > DPG > DPGDownloader). Ensure that the program detects the AD9142A, as indicated in the //Evaluation Board// drop-down list. For this evaluation board, LVDS is the only valid Port Configuration, | + | c. Open DPGDownloader. (Start > All Programs > Analog Devices > DPG > DPGDownloader). Ensure that the program detects the AD9142A, as indicated in the "Evaluation Board" |
{{ : | {{ : | ||
Line 81: | Line 81: | ||
<WRAP centeralign> | <WRAP centeralign> | ||
- | d. Click on //Add Generated Waveform//, and then //Single Tone//. A Single Tone panel will be added to the vector list. Enter the sample rate, in this case 350 MHz and the desired frequency, 50MHz. Enter the digital amplitude. In this case, use -14dBFS. Check the //Generate Complex Data (I & Q)// box and uncheck the //Unsigned Data// box. Select the In-Phase data vector in the //I Data Vector// drop down menu and the Quadrature data vector in the //Q Data Vector//. This should match the image above. \\ \\ | + | d. Click on "Add Generated Waveform," |
e. Click Download ({{: | e. Click Download ({{: | ||
4. The current on the 5V supply should read about 1310mA. \\ | 4. The current on the 5V supply should read about 1310mA. \\ |