This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:dpg:ad9136-fmc-ebz [12 Aug 2022 12:03] – [Quick Start Guide] Shine Cabatan | resources:eval:dpg:ad9136-fmc-ebz [11 Oct 2022 13:55] – [Quick Start Guide] Shine Cabatan | ||
---|---|---|---|
Line 63: | Line 63: | ||
- Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output.< | - Set the frequency of the continuous waveform generator output to **2.0 GHz** and the output level to **+3 dBm**. Enable the output.< | ||
- Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | ||
- | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/ | + | - Open ACE. The board will automatically be recognized by the software. Otherwise, install the plugin for AD9135/ |
- In ACE, apply the configuration wizard settings enumerated below and shown in Figure 5. JESD204B PLL should lock and the indicator should turn green. | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 5. JESD204B PLL should lock and the indicator should turn green. | ||
* **Links:** Dual Link | * **Links:** Dual Link | ||
Line 70: | Line 70: | ||
* **Interpolation: | * **Interpolation: | ||
* **DAC PLL:** False | * **DAC PLL:** False | ||
- | * **FDAC:** 2 GHz | + | * **FDAC:** 2 GHz<WRAP centeralign> |
- In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows: | - In DPG Lite or DPG Downloader, configure generation of two single tone waveforms. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Do this two times then configure the panels as follows: | ||
* **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels. | * **Data Rate** = 2 GHz, **Amplitude** = -1dBFS, **Unsigned Data** is unchecked for both panels. | ||
* **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other. | * **Desired Frequency = 112 MHz** in one panel while **Desired Frequency = 221 MHz** in the other. | ||
* If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits). | * If using AD9135, set **DAC Resolution** to **11 bits**. Otherwise, leave as is (16 bits). | ||
- | - In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. <WRAP centeralign> | + | - In the ADS7-V2 or ADS8-V1 panel in the DPG window, configure **Data Playback** by selecting tone2 for DAC0 and tone1 for DAC1. Set **JESD Mode** to Mode 8, **Links** to Dual, and **Subclass** to 1. <WRAP centeralign> |
- | - Press the download arrow ({{: | + | - Press the download arrow ({{: |