This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ad9129-cbltx-ebz [28 Sep 2012 23:19] – [Initial Set-Up] Dan Fague | resources:eval:dpg:ad9129-cbltx-ebz [05 Feb 2013 18:28] (current) – Added the AD9119-CBLTX-EBZ Dan Fague | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ~~UNDERCONSTRUCTION~~ | + | ====== |
- | ====== AD9129-CBLTX-EBZ Cable Transmitter Evaluation Board Quick Start Guide ====== | + | ===== Getting Started with the AD9119/AD9129 Cable Transmitter Evaluation Board and Software ===== |
- | ===== Getting Started with the AD9129 Cable Transmitter Evaluation Board and Software ===== | + | |
==== What's in the Box ==== | ==== What's in the Box ==== | ||
- | * AD9129-CBLTX-EBZ Evaluation Board | + | * AD9119-CBLTX-EBZ or AD9129-CBLTX-EBZ Evaluation Board |
* Mini-USB Cable | * Mini-USB Cable | ||
* Evaluation Board CD | * Evaluation Board CD | ||
Line 11: | Line 10: | ||
* Spectrum Analyzer Ex: Agilent PXA or Rohde Schwarz FSU | * Spectrum Analyzer Ex: Agilent PXA or Rohde Schwarz FSU | ||
===== Introduction ===== | ===== Introduction ===== | ||
- | The AD9129-CBLTX-EBZ connects to a DPG2 to allow for quick evaluation of the AD9129, a high-speed, RF Digital to Analog converter (RF DAC). The DPG2 automatically formats the data and sends it to the AD9129-CBLTX-EBZ, | + | The AD9119-CBLTX-EBZ and AD9129-CBLTX-EBZ are built from the same printed circuit board, with the only difference being which DAC device is loaded, the AD9119 or the AD9129. This Quick Start Guide will describe the set-up of the AD9129-CBLTX-EBZ, |
+ | |||
+ | The AD9129-CBLTX-EBZ connects to a DPG2 to allow for quick evaluation of the AD9129, a high-speed, RF Digital to Analog converter (RF DAC). The DPG2 automatically formats the data and sends it to the AD9129-CBLTX-EBZ, | ||
===== AD9129 Evaluation Software ===== | ===== AD9129 Evaluation Software ===== | ||
The AD9129 Evaluation Board software has an easy-to-use graphical user interface (GUI). It is included on the Evaluation Board CD, or can be downloaded from the DPG Web site at http:// | The AD9129 Evaluation Board software has an easy-to-use graphical user interface (GUI). It is included on the Evaluation Board CD, or can be downloaded from the DPG Web site at http:// | ||
Line 18: | Line 19: | ||
- | < | + | < |
{{: | {{: | ||
</ | </ | ||
- | < | + | < |
{{ : | {{ : | ||
</ | </ | ||
<WRAP clear> | <WRAP clear> | ||
</ | </ | ||
- | < | + | < |
Figure 1 - Block diagram of the AD9129 lab bench set-up | Figure 1 - Block diagram of the AD9129 lab bench set-up | ||
</ | </ | ||
- | < | + | < |
Figure 2 - Top view of AD9129-CBLTX-EBZ Evaluation Board | Figure 2 - Top view of AD9129-CBLTX-EBZ Evaluation Board | ||
</ | </ |