This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Next revisionBoth sides next revision | ||
resources:eval:dpg:ad9122-ebz [07 May 2018 18:46] – [Hardware Setup (DAC OUTPUT)] Annette Hurman | resources:eval:dpg:ad9122-ebz [09 May 2018 17:22] – [Generating a Test Vector with ACE] Annette Hurman | ||
---|---|---|---|
Line 48: | Line 48: | ||
==== Generating a Test Vector with ACE ==== | ==== Generating a Test Vector with ACE ==== | ||
1. Power up the DPG and connect the USB cable to the PC.\\ \\ | 1. Power up the DPG and connect the USB cable to the PC.\\ \\ | ||
- | 2. Next, run the DPGDownloader Software. To launch DPGDownloader,, | + | 2. Next, run the DPGDownloader Software. To launch DPGDownloader,, |
3. Generate a sine wave by pulling down the “Add Generated Waveform” menu and choosing “Single Tone”. Fill in the form as shown below (Sample Rate = 250MHz, Desired Frequency = 29 MHz, etc.). Note that the Sample Rate should match the input sample rate and not the DAC update rate.\\ \\ | 3. Generate a sine wave by pulling down the “Add Generated Waveform” menu and choosing “Single Tone”. Fill in the form as shown below (Sample Rate = 250MHz, Desired Frequency = 29 MHz, etc.). Note that the Sample Rate should match the input sample rate and not the DAC update rate.\\ \\ | ||
{{ : | {{ : |