This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionNext revisionBoth sides next revision | ||
resources:eval:dpg:ad9122-ebz [23 Oct 2017 17:05] – [Recommended Equipment] Janet Dephoure | resources:eval:dpg:ad9122-ebz [23 Apr 2018 19:05] – [Software Installation] Annette Hurman | ||
---|---|---|---|
Line 1: | Line 1: | ||
- | ====== AD9122 Evaluation Board Quick Start Guide ====== | + | ====== |
- | ===== Getting Started with the AD9122 Evaluation Board ===== | + | ===== Getting Started with the AD9121/AD9122 Evaluation Board ===== |
==== What's in the Box ==== | ==== What's in the Box ==== | ||
* AD9122-M5375-EBZ or AD9122-M5372-EBZ Evaluation Board | * AD9122-M5375-EBZ or AD9122-M5372-EBZ Evaluation Board | ||
* Mini-USB Cable | * Mini-USB Cable | ||
- | * AD9122 Evaluation Board CD | + | * AD9121/AD9122 Evaluation Board CD |
==== Recommended Equipment ==== | ==== Recommended Equipment ==== | ||
* Digital Pattern Generator Series 2 or 3 (DPG): ADI HSC-DAC-DPG-BZ OR System Demonstration Platform( SDP-H1) and FMC to High-Speed DAC Evaluation Board Adaptor(AD-DAC-FMC-ADP) | * Digital Pattern Generator Series 2 or 3 (DPG): ADI HSC-DAC-DPG-BZ OR System Demonstration Platform( SDP-H1) and FMC to High-Speed DAC Evaluation Board Adaptor(AD-DAC-FMC-ADP) | ||
Line 13: | Line 13: | ||
* PC: Windows PC with 2 or more USB ports | * PC: Windows PC with 2 or more USB ports | ||
==== Introduction ==== | ==== Introduction ==== | ||
- | The AD9122 Evaluation Board connects to the Analog Devices Digital Pattern Generator (DPG) to allow for quick evaluation of the AD9122. The DPG allows the user to create many types of digital vectors and transmit these at speed to the AD9122 in any of the AD9122 operating modes. The AD9122 evaluation board is configured over USB with accompanying PC software. | + | The AD9121/AD9122 Evaluation Board connects to the Analog Devices Digital Pattern Generator (DPG) or System Demonstration Platform (SDP-H1, PN: EVAL-SDP-CH1Z) to allow for quick evaluation of the AD9121/AD9122. The DPG or SDP-H1 |
==== Software Installation ==== | ==== Software Installation ==== | ||
- | The DAC Software Suite plus AD9122 Update should be installed on the PC prior connecting the hardware to the PC. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at https:// | + | The DAC Software Suite plus AD9121/AD9122 Update should be installed on the PC prior to connecting the hardware to the PC. The DAC Software Suite is included on the Evaluation Board CD, or can be downloaded from the DPG web site at https:// |
- | ==== Hardware Setup ==== | + | ==== Hardware Setup (DAC OUTPUT) |
- | Once DPGDownloader is installed, the hardware can be connected as shown below. A single 5V power supply powers the evaluation board. The power supply should be able to source up to 2A to cover all of the board’s operating conditions. A low jitter clock source (< 0.5psec RMS) should be used for the DACCLK. A sinusoidal clock output level of 0 to 4dBm is optimal. By default, the DAC outputs are connected to SMA connectors for evaluation. Both DAC outputs are available. Later in document, the modifications for observing the modulator output and different clocking options will be shown. The evaluation board plugs directly into the DPG. The PC connects to both the DPG and the evaluation board through USB cables. | + | Once the DPGDownloader |
- | ^ Equipment | + | * The evaluation board plugs directly into the DPG2 or DPG3. |
- | | Power Supply | + | The PC connects to both the DPG2 and the evaluation board through USB cables |
- | | Signal Source | + | * The evaluation boards plugs into the AD-DAC-FMC-ADP adapter board that plugs into the SDP-H1. |
- | | PC USB Cable | + | The PC connects to both the SDP-H1 and the evaluation board through USB cables as shown in Figure 3 and Figure 4. |
- | | Spectrum Analyzer | + | |
- | | DPG2 | + | {{ : |
- | {{: | + | Figure 1. DPG2 and AD9122 Evaluation Board Bench set-up |
+ | {{ : | ||
+ | Figure 2. DPG2 and AD9122 Evaluation Board | ||
+ | {{ : | ||
+ | Figure 3. SDP-H1 and AD9122 Evaluation Board Bench set-up | ||
+ | {{ : | ||
+ | Figure 4. SDP-H1 and AD9122 Evaluation Board | ||
+ | |||
+ | ===== BASIC HARDWARE SETUP ===== | ||
+ | Connect the equipment to the AD9122 evaluation board per the following table: | ||
+ | * Equipment Connects to AD9122 Eval Board | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | | ||
+ | * SDP-H1 J4(FMC connector) | ||
===== Getting Started ===== | ===== Getting Started ===== | ||
- | It is suggested that the basic set-up | + | It is suggested that the basic set-up |
==== Generating a Test Vector with ACE ==== | ==== Generating a Test Vector with ACE ==== | ||
Line 52: | Line 69: | ||
==== Generating a Test Vector with the SPI Controller ==== | ==== Generating a Test Vector with the SPI Controller ==== | ||
- | Launch the AD9122 SPI GUI by clicking the AD9122 SPI button. | + | Launch the AD9122 SPI GUI by clicking the AD9122 SPI button.\\ \\ |
1. Power up the DPG and connect the USB cable to the PC.\\ \\ | 1. Power up the DPG and connect the USB cable to the PC.\\ \\ | ||
2. Next, run the DPGDownloader Software. To launch DPGDownloader,, | 2. Next, run the DPGDownloader Software. To launch DPGDownloader,, |