Wiki

Differences

This shows you the differences between two versions of the page.

Link to this comparison view

Both sides previous revisionPrevious revision
resources:eval:dpg:ad9119-mix-ebz [15 Oct 2012 17:04] – removing under construction tag Dan Fagueresources:eval:dpg:ad9119-mix-ebz [02 Nov 2012 20:38] (current) – [Mix-Mode Operation] Dan Fague
Line 18: Line 18:
  
  
-<WRAP col2 50%>+<WRAP column 40%>
 {{:resources:eval:dpg:ad9129:bench_setup_9119_evb.png?350 |}}  {{:resources:eval:dpg:ad9129:bench_setup_9119_evb.png?350 |}} 
 </WRAP> </WRAP>
-<WRAP right 50%>+<WRAP column 55%>
 {{:resources:eval:dpg:ad9129:figure2_9129-MIX-EBZ.png?400 |}}  {{:resources:eval:dpg:ad9129:figure2_9129-MIX-EBZ.png?400 |}} 
 </WRAP> </WRAP>
 <WRAP clear> <WRAP clear>
 </WRAP> </WRAP>
-<WRAP col2 50%>+<WRAP column 40%>
 Figure 1 - Block diagram of the AD9119 lab bench set-up Figure 1 - Block diagram of the AD9119 lab bench set-up
 </WRAP> </WRAP>
-<WRAP right 50%>+<WRAP column 55%>
 Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB) Figure 2 - Top view of AD9119-MIX-EBZ Evaluation Board (uses the AD9129 EVB)
 </WRAP> </WRAP>
Line 118: Line 118:
 When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents.  When using mix-mode and targeting a signal to the second Nyquist zone, it is important to remember that the center frequency chosen in the DPG window is the offset from the DACCLK sample frequency, not 0 Hz. For example, to place the carrier at 1982.5 MHz with a 2.4576 GHz DACCLK as in Figure 12, program the DPG Downloader center frequency to 475 MHz and enable mix-mode. Figure 12 shows the IMD performance of several different DAC output currents and the loss in output power expected with lower currents. 
  
-<WRAP col2 50%> {{:resources:eval:dpg:ad9129:figure12b_9129-MIX-EBZ.png?400 |}}+<WRAP column 48%> {{:resources:eval:dpg:ad9129:figure12b_9129-MIX-EBZ.png?400 |}}
 </WRAP> </WRAP>
-<WRAP right 50%> {{:resources:eval:dpg:ad9129:figure12a_9129-MIX-EBZ.png?400 |}}+<WRAP column 48%> {{:resources:eval:dpg:ad9129:figure12a_9129-MIX-EBZ.png?400 |}}
 </WRAP> </WRAP>
 <WRAP clear> <WRAP clear>
resources/eval/dpg/ad9119-mix-ebz.1350313483.txt.gz · Last modified: 15 Oct 2012 17:04 by Dan Fague