This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision | ||
resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 08:15] – Removed ADS8 Shine Cabatan | resources:eval:dpg:ace_ad9144-fmc-ebz [12 Aug 2022 11:51] – old revision restored (12 Aug 2022 11:46) Shine Cabatan | ||
---|---|---|---|
Line 34: | Line 34: | ||
* [[adi> | * [[adi> | ||
- | <note important> | + | <note important> |
+ | * Do not install ACE on a computer with DAC Software Suite. | ||
+ | * **Known Issue:** ACE may fail to detect HS-DAC boards, details [[resources: | ||
+ | </ | ||
===== Hardware Needed ===== | ===== Hardware Needed ===== | ||
Line 51: | Line 54: | ||
===== Quick Start Guide ===== | ===== Quick Start Guide ===== | ||
- | - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/ | + | - Attach AD9144-FMC-EBZ onto the FMC connector of ADS7-V2 controller board. Connect the evaluation board to PC via USB, the continuous waveform generator output to J1, and one of the DAC outputs (J4/ |
- Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | - Set the frequency of the continuous waveform generator output to **1.5 GHz** and the output level to **+3 dBm**. Enable the output. <WRAP centeralign> | ||
- Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | - Start DPG Lite or DPG Downloader. A panel named after the detected controller board should appear at the bottom of the DPG window. The device on the evaluation board and the data interface should also be automatically detected by the software and shown at **Evaluation Board** and **Port Configuration**, | ||
- | - Open ACE. The board will automatically be recognized by the software as shown in Figure 3. Otherwise, install the plugin for AD9144 evaluation board by following the steps in this page: [[: | + | - Open ACE. The board will automatically be recognized by the software as shown in Figure 3. Otherwise, install the plugin for AD9144 evaluation board by following the steps in this page: [[: |
- In ACE, apply the configuration wizard settings enumerated below and shown in Figure 4. JESD204B PLL should lock and the indicator should turn green. | - In ACE, apply the configuration wizard settings enumerated below and shown in Figure 4. JESD204B PLL should lock and the indicator should turn green. | ||
* **Links:** Single Link | * **Links:** Single Link | ||
Line 61: | Line 64: | ||
* **Interpolation: | * **Interpolation: | ||
* **DAC PLL:** False | * **DAC PLL:** False | ||
- | * **FDAC:** 1.5 GHz <WRAP centeralign> | + | * **FDAC:** 1.5 GHz <WRAP centeralign> |
- In DPG Lite or DPG Downloader, configure single tone waveform generation. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Apply the following settings: | - In DPG Lite or DPG Downloader, configure single tone waveform generation. From the **Add Generator Waveforms** pulldown menu, select **Single Tone**. Apply the following settings: | ||
* **Data Rate:** 750 MHz | * **Data Rate:** 750 MHz | ||
Line 67: | Line 70: | ||
* **DAC Resolution: | * **DAC Resolution: | ||
* **Amplitude: | * **Amplitude: | ||
- | * **Unsigned Data: | + | * **Unsigned Data: |
* **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status> | * **Generate Complex Data (I & Q):** checked <insert DPG screenshot with lane rate and synced status> | ||
- | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign> | + | - In the ADS7-V2 panel in the DPG window, configure **Data Playback** by selecting tones for the DAC outputs from each dropdown menu. Set **JESD Mode** to Mode 0, **Links** to Single, and **Subclass** to 0.<WRAP centeralign> |
- | - Press the download arrow ({{: | + | - Press the download arrow ({{: |