This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | |||
resources:eval:dpg:ace_ad9144-ebz [18 Mar 2016 21:01] – [Introduction] Michele Viani | resources:eval:dpg:ace_ad9144-ebz [18 Mar 2016 21:03] (current) – [AD9144 Evaluation Software] Michele Viani | ||
---|---|---|---|
Line 15: | Line 15: | ||
The AD9144-EBZ connects to a DPG3 for quick evaluation of the [[adi> | The AD9144-EBZ connects to a DPG3 for quick evaluation of the [[adi> | ||
===== AD9144 Evaluation Software ===== | ===== AD9144 Evaluation Software ===== | ||
- | The AD9144 Evaluation Board software | + | The AD9144 Evaluation Board software |
===== Hardware Setup ===== | ===== Hardware Setup ===== | ||
Connect +5.0V to P5, GND to P6. A low phase noise high frequency clock source should be connected to the SMA connector, J1. This is the DACCLK input. The spectrum analyzer should be connected to the SMA connector, J4. A +1.0V power supply must be connected to the VTT probe point near SMA connector J9, along with a GND connection to the GND probe point next to it. The evaluation board connects to the DPG3 through the connectors P4. The PC should be connected to the EVB using the mini-USB connector XP2 after installation of the Evaluation Board software. Figure 1 shows the block diagram of the set-up. | Connect +5.0V to P5, GND to P6. A low phase noise high frequency clock source should be connected to the SMA connector, J1. This is the DACCLK input. The spectrum analyzer should be connected to the SMA connector, J4. A +1.0V power supply must be connected to the VTT probe point near SMA connector J9, along with a GND connection to the GND probe point next to it. The evaluation board connects to the DPG3 through the connectors P4. The PC should be connected to the EVB using the mini-USB connector XP2 after installation of the Evaluation Board software. Figure 1 shows the block diagram of the set-up. |