This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:dpg:ace_ad9144-ebz [18 Mar 2016 20:58] – [AD9144-EBZ Evaluation Board Quick Start Guide Using ACE (Analysis|Control|Evaluate) Software] Michele Viani | resources:eval:dpg:ace_ad9144-ebz [18 Mar 2016 21:03] (current) – [AD9144 Evaluation Software] Michele Viani | ||
---|---|---|---|
Line 14: | Line 14: | ||
===== Introduction ====== | ===== Introduction ====== | ||
The AD9144-EBZ connects to a DPG3 for quick evaluation of the [[adi> | The AD9144-EBZ connects to a DPG3 for quick evaluation of the [[adi> | ||
+ | ===== AD9144 Evaluation Software ===== | ||
+ | The AD9144 Evaluation Board software runs on the easy-to-use ACE (Analysis|Control|Evaluate) graphical user interface (GUI). It is included on the Evaluation Board CD. Registers on the AD9144 and AD9516 products are programmed via a USB cable connecting the user’s PC to the AD9144-EBZ XP2 connector. Software in the AD9144-EBZ PIC processor (XU1) provides the interface between the USB bus and the SPI busses of the AD9144 and AD9516. | ||
+ | ===== Hardware Setup ===== | ||
+ | Connect +5.0V to P5, GND to P6. A low phase noise high frequency clock source should be connected to the SMA connector, J1. This is the DACCLK input. The spectrum analyzer should be connected to the SMA connector, J4. A +1.0V power supply must be connected to the VTT probe point near SMA connector J9, along with a GND connection to the GND probe point next to it. The evaluation board connects to the DPG3 through the connectors P4. The PC should be connected to the EVB using the mini-USB connector XP2 after installation of the Evaluation Board software. Figure 1 shows the block diagram of the set-up. | ||
+ | <WRAP center> | ||
+ | |||
+ | | {{: | ||
+ | | Figure 1. Block diagram of the AD9144 lab bench set-up | ||
+ | </ | ||