This is an old revision of the document!
This page will detail the prototype hardware that ADI is developing to prove out and prototype this reference design. The hardware is composed of 2 main platforms:
Each platform is composed of 4 primary pieces of hardware:
Additional pieces of hardware will be needed, such as cables, test equipment and power supplies.
With these 4 key pieces of hardware, the full signal chain (including Digitizer) can be evaluated for functionality and performance. Additionally, all control of the signal chain is conducted from a central location (FPGA on the ZCU102), which allows for coordinated control system prototyping.
Below is a diagram showing how these pieces will fit together to complete the prototyping system.