This is an old revision of the document!
The DC2872A is an evaluation board for demonstrating the performance and ease of use of the LTM2985, an isolated 10-channel temperature measurement system on a chip, software compatible with the LTC2986-1. It provides 5kV isolated power and SPI interface to the precision temperature-to-bits converter.
The DC2872A is designed to allow easy evaluation of the LTM2985 and may be connected to any one of the sensor daughter boards.
These daughter boards allow evaluation of the various sensors the LTM2985 supports. For the serial digital interface, the DC2872A may be connected to the DC2026 Linduino® One.
Reference Designator | Quantity | Description | Comments |
---|---|---|---|
VCC | 1 | Isolated Analog Power Supply | Installed |
GND | 3 | Circuit Ground | 1 installed, 2 DNI |
CS_N | 1 | Serial SPI Chip Select | DNI |
SCK | 1 | Serial SPI Clock Input | DNI |
SDI | 1 | Serial SPI Data Input | DNI |
SDO | 1 | Serial SPI Digital Output | DNI |
DOUT | 1 | Digital Output | DNI |
VCC2 | 1 | 5V Nominal Isolated Supply Voltage | Installed |
GND2 | 2 | Isolated Ground | 1 installed, 1 DNI |
VREF | 1 | Reference output pin | Installed |
INT | 1 | Interrupt | DNI |
DIN | 1 | Digital Input | DNI |
P1 | 1 | 2-pin header for shorting INT and DIN | Installed |
Figure 1: DC2872A connected to a daughter board and DC2026C (Linduino)
The demo software helps program and run the LTM2985. It can configure, check and save the configuration, run the LTM2985, output the results into
a file, and even create Linduino ready C code based on the configuration. Refer to software manual LTC2986-LTM2985DSM for more detailed information.
Figure 2: LTM2985 Demo Software
Because the daughter boards are connected to the isolated side of the LTM2985, the LTM2985 demo software can't read the daughter board's EEPROM
contents for its address and the precise value of some sense resistors stored there upon test. This is the reason for the note on the LTC2986-LTM2985DSM
saying that the section on Loading The Configuration from a Daughter Board only applies to the LTC2986 and LTC2986-1.
Figure 3: DC2211 Universal Temperature Measurement Board
The universal temperature measurement board allows the user to connect any of the LTM2985 supported sensors to the DC2872A demo board.
It has a built-in sense resistor for RTD applications as well as a cold junction sensor diode for thermocouple applications. The sense resistor
is a 2kΩ ±0.1% 10ppm/°C sense resistor on channels 1 and 2 which may be used with any of the supported RTD sensor types.
The external interface on the universal temperature measurement board is an 8-position screw-terminal block with the flowing pinout.
DC2211 Terminal Connector Pinout
Position | Connection |
---|---|
Position A | LTM2985 CH2 as well as the low side of the on-board 2k sense resistor |
Position B | LTM2985 CH3 |
Position C | LTM2985 CH4 |
Position D | LTM2985 CH5 |
Position E | Common/Ground Connection |
Position F | Common/Ground Connection |
Position G | Common/Ground Connection |
Position H | Common/Ground Connection |
DC2211 Schematics and Design Files
Figure 4: DC2212 Thermocouple Daughter Board
The thermocouple board demonstrates the flexibility, accuracy, and low noise features of the LTM2985 thermocouple modes.
If the user wishes to connect external sensors to the thermocouple board, two universal-type thermocouple
jacks (J2 and J3) are available. The user
may connect any of the LTM2985 supported thermocouples (B, E, J, K, N, R, S, or T) as well as custom thermocouples through these jacks.
To demonstrate the flexibility of the LTM2985, the thermocouple board includes cold junction diodes (Q1 and Q2) embedded in each thermocouple
socket. Alternatively, a 4-wire PT100 RTD (R5) can be used as the cold junction sensor for either or both thermocouples.
To demonstrate the low system noise and offset of the LTM2985, the thermocouple board provides a short to ground on channel 5.
To demonstrate the accuracy of the LTM2985, the thermocouple board allows the user to connect a thermocouple
calibrator or an external voltage
source to CH10 of the LTM2985 through a pair of banana jacks (J4 and J5).
DC2212 Schematics and Design Files
Figure 5: DC2213 Dedicated RTD Board
The DC2213 dedicated RTD board demonstrates the flexibility, accuracy, and low noise features of the LTM2985 RTD sensor modes. The DC2213
provides several circuits demonstrating the features of the LTM2985.
The DC2213 provides a 2kΩ ±0.1% 10ppm/°C sense resistor on channels 2 and 3 which may be used with any of the RTD sensor circuits on this
board. An additional Kelvin connection is also provided to this sense resistor on channel 1.
To demonstrate the low system noise of the LTM2985, the dedicated RTD board provides a 0°C PT100 simulator (100Ω ±0.01% 10ppm/°C)
on channels 3 to 6 configured as a 4-wire sensor. In addition to this the user may use this
circuit to demonstrate how the rotated mode eliminates
measurement error introduced by parasitic thermocouples.
To facilitate this measurement, the DC2213 provides an external thermocouple interface
which acts as a parasitic
thermocouple.
To see the effects of parasitic thermocouples on non-rotated measurement modes, first measure the on-board 0°C
PT100 simulator in a non-rotated
configuration and see the measurement error as the thermocouple’s temperature
changes. To see the benefit of the rotated measurement mode, switch
from the no rotation/sharing to the rotation/
sharing configuration and see the errors introduced by the parasitic thermocouple minimized.
If the user wishes to connect an external RTD to the sensor board, a 4-position terminal block is provided. The user may connect any of the LTM2985
supported RTDs as well as custom RTDs to the DC2872A demo board through this
interface. The interface may be configured for 3 or 4 wire sensors.
To demonstrate the accuracy of the LTM2985,
the user may also connect an RTD calibrator or precision resistors to this interface.
DC2213 Schematics and Design Files
Figure 6: DC2214 Thermistor Daughter Board
The DC2214 dedicated thermistor board includes several circuits to demonstrate the flexibility, accuracy,
and low noise features of the LTM2985
thermistor sensor modes.
The DC2214 provides a 10kΩ ±0.1% 15ppm/°C sense
resistor on channels 1 and 2 which is shared with all of the thermistor sensor circuits
on this board.
To demonstrate the low system noise of the LTM2985 the dedicated thermistor board provides a 25°C 10k thermistor simulator (10kΩ ±0.1% 15ppm/°C)
on channels 2-4 configured as a differential sensor. In addition to this the user may use this circuit to demonstrate how the rotated mode eliminates
measurement error introduced by
parasitic thermocouples. To facilitate this demonstration the DC2214 provides an external thermocouple interface
which acts as a parasitic thermocouple.
To see the effects of parasitic thermocouples on nonrotated measurement modes, first measure the on-board
25°C 10k thermistor simulator in a
no-rotation/sharing configuration and see the measurement error as the
thermocouple’s temperature changes. To see the benefit of the
rotated measurement mode, switch to the rotation/
sharing configuration and see the errors introduced by the parasitic thermocouple disappear (the
effects are more
significant with lower excitation current).
The DC2214 also includes a 499kΩ (0.1% 15ppm/°C) thermistor simulator on channels 9 and 10. Ideally, this
resistor simulates –30.59°C for a
44008 (30k) thermistor and –51.94°C for a 44006 (10k) thermistor. Note, the 10k
thermistor reports the temperature, but also indicates a soft fault since
the temperature is below the thermistor’s specified minimum temperature. In addition to the fixed value thermistor simulators, there is a variable resistor
thermistor simulator as well. This circuit can be used to demonstrate the range of the various LTM2985 thermistor sensor modes as well as demonstrate
the fault detection capabilities of the LTM2985.
If the user wishes to connect an external thermistor to the daughter board, a 2-position terminal block is provided. The user may connect any of the
LTCM2985 supported thermistors as well as custom thermistors to the DC2872A demo board through this interface. To demonstrate the accuracy of
the LTM2985, the user may connect external resistance standards to this interface.
DC2214 Schematics and Design Files
Figure 7: DC2210 Experimenter Board
The DC2210 experimenter board brings all LTM2985 channels plus the COM connection out to a proto area and a 24-position terminal block. The
user may connect any of the supported sensors and sense resistors
to any of the LTM2985 inputs in this area. Please note that only CH1 to CH10
are valid on the DC2210 when used in conjunction with the DC2872A.
DC2210 Schematics and Design Files (part of LTC2986-1 Kit, cannot be bought standalone)