Differences
This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision |
resources:eval:ads7-v1 [31 Oct 2014 19:10] – Add link to www.analog.com Robin Getz | resources:eval:ads7-v1 [06 Mar 2015 22:13] – [Preface] Jiayuan Wang |
---|
====== ADS7-V1EBZ HIGH SPEED EVALUATION BOARD ====== | ====== ADS7-V1EBZ HIGH SPEED EVALUATION BOARD ====== |
===== Preface ===== | ===== Preface ===== |
The [[adi>en/content/CU_High-Speed_ADC_FIFO_evaluation_tools/fca.html#ADS7-V1|ADS7-V1]] Evaluation Board was developed to support the evaluation of Analog Devices high speed A/D converters, D/A converters and Transceivers with JESD204B bit rates up to 12.5 Gbps. This Wiki site provides a high level overview of the platform. In addition, each use case of the board has its own section (e.g. using Using the ADS7-V1 for HIgh Speed A/D Converter Evaluation). The ADS7-V1 is intended to be used only with specified Analog Devices Evaluation Boards. The ADS7-V1 is not intended to be used as a development platform, and no support is available for standalone operation. Please refer to Xilinx and its approved distribuitors for FPGA Development Kits.\\ | The [[adi>en/content/CU_High-Speed_ADC_FIFO_evaluation_tools/fca.html#ADS7-V1|ADS7-V1]] Evaluation Board was developed to support the evaluation of Analog Devices high speed A/D converters, D/A converters and Transceivers with JESD204B bit rates up to 12.5 Gbps. This Wiki site provides a high level overview of the platform. In addition, each use case of the board has its own section (e.g. Using the ADS7-V1 for HIgh Speed A/D Converter Evaluation). The ADS7-V1 is intended to be used only with specified Analog Devices Evaluation Boards. The ADS7-V1 is not intended to be used as a development platform, and no support is available for standalone operation. Please refer to Xilinx and its approved distribuitors for FPGA Development Kits.\\ |
\\ | \\ |
| |