Both sides previous revisionPrevious revisionNext revision | Previous revisionLast revisionBoth sides next revision |
resources:eval:ad9864_ad9874-eval_platform [16 Dec 2015 16:10] – Paul Hendriks | resources:eval:ad9864_ad9874-eval_platform [14 Jan 2021 05:11] – user interwiki links Robin Getz |
---|
====== AD9864EBZ and AD9874EBZ Demo and Evaluation Platform====== | ====== AD9864EBZ and AD9874EBZ Demo and Evaluation Platform====== |
===== Summary ===== | ===== Summary ===== |
This wiki site includes information about the [[adi>adAD9864|AD9864]] and [[adi>AD9874|AD9874]] evaluation boards. Both boards use the same software and are equivalent in all respect other than the IC version used to populate it. The AD9864 and AD9874 datasheets provide a significant amount of information to aid in the understanding of these narrow band IF receivers. The datasheet along with the user guide and other PCB related files provided here should be consulted when using the evaluation board. The AD9864/AD9874EBZ is compatible with the ADI [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] FPGA-Based Data Capture Kit. The user guide describes the AD9864_74 evaluation board along with the SPI GUI and Visual Analog software used to configure and analyze the data output of the device. | This wiki site includes information about the [[adi>AD9864|AD9864]] and [[adi>AD9874|AD9874]] evaluation boards. Both boards use the same software and are equivalent in all respect other than the IC version used to populate it. The AD9864 and AD9874 datasheets provide a significant amount of information to aid in the understanding of these narrow band IF receivers. The datasheet along with the user guide and other PCB related files provided here should be consulted when using the evaluation board. The AD9864/AD9874EBZ is compatible with the ADI [[adi>hsadcevalboard|HSC-ADC-EVALCZ]] FPGA-Based Data Capture Kit. The user guide describes the AD9864_74 evaluation board along with the SPI GUI and Visual Analog software used to configure and analyze the data output of the device. |
| |
| |
Any questions can be submitted via Analog Device's [[https://ez.analog.com/welcome|EZONE]]. | Any questions can be submitted via Analog Device's [[ez>welcome|EZONE]]. |
| |
\\ | \\ |
\\ | \\ |
===== Helpful Links ===== | ===== Helpful Links ===== |
* [[adi>AD9864|AD9864]]and [[adi>AD9874|AD9874]] data sheet ([[http://www.analog.com/en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HSC-ADC-EVALCZ.html#eb-overview|HSC-ADC-EVALCZ]]) | * [[adi>AD9864|AD9864]]and [[adi>AD9874|AD9874]] data sheet ([[adi>en/design-center/evaluation-hardware-and-software/evaluation-boards-kits/EVAL-HSC-ADC-EVALCZ.html#eb-overview|HSC-ADC-EVALCZ]]) |
* High Speed ADC Capture Evaluation Kit Rev C | * High Speed ADC Capture Evaluation Kit Rev C |
* [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/dbconvert.html|VRMS / dBm / dBu / dBV Calculator]] | * [[adi>en/design-center/advanced-selection-and-design-tools/interactive-design-tools/dbconvert.html|VRMS / dBm / dBu / dBV Calculator]] |
* [[adi>designtools/en/rfimpd/Default.aspx|ADI RF Impedance Matching Tool]] | * [[adi>en/design-center/interactive-design-tools/rf-impedance-matching-calculator.html|ADI RF Impedance Matching Tool]] |
* [[https://form.analog.com/form_pages/rfcomms/adisimrf.aspx|ADIsimRF Software]] | * [[https://form.analog.com/form_pages/rfcomms/adisimrf.aspx|ADIsimRF Software]] |
| |
| |
===== AD9864/AD9874 Evaluation Platform User Guides ===== | ===== AD9864/AD9874 Evaluation Platform User Guides ===== |
[[ftp://ftp.analog.com/pub/HSC_ADC_Apps/AD9864_AD9874_Evaluation_Platform|User Guide for the AD9864/AD9874]] \\ | {{:resources:eval:user-guides:ad9864_ad9874_users_guide.pdf|Users Guide for the AD9864/AD9874[pdf file]}} |
| |
\\ | \\ |
\\ | \\ |
===== Evaluation Board PCB Files ===== | ===== Evaluation Board PCB Files ===== |
AD9864/AD9874 Evalaution Board Schematic Board 15006 Rev B {{:resources:eval:user-guides:15006_revb.pdf| SCHEMATIC [PDF File]}} \\ | AD9864/AD9874 Evalaution Board Schematic Board 15006 Rev C {{:resources:eval:user-guides:15006c_sch.pdf| SCHEMATIC [PDF File]}} \\ |
AD9864/AD9874 Evaluation Board Gerber Files Board 15006 Rev B {{:resources:eval:user-guides:gerber_15006b.zip| GERBERS [Zip File]}} \\ | AD9864/AD9874 Evaluation Board Gerber Files Board 15006 Rev C {{:resources:eval:user-guides:gerber_15006c.zip| GERBERS [Zip File]}} \\ |
AD9864/AD9874 Evaluation Board BOM File Board 15006 Rev B {{:resources:eval:user-guides:15006b_bom.xls|Bill of Material [XLS file]}} \\ | AD9864/AD9874 Evaluation Board BOM File Board 15006 Rev C {{:resources:eval:user-guides:15006c_bom.zip|Bill of Material [Zip file]}} \\ |
\\ | \\ |
\\ | \\ |
===== AD9864/AD9874 Software Files ===== | ===== AD9864/AD9874 Software Files ===== |
AD9864/AD9874 DemoTool Software Installation Files {{:resources:eval:user-guides:ad9864_74_spi_gui.zip| AD9864_74 SPI GUI [Zip File]}} | AD9864/AD9874 DemoTool Software Installation Files {{:resources:eval:user-guides:ad9864_74_spi_gui_.zip| AD9864_74 SPI GUI [Zip File]}} |
| |
ADI Visual Analog Software Installation Files | ADI Visual Analog Software Installation Files |
[[http://www.analog.com/en/design-center/interactive-design-tools/visualanalog.html|ADI Visual Analog]] | [[adi>en/design-center/interactive-design-tools/visualanalog.html|ADI Visual Analog]] |
\\ | \\ |
\\ | \\ |