This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revision | Last revisionBoth sides next revision | ||
resources:eval:ad9695-1300ebz [19 Jul 2018 16:15] – [Configuring the Board] Judy Chui | resources:eval:ad9695-1300ebz [29 Aug 2019 20:20] – [Configuring the Board] Judy Chui | ||
---|---|---|---|
Line 61: | Line 61: | ||
- The [[ads7-v2|ADS7-V2EBZ]] should appear in the Device Manager as shown in Figure 6.< | - The [[ads7-v2|ADS7-V2EBZ]] should appear in the Device Manager as shown in Figure 6.< | ||
- If the Device Manager does not show the [[ads7-v2|ADS7-V2EBZ]] listed as shown in Figure 6, unplug all USB devices from the PC, uninstall and re-install ACE and restart the hardware setup from step 1. | - If the Device Manager does not show the [[ads7-v2|ADS7-V2EBZ]] listed as shown in Figure 6, unplug all USB devices from the PC, uninstall and re-install ACE and restart the hardware setup from step 1. | ||
- | - On the AD9695 evaluation board, provide a clean, low jitter | + | - On the AD9695 evaluation board, provide a clean, low jitter |
- On the ADS7-V2, provide a clean, low jitter clock source to connector **J3** and set the amplitude to 10 dBm. This is the Reference Clock for the gigabit transceivers in the FPGA. The REFCLK frequency can be calculated using the following empirical formulae:< | - On the ADS7-V2, provide a clean, low jitter clock source to connector **J3** and set the amplitude to 10 dBm. This is the Reference Clock for the gigabit transceivers in the FPGA. The REFCLK frequency can be calculated using the following empirical formulae:< | ||
- On the AD9695 evaluation board, connect a clean signal generator with low phase noise to **J101** or **J104** via coaxial cable for channels A and B respectively. It is recommended to use a narrow-band, | - On the AD9695 evaluation board, connect a clean signal generator with low phase noise to **J101** or **J104** via coaxial cable for channels A and B respectively. It is recommended to use a narrow-band, |