This shows you the differences between two versions of the page.
Both sides previous revisionPrevious revisionNext revision | Previous revision | ||
resources:eval:ad9694-500ebz [14 Jan 2021 05:11] – user interwiki links Robin Getz | resources:eval:ad9694-500ebz [20 May 2022 17:52] (current) – [Visual Analog Setup] Judy Chui | ||
---|---|---|---|
Line 71: | Line 71: | ||
- On the VisualAnalog “New Canvas” window, and select the desired canvas. **Note: The current canvases for VisualAnalog only support operating both pairs of channels in the AD9694 in the same chip operating mode with the same decimation rate. If Pair AB is in full bandwidth mode then Pair CD must also be in full bandwidth mode. If Pair AB is in real DDC0/DDC1 mode with a decimation rate of 2 then pair CD must also be in real DDC0/DDC1 mode with a decimation rate of 2.**{{ : | - On the VisualAnalog “New Canvas” window, and select the desired canvas. **Note: The current canvases for VisualAnalog only support operating both pairs of channels in the AD9694 in the same chip operating mode with the same decimation rate. If Pair AB is in full bandwidth mode then Pair CD must also be in full bandwidth mode. If Pair AB is in real DDC0/DDC1 mode with a decimation rate of 2 then pair CD must also be in real DDC0/DDC1 mode with a decimation rate of 2.**{{ : | ||
- Next, program the FPGA in VisualAnalog by clicking into the **ADC Data Capture Settings** block and selecting the **Capture Board** tab. Use the **Browse** button to navigate to the **ad9694_ads7v2.bin** file and then click **Program**. The **FPGA_DONE** LED should illuminate on the ADS7-V1 board indicating that the FPGA has been correctly programmed. {{ : | - Next, program the FPGA in VisualAnalog by clicking into the **ADC Data Capture Settings** block and selecting the **Capture Board** tab. Use the **Browse** button to navigate to the **ad9694_ads7v2.bin** file and then click **Program**. The **FPGA_DONE** LED should illuminate on the ADS7-V1 board indicating that the FPGA has been correctly programmed. {{ : | ||
- | - Click the **General** button in the **ADC Data Capture Settings** block. On the **General** tab make sure the clock frequency is set to 2x the input clock. For example, if the input clock to the AD9694 is 368.64 MHz then set the **Clock Frequency (MHz)** to 737.28 MHz. The FFT capture length may be changed to 131072 (128k) or 262144 (256k) per channel. The ADS7-V2 FPGA software supports up to 2M FFT capture (1M per channel).{{ : | + | - Click the **General** button in the **ADC Data Capture Settings** block. On the **General** tab make sure the clock frequency is set to match the sample |
- If VisualAnalog opens with a collapsed view, click on the “Expand Display” icon (see figure 5){{ : | - If VisualAnalog opens with a collapsed view, click on the “Expand Display” icon (see figure 5){{ : | ||
- On the **Device** tab. Make sure that **Enable Alternate REFCLK** option is checked. | - On the **Device** tab. Make sure that **Enable Alternate REFCLK** option is checked. | ||
Line 106: | Line 106: | ||
- When making changes to the DDC settings the **DDC Soft Reset** must be written afterwards. | - When making changes to the DDC settings the **DDC Soft Reset** must be written afterwards. | ||
==== Obtaining an FFT - 1 DDC Per ADC Pair in Complex Mode with Decimation by 2 Mode ==== | ==== Obtaining an FFT - 1 DDC Per ADC Pair in Complex Mode with Decimation by 2 Mode ==== | ||
- | - The first item to configure in Visual Analog is the input clock frequency. | + | - The first item to configure in Visual Analog is the input clock frequency. |
- | - In this example, with an input clock of 368.64MHz, the output sample rate is 184.32MSPS. | + | - In this example, with a sample |
- Click the Run button in Visual Analog and you should see the capture data similar to the plot below. {{ : | - Click the Run button in Visual Analog and you should see the capture data similar to the plot below. {{ : | ||
- Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the **Fund Power** reading in the left panel of the VisualAnalog FFT window.) Adjust the input signal to -1.4 dBFS or less in the FFT in Visual Analog (this accounts for the approximately -0.4 dB loss in the DDC. Recall that the mixing process incurs a 6dB additional loss; the signal amplitude is -7.4 dBFS in this plot. | - Adjust the amplitude of the input signal so that the fundamental is at the desired level. (Examine the **Fund Power** reading in the left panel of the VisualAnalog FFT window.) Adjust the input signal to -1.4 dBFS or less in the FFT in Visual Analog (this accounts for the approximately -0.4 dB loss in the DDC. Recall that the mixing process incurs a 6dB additional loss; the signal amplitude is -7.4 dBFS in this plot. |