This shows you the differences between two versions of the page.
Next revision | Previous revision | ||
resources:eval:ad9681-125ebz [20 Oct 2013 01:11] – created Doug Ito | resources:eval:ad9681-125ebz [09 Jan 2021 00:22] (current) – user interwiki links Robin Getz | ||
---|---|---|---|
Line 1: | Line 1: | ||
+ | ====== EVALUATING THE AD9681 ANALOG-TO-DIGITAL CONVERTER ====== | ||
+ | ===== Preface ===== | ||
+ | This user guide describes the [[adi> | ||
+ | \\ | ||
+ | \\ | ||
+ | There are two versions of the [[adi> | ||
+ | \\ | ||
+ | \\ | ||
+ | The [[adi> | ||
+ | |||
+ | ===== Typical Measurement Setup ===== | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 1. Evaluation Board Connection—[[adi> | ||
+ | </ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 1A. Evaluation Board Connection—[[adi> | ||
+ | </ | ||
+ | ===== Features ===== | ||
+ | * SPI interface for setup and control | ||
+ | * External, on-board oscillator | ||
+ | * On-board LDO regulator or switching regulator, needing a single external 6V, 2A dc supply | ||
+ | * ADC VREF configurable for ADC-internal reference, on-board reference, off-board reference | ||
+ | * VisualAnalog® and SPIController software interfaces | ||
+ | |||
+ | ===== Helpful Documents ===== | ||
+ | * [[adi> | ||
+ | * High speed ADC FIFO evaluation kit ([[adi> | ||
+ | * HSC-ADC-EVALDZ Wiki Guide [[/ | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | |||
+ | ===== Design and Integration Files ===== | ||
+ | * [[adi> | ||
+ | * {{: | ||
+ | ===== Equipment Needed ===== | ||
+ | * Analog signal source(s) and antialiasing filter(s) | ||
+ | * Sample clock source (if not using the on-board crystal oscillator) | ||
+ | * Switching power supply (6.0V, 2.5A) for AD9681-125EBZ | ||
+ | * Switching power supply (12V, 3,3A) for HSC-ADC-EVALDZ or HSC-ADC-EVALEZ | ||
+ | * PC running Windows® | ||
+ | * USB 2.0 port | ||
+ | * [[adi> | ||
+ | * [[adi> | ||
+ | |||
+ | ===== Getting Started ===== | ||
+ | This section provides quick start procedures for using the [[adi> | ||
+ | |||
+ | ==== Configuring the Board ==== | ||
+ | Before using the software for testing, configure the evaluation board as follows: | ||
+ | - Connect the evaluation board to the data capture board, as shown in Figure 1. The Tyco connector version slides horizontally to connect to the [[adi> | ||
+ | - On the ADC evaluation board, confirm that the jumpers are installed as shown in Figure 2. | ||
+ | - Connect one 6V, 2.5A switching power supply (such as the CUI, Inc., EPS060250UH-PHP-SZ that is supplied) to the [[adi> | ||
+ | - Connect the 12V, 3.3A switching power supply to the [[adi> | ||
+ | - Connect the capture board to the PC using a USB cable. | ||
+ | - On the ADC evaluation board, use a clean signal generator with low phase noise to provide an input signal to the desired channel(s). Use a shielded, RG-58, 50Ω coaxial cable (optimally 1 m or shorter) to connect the signal generator. For best results, use a narrow-band, | ||
+ | |||
+ | ===== Evaluation Board Hardware ===== | ||
+ | The evaluation board provides the support circuitry required to operate the [[adi> | ||
+ | \\ | ||
+ | See [[adi> | ||
+ | |||
+ | ==== Power Supplies ==== | ||
+ | This evaluation board comes with a wall-mountable switching power supply that provides a 6V, 2A maximum output. Connect the supply to a 100V ac to 240V ac, 47Hz to 63Hz wall outlet. The output from the supply is provided through a 2.1mm inner diameter jack that connects to the printed circuit board (PCB) at P101. The 6V supply is fused and conditioned on the PCB before connecting to the low dropout linear regulators that supply the proper bias to each of the various sections on the board.\\ | ||
+ | \\ | ||
+ | The evaluation board can be powered in a nondefault condition using external bench power supplies. To do this, remove the E102, E103, E110, and E113 ferrite beads to disconnect the on-board LDOs from the power planes. Note that in some board configurations some of these might already be uninstalled. P102 and P103 headers can be installed to facilitate connection of external bench supplies to the board. E106, E107, E108 and E109 need to be populated to connect P102 and P103 to the board power domains. A 1.8V , 0.5A supply is needed for both 1.8V_DUT_AVDD and 1.8V_DRVDD. Although the voltage requirements are the same for 1.8V_DUT_AVDD and 1.8V_DRVDD, it is recommended that separate supplies be used for each of these.\\ | ||
+ | \\ | ||
+ | Two additional supplies, 3.3V_CLK and 1.8V_DVDD, are used to power additional on board circuitry. If used, these supplies should each have at least 0.5A current capability.\\ | ||
+ | |||
+ | ==== Input Signals ==== | ||
+ | When connecting the ADC clock and analog source, use clean signal generators with low phase noise, such as the Rohde & Schwarz SMA, or an equivalent. Use a shielded, RG-58, 50Ω coaxial cable (optimally 1 m or shorter) for connecting to the evaluation board. Enter the desired frequency and amplitude (see the Specifications section in the data sheet). When connecting the analog input source, use of a multipole, narrow-band band-pass filter with 50Ω terminations is recommended. Analog Devices uses band-pass filters from TTE and K&L Microwave, Inc. Connect the filters as close to the evaluation board as possible.\\ | ||
+ | \\ | ||
+ | If an external clock source is used instead of the onboard crystal oscillator, it should also be supplied with a clean signal generator as previously specified for the analog input signals. Analog Devices evaluation boards typically can accept ~2.8V p-p or 13 dBm sine wave input for the clock at the board SMA clock connector. If an external off-board clock source is used, remove the jumper on J804, and C810, to disable and disconnect the on-board crystal oscillator. | ||
+ | |||
+ | ==== Output Signals ==== | ||
+ | The default setup uses the Analog Devices high speed converter evaluation platform ([[adi> | ||
+ | |||
+ | ===== Jumper Settings ===== | ||
+ | Set the jumper settings/ | ||
+ | \\ | ||
+ | == Table 1. Jumper Settings == | ||
+ | ^Jumper | ||
+ | |J204 |Use this jumper to power down the ADC. Using the SPI, the PDWN pin can be configured to invoke the STBY (standby) function instead of power down.| | ||
+ | |P1 |This jumper sets the ADC for SPI communications with the [[adi> | ||
+ | |J804 |This jumper enables the on-board crystal oscillator. Remove this jumper (and optimally C810) if an external off-board clock source is used.| | ||
+ | |J202 |This jumper selects between internal V< | ||
+ | \\ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 2. Default Jumper Connections for [[adi> | ||
+ | </ | ||
+ | {{ : | ||
+ | <WRAP centeralign> | ||
+ | //Figure 2A. Default Jumper Connections for [[adi> | ||
+ | </ | ||
+ | ===== Evaluation Board Circuitry ===== | ||
+ | This section explains the default and optional ADC settings or modes allowed on the [[adi> | ||
+ | \\ | ||
+ | ==== Power ==== | ||
+ | Connect the switching power supply that is supplied in the evaluation kit between a rated 100V ac to 240V ac, 47Hz to 63Hz wall outlet and P101.\\ | ||
+ | \\ | ||
+ | ==== Analog Input ==== | ||
+ | The eight channel inputs on the evaluation board are set up for a double balun-coupled analog input with a 50Ω impedance. The default analog input configuration supports analog input frequencies of up to ~200 MHz.\\ | ||
+ | \\ | ||
+ | ==== RBIAS ==== | ||
+ | RBIAS has a default setting of 10 kΩ (R205 and R288) to ground and is used to set the ADC core bias current. Note that using a resistor value other than 10kΩ, 1% resistors for RBIAS1 and RBIAS2 may degrade the performance of the device.\\ | ||
+ | \\ | ||
+ | ==== Clock ==== | ||
+ | The default clock input circuit is derived from a simple transformer-coupled circuit using a high bandwidth 1:1 impedance ratio transformer (T801) that adds negligible jitter to the clock path. The clock input is 50 Ω terminated and ac-coupled to handle single-ended sinusoidal inputs. The transformer converts the single-ended input to a differential signal that is clipped by CR801 before entering the ADC clock inputs. The [[adi> | ||
+ | \\ | ||
+ | The [[adi> | ||
+ | |||
+ | ===== Modes of Operation ===== | ||
+ | ==== Standalone (PIN) Mode ==== | ||
+ | The [[adi> | ||
+ | Table 2 and Table 3 specify the settings for pin mode operation. | ||
+ | |||
+ | == Table 2. Digital Output Format Pin Settings == | ||
+ | ^SDIO/OLM (P1 Pin 2) Voltage | ||
+ | |1.8V_DUT_AVDD (jumper P1 Pin 2 to Pin 3) |Two-lane. 1× frame, 16-bit serial output| | ||
+ | |GND (" | ||
+ | |||
+ | == Table 3. Digital Test Pattern Pin Settings == | ||
+ | ^SCLK/DTP (P1 Pin 5) Voltage | ||
+ | |GND (" | ||
+ | |1.8V_DUT_AVDD (jumper P1 Pin 5 to Pin 6) |10 0000 0000 0000 | | ||
+ | |||
+ | Note that the above settings only apply when CSB1 and CSB2 are tied high (P1 Pin 8 and Pin 11 " | ||
+ | |||
+ | Additional information on the Standalone (PIN) Mode is provided in the [[adi> | ||
+ | ==== Default Mode ==== | ||
+ | To operate the device under test (DUT) using the SPI, follow the jumper settings for P1 as shown in Table 1. | ||
+ | |||
+ | ===== How To Use The Software For Testing ===== | ||
+ | ==== Setting up the ADC Data Capture ==== | ||
+ | The installers for VisualAnalog and SPIController are in the following locations: | ||
+ | [[ftp:// | ||
+ | [[ftp:// | ||
+ | Run these installers on the PC that is connected to the evaluation setup before proceeding. | ||
+ | |||
+ | After configuring the board hardware, set up the ADC data capture using the following steps: | ||
+ | - Start VisualAnalog on the connected PC. The appropriate part type should be listed in the status bar of the **VisualAnalog – New Canvas** window. Select the template that corresponds to the type of testing to be performed (see Figure 3).{{ : | ||
+ | - After the template is selected, a message might appear asking if the default configuration can be used to program the FPGA (see Figure 4). If this message appears, click **Yes**, and the window will close.\\ {{ : | ||
+ | - To change features to settings other than the default settings, click the **Expand Display** button, located on the bottom right corner of the window (see Figure 5), to see what is shown in Figure 6.\\ | ||
+ | {{ : | ||
+ | <WRAP centeralign>// | ||
+ | \\ | ||
+ | \\ | ||
+ | \\ | ||
+ | </ | ||
+ | <WRAP centeralign>// | ||
+ | 4. To configure VisualAnalog to operate with the AD9681, push the Settings button on the ADCDataCapture block, as shown in Figure 7. | ||
+ | {{ : | ||
+ | <WRAP centeralign>// | ||
+ | \\ | ||
+ | \\ | ||
+ | 5. In the ADC Data Capture Settings Window, General Tab, select AD9681 to be the device, enter the sample clock frequency (125 is the default value), as shown in Figure 8. The sample frequency entered here is used for scaling of frequency values in test results and graphs. In the Output Data field, the channels to be tested are selected, as well as the FFT capture depth (" | ||
+ | {{ : | ||
+ | <WRAP centeralign>// | ||
+ | \\ | ||
+ | \\ | ||
+ | 6. In the ADC Data Capture Settings Window, Capture Board Tab, enter 30 in the Fill Delay field. Push the Browse button to navigate to the FPGA program file for the AD9681. The default installation location and filename will be similar to:\\ | ||
+ | For HSC-ADC-EVALDZ FPGA board\\ | ||
+ | C:\Program Files (x86)\Analog Devices\VisualAnalog\Hardware\HADv6\AD9681_hadv6.mcs\\ | ||
+ | For HSC-ADC-EVALEZ FPGA board\\ | ||
+ | C:\Program Files (x86)\Analog Devices\VisualAnalog\Hardware\HADv6\ad9681_evalez.mcs\\ | ||
+ | Select the appropriate program and then push the **program button**. | ||
+ | {{ : | ||
+ | <WRAP centeralign>// | ||
+ | \\ | ||
+ | \\ | ||
+ | 7. VisualAnalog is now setup to work with the AD9681-125EBZ in the default condition. Other VisualAnalog features and capture settings are documented in the [[adi> | ||
+ | ===== Evaluation And Test ===== | ||
+ | ==== Setting up the SPI Controller Software ==== | ||
+ | After the ADC data capture board setup is complete, set up the SPI controller software using the following procedure: | ||
+ | - Open the SPI controller software by going to the **Start** menu or by double-clicking the **SPIController** software desktop icon. If prompted for a configuration file, select .cfg file whose name begins with AD9681. If not prompted, check the title bar of the window to determine which configuration is loaded. If necessary, choose **Cfg Open** from the **File** menu and select the appropriate file based on your part type. Note that the **CHIP ID(1)** box should be filled to indicate whether the correct SPI controller configuration file is loaded (see Figure 10).{{ : | ||
+ | - Click the **New DUT** button in the **SPIController** window (see Figure 11){{ : | ||
+ | - In the **ADCBase 0** tab of the **SPIController** window, find the **CLOCK DIVIDE(B)** box (see Figure 12), and the **MODES(8)** box (see Figure 13). If using the clock divider, use the drop-down box to select the correct clock divide ratio, if necessary. If there is any interruption of the ADC clock during power-up or during operation, a Digital Reset may be needed to re-initialize the ADC (Figure 13). For additional information, | ||
+ | - Note that other settings can be changed on the **ADCBase 0 tab** (see Figure 12) and the **ADC A** through **ADC D** tabs (see Figure 14) to set up the part in the desired mode. The **ADCBase 0** tab settings affect the entire part, whereas the settings on the **ADC A** through **ADC D** tabs each affect the selected channel only. The B1 (Bank1), B2 (Bank2) and All buttons at the right end of the SPIController button row (as seen in Figure 13 and Figure 14) determine which bank of ADCs is affected by the SPIController settings. The All button is pushed by default which means that the **ADCBase 0** tab settings affect all channels on both ADC banks. The settings in the **ADC A** through **ADC D** will likewise affect their respective channels in both banks. For example, with the All button pushed, settings in the **ADC A** tab will affect channels A1 and A2. If the All button is un-pushed and the B1 (Bank1) button remains pushed, the settings in the **ADC A** tab will only affect channel A1. See the data sheet, the [[adi> | ||
+ | - Invoke a Digital Reset as shown in Figure 13 before testing. After selecting Reset, select Chip run to return to normal operation. | ||
+ | - To begin testing, click the **Run** or **Continuous Run** button in the **VisualAnalog** toolbar (see Figure 15).{{ : | ||
+ | |||
+ | ==== Adjusting the Amplitude of the Input Signal ==== | ||
+ | The next step is to adjust the amplitude of the input signal for each channel as follows: | ||
+ | - Adjust the amplitude of the input signal so that the fundamental is at the desired level. Examine the **Fund Power** reading in the left panel of the **VisualAnalog Graph - AD9681 FFT** window (see Figure 16).{{ : | ||
+ | - Repeat this procedure for the other channels, if desired | ||
+ | - Click the floppy-disk icon within the **VisualAnalog Graph - AD9681 FFT** window to save the performance data as a .csv formatted file for plotting or analysis. | ||
+ | ===== Troubleshooting Tips ===== | ||
+ | Lack of SPI communication will cause difficulty in configuring the ADC. | ||
+ | * Go to the **Global** tab of the **SPIController** window and push the **Read** button in the **GENERIC READ/ | ||
+ | * Check that there is correct power to the [[adi> | ||
+ | * Check that the USB cable is properly connected from the PC to the [[adi> | ||
+ | * The LED on the **VisualAnalog ADCDataCapture** block should be green. If it is red, push the USB button on the same block to refresh the connection.\\ | ||
+ | |||
+ | If the FFT plot appears abnormal, do the following: | ||
+ | * If you see an abnormal noise floor, go to the **ADCBase0** tab of the **SPIController** window and toggle the **Chip Power Mode** in **MODES(8)** from **Chip Run** to **Reset** and back (Figure 13). | ||
+ | * If you see a normal noise floor when you disconnect the signal generator from the analog input, be sure that you are not overdriving the ADC. Reduce the input level, if necessary. | ||
+ | * In **VisualAnalog**, | ||
+ | |||
+ | If the FFT appears normal but the performance is poor, check the following: | ||
+ | * Make sure that an appropriate filter is used on the analog input. | ||
+ | * Make sure that the signal generators for the clock and the analog input are clean (low phase noise). | ||
+ | * Change the analog input frequency slightly if noncoherent sampling is being used. | ||
+ | * Make sure that the SPI configuration file matches the product being evaluated.\\ | ||
+ | |||
+ | If the FFT window remains blank after **Run** in VisualAnalog is clicked, do the following: | ||
+ | * Make sure that the evaluation board is securely connected to the [[adi> | ||
+ | * Make sure that the correct FPGA program was installed by clicking the **Settings** icon in the **ADC Data Capture** block in VisualAnalog. Then select the **FPGA** tab and verify that the proper FPGA .mcs file (one containing " | ||
+ | * Make sure that the FPGA has been programmed by verifying that the **DONE** LED is illuminated on the [[adi> |